How Does the Fuel Cell Come to Have So Many Advantages?

1. Because It's a Fuel Cell Not a Storage Cell!

The name "cell" can be misleading: the fuel cell is not a storage battery, it is a device that directly converts the chemical energy of hydrogen and oxygen into electricity. The fuel cell can continue to produce electricity as long as it is fed with hydrogen and oxygen and the reaction products are removed. The fuel cell uses a catalyst to combine hydrogen and oxygen to produce electricity, with water formed as a byproduct. This is the key to its great advantages. For because it produces electricity directly from a chemical reaction, it is far more efficient than conventional processes which need various energy conversions for producing electric power. Although the principle is simple, and has been known since it was used in the early U.S. space program, Toshiba's engineers have expanded the useful life of the fuel cell, ensuring long service at high efficiencies, and greatly widened the range of possible useful applications. For instance, a total 172 units of the 200kW-capacity PC25 series fuel cell have been already delivered to 58 nations, and have an accumulated total running time of 1.6 million hours.

2. Because It Uses Readily Available Fuels

The fuel cell can use the unlimited supply of oxygen in the air, and almost any hydrogen-rich gas. Methane generated from biomass (composted vegetation), or the anaerobic digester gas from sewage or other waste products, are among the wide range of possible sources that include natural gas, LPG and naphtha. This means inherently low fuel costs and/or useful contributions to the costs of running sewage or waste-treatment plants.

3. Because It is Essentially Non-Polluting

Because the power plants uses only low-temperature combustion of the hydrogen discharged from the anode, the oxides of nitrogen and sulfur compounds that can cause serious pollution, including acid rain, occur in inherently very low concentrations.

4. Because It is Highly Efficient and Compact

The basic energy conversion efficiency of the Toshiba PC25C for electricity generation is 40%, equivalent to very large and most efficient thermal power stations. But the heat energy released can also be used (so-called co-generation), and even the byproduct water is valuable wherever water is in short supply. This raises the potential overall efficiency to 80%! And this efficiency is achieved in a very compact unit. For instance, the 200kW PC25C is only 5.5m wide, 3.0m high, and 3.0m wide!

5. Because the Applications are Virtually Unlimited

Fuel cells, which generate direct current (DC), are combined with AC converters (another Toshiba specialty) to provide independent electricity supplies for hospitals or computer centers, where power failures could have disastrous consequences. Such units can also help utility companies to provide cost-effective distributed generation to supplement the power grid, and serve to make waste- and sewage-treatment plants more economically viable. The car manufacturers are also looking to small fuel cells to provide non-polluting power for the next generation of cars. The clear advantages of the fuel cell, long evident to Toshiba engineers, have now been recognized by the prestigious award of the Minister of Trade and Industry. Toshiba is therefore ideally positioned to serve the power needs of the century about to dawn.

Visit the Toshiba America homepage for more information.

Now visit Toshiba's Web Site in PointCast by clicking here.