toshiba worldwide   toshiba america
     
 
Search:  
 
Products
Microwave
Related Information
Press Releases  |  Product Brief  |  Power FETs for Solid-state Power Amplifiers Article  |  Product Guide  |  Power GaAs FET Application Note  | 

Toshiba is a leading supplier of high-performance gallium arsenide (GaAs) microwave devices as well as a new line of gallium nitride (GaN) high electron mobility transistor (HEMT) products that operate in the X frequency band. The company's line-up of products consists of a series of components within the S, C, X and Ku frequency bands, which are used in a wide variety of wireless applications. These applications include personal communications systems (PCS), multi channel distribution system (MMDS), Wireless LAN/WAN systems, point-to-point terrestrial microwave radio, wireless local loop (WLL), satellite communications systems (SATCOM) such as high power solid state power amplifiers (SSPA) and very small aperture terminals (VSAT), radar systems, mobile communications and other communication systems. Targeted applications for the new GaN products include satellite communications (SATCOM), terrestrial point-to-point communications, radar systems and medical applications such as those used in oncology.

C-, S-, X- and Ku-Band
Toshiba continues to maintain its leadership in the C-, S-, X- and Ku-Band frequency ranges by developing the highest output power, as well as offering the broadest product line-up in the industry. The C- and Ku-Band devices are optimized for use in solid-state power amplifiers (SSPAs) for SATCOM and VSAT applications. The power level for

C-Band is 4 watts (W) up to 80W, which is the highest offered in the industry for its frequency band. In addition, the Ku-Band also offers the highest power levels in the industry for its frequency band, ranging from 2W to 30W. The first GaN product, the TGI8596-50, provides output power of 50W. Higher gain, higher output power GaN devices are currently under development.

Toshiba also offers an ultra linear GaAs FETs product family, designated the UL family, for C-Band frequency range with higher gain, lower intermodulation distortion and higher efficiency. The UL product family includes products from 4 watts (W) up to 25W and was developed for point-to-point microwave digital radio for terrestrial communications and block up converter or VSAT terminal for satellite communications.

Toshiba America Electronic Components, Inc. (TAEC) is the North American engineering, manufacturing, marketing, and sales arm for Toshiba Microwave Semiconductors. TAEC has established customer service, engineering support sales offices, and sales representatives throughout North America to provide the best possible service.

Please browse the product categories on the left for detailed datasheets on the latest microwave devices available from Toshiba. For availability and pricing, please contact the TAEC sales office or the sales representative nearest you (see the "Sales Contact" tab above).