TOSHIBA
United States
Toshiba USA   Toshiba Americas   Toshiba Worldwide
 
 
Enter Search Term
 
Home  News  Media Resources  Product Overview
Product Overview

Products that Help Lead Innovation
Toshiba offers a broad range of enabling technology solutions that allow OEMs, ODMs, CMs, VARs, and fabless chips companies to develop advanced integrated products for the computing, networking, communications, digital consumer, automotive and other markets. Photo Gallery
 
 
 
Analog Components

A wide selection of LED display drivers and LED backlight/lighting drivers, shock sensor amplifier ICs, audio power amps, motor controller and driver (MCDs) ICs including DC brushed motor drivers, stepping motor drivers, and brushless (BLDC) motor controllers /drivers and more. more

Automotive

Toshiba offers single-chip CD-MP3 ICs, audio amps, graphics display chips, Bluetooth ICs, RFICs, ARM® processor based Microcontrollers for entertainment/information, body/chassis and safety/security applications. These Toshiba system-level solutions reduce cost, design cycles and enhance reliability. more

Custom System-on-Chip (SoC)/ASIC

Toshiba is an industry leader in providing ASIC and COT services to customers that require advanced CMOS process technologies. Key offerings from the company include support for 65nm, 40nm and 28nm CMOS process technologies, advanced 300 mm wafer fab, shuttle services that enable an ASIC prototype with low NRE costs, two U.S.-based Design Centers and more. more

Diodes

Toshiba offers a broad line up of diodes including general-purpose, fast and ultra-fast recovery, Schottky, PiN diodes for RF switch, Varactors for voltage-controlled oscillators (VCO), and diodes for ESD protection. more

Imaging Components

Toshiba is a leader in imaging solutions and provides a wide range of CMOS sensors that feature Backside Illumination (BSI) for better light sensitivity and CCD (charge-coupled device) image sensors. The Toshiba CMOS image sensors employ a low-noise pixel structure that achieves high-picture quality with low-power consumption, even in low-light conditions, for camera phones and other mobile applications. Toshiba has also a line of ultra-compact camera modules with a 64 percent reduction in module size compared to other modules using the same sensor. The CCD linear image sensors provide speed and high-image quality for printers, scanners, and bar-code readers. more

Linear ICs

Toshiba offer a wide range of general purpose linear ICs including power supply ICs, intelligent power devices, motor drivers, operational amplifier ICs & comparator ICs, interface drivers and small signal MMICs. more

Logic ICs

As a leader in logic technology, Toshiba offers one of the industry's broadest selection of logic products specializing in low voltage and small packaging options to meet today's design demands for computing, consumer and telecommunications. more

Medical and Industrial Tubes

Toshiba offers imaging system components for a variety of medical, dental and industrial applications. Toshiba also provides microwave tubes used for broadcasting, data communications, radar devices, medical accelerators and industrial heating, along with higher power devices for advanced scientific fields such as large-scale accelerators and nuclear fusion facilities. more

Memory

Toshiba is the inventor of NAND Flash technology and the principal innovator of both NOR and NAND Flash memory. Today, Toshiba offers one of the industry's broadest line-ups of MLC and SLC NAND Flash-based storage solutions enabling a wide range of applications. The company offers enterprise grade NAND Flash components, solid state drives, embedded NAND Flash solutions such as e-MMC™, SmartNAND™ and BENAND™ and removable SD Cards and USB Flash drives with industry leading performance and capacities. A leading innovator in packaging technology, Toshiba also offers Multi-chip Packages (MCPs) combining NAND and other memory devices in a single component for mobile devices. more

Microcontrollers

The company offers an extensive line-up of 32-bit microcontrollers based on ARM® processing cores and 8-, 16- and 32-bit CISC and 32-bit RISC microcontrollers using Toshiba's original design CPU cores. Toshiba microcontrollers contain a wide selection of memory options, LCD controllers, power ranges, clock speeds and other popular on-chip peripherals, to cover a wide array of applications such as consumer products, home appliances, home automation, industrial and automotive applications. more

Microwave Products

Toshiba is a leading supplier of high-performance gallium nitride (GaN) and gallium arsenide (GaAs) microwave devices that operate in S, C, X, Ku and Ka frequency bands. The company's high power products are used in wireless applications such as, SATCOM (SSPA/BUC/VSAT), microwave link (PTP, PTMP), RADAR, medical equipment, and industrial applications. Toshiba recently introduced the development of Ka-band high power GaN HEMTs to support SATCOM applications and new efficient, high-gain power GaAs FETs, MMICs, and modules. more

Optical Semiconductor Devices

As a leading Optoelectronics supplier, Toshiba offers a wide range of photocouplers. Housed in a white mold package, Toshiba's photocouplers consist of either a GaAs or GaAlAs infrared LED(s) and a silicon photodetector(s). GaAlAs LEDs are adopted in high-speed photo-IC types due to their high-speed and high-light output. Toshiba's innovative white mold packaging contributes to high sensitivity, high CTR and superb reliability. To meet the space-saving requirements of increasingly smaller and thinner end products, packaging options include mini-flat packages (MFSOPs) and half-pitch (1.27 mm) mini-flat SOP packages. Toshiba also offers a series of fiber optic devices called TOSLINK™ which use optical interconnects to achieve noise-free transmission. more

RF Devices

Toshiba offers broad line up of Radio-Frequency devices which include MOSFETs, Bipolar transistors, Diodes, RF Cell packs, and RF amplifier ICs. A complete line-up of surface-mounted parts is offered to support miniaturized, higher-performance electronic devices. more

Storage Products

Toshiba is a leading total storage provider who combines execution agility with the resources of a global technology corporation. We offer the industry's most comprehensive range of storage technologies, from hard disk drives (HDDs) to solid state drives (SSDs). Toshiba is the world's only storage supplier that owns design, development, manufacturing, sales, and other infrastructure functions spanning the enterprise, mobile, and retail environments for both HDD and SSD products. more

Transistors

Toshiba offers power semiconductors for computing, consumer, industrial and automotive applications that require high reliability, power efficiency and a compact design. The product line includes low and high voltage MOSFETs, DC-DC MCMs, DTMOS, IGBTs, Bipolar Transistors, Diodes, Regulators, IPDs, Transistor Couplers, IC couplers and System Power Devices. more

Wireless/Mobile Applications Products

Toshiba now offers TransferJet™ a close-proximity wireless data transfer LSI for transfer of large files between electronic devices by simply touching the devices together. As a founding member of the Bluetooth SIG, participation in the TransferJet Consortium and participant in other standards bodies such as MPEG and MIPI, Toshiba products are designed to comply with applicable global standards. Toshiba RFICs for keyless entry and tire pressure monitoring systems, bridge chips, LCD controllers, flexible I/O expanders, and Bluetooth ICs provide the right technology to meet wireless communications design needs. These products enable new features in mobile handsets, portable consumer electronics, tablets, ebooks and other mobile devices. more wireless more mobile apps

1Based on MTBF statistical values. MTBF (Mean Time Between Failure) is not a guarantee or estimate of product life; it is a statistical value related to mean failure rates for a large number of products which may not accurately reflect actual operation. Actual operating life of the product may not resemble the MTBF.

SmartNAND and TOSLINK are trademarks of Toshiba Corporation.

Bluetooth is a trademark of the Bluetooth SIG. ARM is a registered trademark of ARM Limited in the EU and other countries. e-MMC is a trademark of the MultiMediaCard Association.

All other tradenames are trademarks of their respective manufacturer and may be registered in certain jurisdictions.

TransferJet is a trademark of Sony Corporation.