Toshiba
News
   
Print This Page   Close Window
 

TOSHIBA ANNOUNCES COMPLETE RF SOLUTION FOR DIGITAL TV TUNERS

Extensive Line of Consumer Electronics Components Facilitates Rapid Compliance with New FCC Ruling Requiring Digital TV Tuners in New TVs

IRVINE, Calif., October 14, 2002 -- In response to the FCC's recent mandate requiring digital TV tuners in new television sets within two to five years, Toshiba America Electronic Components, Inc. (TAEC)* today announced that the company offers a complete set of radio frequency (RF) integrated discrete devices required for a digital television (DTV) tuner to help enable TV manufacturers to comply with this new ruling. Developed by Toshiba Corp. (Toshiba), these devices include varactors, FETs, dual gate MOSFETS, pin diodes and Schottky Barrier diodes.

Under the new FCC regulation, all but the smallest new televisions sold in the United States must be able to receive digital broadcast signals by 2007. By 2004, digital tuners must be included in half of the sets with 35-inch screens or larger, with other sizes phasing in throughout the five-year transition period. In addition, all TV receiving equipment, such as VCRs and DVD player/recorders must be capable of receiving DTV after July 1, 2007.

"To help TV manufacturers meet this requirement, Toshiba provides a one-stop solution for RF devices," said Tom Chand, business development engineer for TAEC's RF devices. "As a leading supplier of RF discrete devices for consumer electronics (CE) devices, with approximately 40 percent of the market for analog CE devices and 15 percent of the market for digital CE devices, we're prepared to support the industry's transition to digital TV."

"Despite relatively flat TV unit sales, HD integrated sets and monitors are continuing to experience strong growth this year, as shipments are expected to increase about 80 percent over last year," says Danielle Levitas, director of Consumer Devices and Interactive Services research at IDC. "Large screen televisions dominate HDTV sales and the FCC order requiring digital tuner integration into these larger TVs, beginning in mid-2004, will help push the DTV transition forward."

Toshiba's RF solution for DTV tuners includes the discrete devices required for the Low Noise Amplifier (LNA) Gain Control and Mixer functions in the tuner, (See Figure 1. Digital TV Tuner Block Diagram available at tv.tuner.toshiba.com). These devices are optimized for high gain and frequency response with low noise figures for best performance in a DTV application. An Advanced Television System Committee (ATSC) digital tuner must be capable of tuning the entire VHF (30MHz to 300MHz) and UHF (300MHz to 3GHz) broadcast bands as well as all standard cable bands, and Internet Relay Chat (IRC) and HRC bands.

The low noise amplifier is a wideband RF amplifier, that together with the gain control block must increase the signal level into the first mixer while minimizing the receiver noise figure (NF). In most cases the signal strength is very low compared to the carrier noise as the signal is received from the antenna. The LNA is responsible for amplifying the signal, while keeping the carrier noise level low. During the next stage, the signal is sent to the Gain Control block. In a typical design, the Gain Control block is comprised of a two stage mixer with a phase lock loop circuit and a +44MHz amplifier, which locks onto the desired channel and outputs a 44MHz signal from the tuner. The PLL circuit ensures the desired station stays locked. Without it, the station would drift in and out of reception because of the shift in frequency. After the Gain Control block, the desired signal is sent to the final stage Mixer, which incorporates the desired signal and an IF signal, generated from an Oscillator. This "mixed" signal is then out of the Tuner block. For product details, please refer to the technical specifications table below.

About Digital Television
The FCC's mandate is intended to spur the transition to DTV, which is expected to be complete in 2007. Today, television stations in many areas broadcast both conventional analog television signals and digital signals, using additional spectrum for the digital signals on loan from the FCC. More than 200 stations are already broadcasting digital television signals, reaching an estimated 70 percent of U.S. homes. Under the FCC guidelines, once 85 percent of a broadcaster's viewing area is capable of receiving a digital signal, the broadcaster must give back its analog spectrum, which the government plans to auction for other uses, such as wireless applications. Consumers with older TVs will be able to buy set-top boxes if they want to receive broadcasts from digital stations over analog TVs.

Digital TV based on the ATSC digital standard adopted by the FCC will provide improved picture quality with vivid pictures and crisp sound, free from interference, snow and ghosts that can occur with broadcast analog TV signals. In addition to improved pictures, DTV offers a range of new possibilities to broadcasters, such as sending multiple programs over one channel or offering video games, the Internet or interactive services. The digital television signal is enhanced with CD-quality theater-like audio in the 5.1 channel digital Dolby format with separate left and right front channels, left and right rear channels and subwoofer channels.

Technical Specifications: Toshiba RF ICs for Digital TV Tuners
Functional Block of Tuner Application Band Description Part Number Package PriceQ: 3000K
Low Noise Amp Boost incoming signal UHF and VHF Signal Amplifier 2SC3607 PW-MINI $0.49
Gain Control Block Tuning varicap diode Wide-band VHF Automatic Gain Control - Single Pin Diode 1SV271 USC $0.19
RF Amp UHF 9V Dual Gate MOSFET 3SK232 SMQ $0.55
RF Amp UHF 9V Dual Gate MOSFET 3SK291 SMQ $0.27
RF Amp UHF 9V Dual Gate MOSFET 3SK293 USQ $0.29
Mixer Mixer N/A Schottky Diode 3SK260 USQ $0.13
Mixer N/A Schottky Diode 1SS315 USC $0.23

Pricing and Availability
Samples of the devices are available now, with production quantities available in the 4th quarter of 2002.

*About TAEC
Combining quality and flexibility with design engineering expertise, TAEC brings a breadth of advanced, next-generation technologies to its customers. This broad offering includes semiconductors, flash memory-based storage solutions, optical communication devices, displays and rechargeable batteries for the computing, wireless, networking, automotive and digital consumer markets.

TAEC is an independent operating company owned by Toshiba America Inc., a subsidiary of Toshiba, the second largest semiconductor company worldwide in terms of global sales for the year 2001 according to Gartner/Dataquest's Worldwide Semiconductor Market Share Ranking. Toshiba is a world leader in high-technology products with more than 300 major subsidiaries and affiliates worldwide. For additional company and product information, please visit TAEC's web site at chips.toshiba.com. For technical inquiries, please e-mail Tech.Questions@taec.toshiba.com.


TO-245