Toshiba
News
   
Print This Page   Close Window
 

TOSHIBA EXPANDS DYNASTRON™ CMOS IMAGE SENSOR LINE-UP WITH 3.2-MEGAPIXEL CHIP

Adoption of New Higher Resolution Devices in High-End Camera Phones Expected to Spur Displacement of Low-End Digital Still Cameras

SAN JOSE, Calif., September 27, 2005 -- Toshiba America Electronic Components, Inc. (TAEC)* today announced the further expansion of its industry-leading Dynastron™ complementary metal oxide semiconductor (CMOS) image sensor product line with the addition of a new 3.2-megapixel CMOS image sensor chip. Designated ET8E99-AS, the new chip has a small 2.7-micron (um) pixel pitch with a 1/2.6-inch optical format and incorporates an analog-to-digital (A/D) converter. Combining superb picture quality with low-power consumption, it is targeted at high-end camera-enabled mobile handset applications. Toshiba Corporation (Toshiba) will be exhibiting the ET8E99-AS at CEATEC JAPAN 2005 being held from October 4 to October 8 at Makuhari Messe.

"With the launch of the new 3.2-megapixel ET8E99-AS CMOS image sensor, we can meet cell phone manufacturers' high-end camera phone requirements for a small device with excellent image quality and low-light performance. This advancement heralds the real start of camera phones competing directly with and displacing low-end digital still cameras," said Andrew Burt, director of the Wireless Business Unit at TAEC. "Concurrently we project continued strong demand for our existing complement of 2-megapixel, 1.3-megapixel and VGA-resolution Toshiba Dynastron CMOS image sensors. Our customers tell us that Toshiba satisfies a critical need with its ability to support the full range of market requirements across resolution sizes in production volumes."

The ET8E99-AS CMOS image sensor is an area color image sensor that incorporates an A/D converter in non-diced wafer form. It achieves approximately 3.2 megapixels of array resolution in a small 1/2.6-inch optical format with reduced pixel pitch of 2.7um and a pixel size sufficient to record detailed, high-resolution images. It also offers low-power consumption, smearless imaging and high-speed operation.

Other Features
Other features include the following:
  • In video mode, capable of a high-speed frame rate of 15 frames per second (fps) at QXGA output and 30fps at 3-to-1 vertical pixel binning
  • To support simplified design of an optimized camera system, incorporates automatic blemish correction and detection, gain control and lens shading compensation
  • To support a flexible input clock, incorporates a phase locked loop circuit
  • Can use with a companion Toshiba image signal processor (ISP) chip that provides YUV or JPEG encoded data or employ another suitable external ISP chip

Toshiba Dynastron CMOS Image Sensors

Toshiba is a pioneer and recognized leader in the development of CMOS image sensors with core competencies in advanced sensor technology and sophisticated signal processing technology. Toshiba Dynastron CMOS image sensors employ a special square pixel design that enables them to achieve CCD-quality images with low-power consumption, even in low-light conditions. Dynastron CMOS image sensors have proven their superiority in image quality comparisons by offering demonstrably better color balance and picture quality.

Toshiba currently offers the TCM8230MD VGA camera module, the TCM8240MD 1.31-megapixel camera module, and the ET8EA3-AS 2-megapixel and new ET8E99-AS 3.2-megapixel CMOS image sensor chips. The company is continuing to develop devices that combine smaller pixel sizes with higher resolution.

Pricing and Availability
Samples of the ET8E99-AS are currently available with mass production planned for the end of 2005 at a monthly output rate of 300,000 units or greater. Sample pricing is $45.00 each based on a quantity of 1,000 pieces per year.

Technical Specification Summary
Part Number ET8E99-AS
Optical Format 1/2.6 inch
Pixel Count 2,080 (H) x 1,560 (V) maximum
Pixel Pitch 2.7um (H) x 2.7um (V)
Output Signal RAW data: 12-bit parallel/subLVDS serial
Clock Frequency 6MHz to 20MHz
Frame Rate 15fps at QXGA output
30fps at 3-to-1 vertical pixel binning
Interface Control I2C bus
Power Supply 1.5±0.1 volts (V) digital
2.8±0.2V analog and I/O
Power Consumption 240mW at 15fps QXGA output
Operating Temperature -20º - 60°C
Functionality Digital zoomed VGA image in combination with an external processor, automatic blemish detection and correction, lens shading compensation, support for programmable drive strength, variable electronic shutter, variable gain control, built-in feedback clamp
Package Non-diced wafer

*About TAEC
Combining quality and flexibility with design engineering expertise, TAEC brings a breadth of advanced, next-generation technologies to its customers. This broad offering includes memory and flash memory-based storage solutions, a broad range of discrete devices, displays, medical tubes, ASICs, custom SOCs, microprocessors, microcontrollers and wireless components for the computing, wireless, networking, automotive and digital consumer markets.

TAEC is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corp. (Toshiba), Japan's second largest semiconductor manufacturer and the world's ninth largest integrated manufacturer of electric and electronic equipment. In almost 130 years of operation, Toshiba has recorded numerous firsts and made many valuable contributions to technology and society. For additional company and product information, please visit TAEC's website at chips.toshiba.com. For technical inquiries, please e-mail Tech.Questions@taec.toshiba.com.

Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice. Technical and application information contained here is subject to the most recent applicable Toshiba product specifications. In developing designs, please ensure that Toshiba products are used within specified operating ranges as set forth in the most recent Toshiba product specifications and the information set forth in Toshiba's "Handling Guide for Semiconductor Devices," or "Toshiba Semiconductor Reliability Handbook." This information is available at www.chips.toshiba.com, or from your TAEC representative.

All trademarks and tradenames used herein are the properties of their respective holders. Dynastron is a trademark of Toshiba Corporation.

WRLS 05 293