Toshiba
News
   
Print This Page   Close Window
 
TOSHIBA EXPANDS FAMILY OF LOW-PROFILE, LIGHTWEIGHT LED-BACKLIT LCD PANELS FOR NOTEBOOK PCs
New 10.4-inch and 10.6-inch Mercury-Free1 LED Backlit LCD Modules
for Mobile Notebook Applications

TOKYO and IRVINE, Calif., Mar. 20, 2007 —Toshiba Matsushita Display Technology Co., Ltd. (TMD), and Toshiba America Electronic Components, Inc., TMD’s sales and marketing arm in the Americas, announced development of new 10.4-inch and 10.6-inch thin-film transistor (TFT) liquid crystal display (LCD) panels for notebook PC applications, each incorporating an LED (light emitting diode) backlighting system to provide low-profile, lightweight, and low-power consumption features. The newly developed products expand TMD’s range of LED-backlit LCD panels for mobile notebook

 
SMOS PART # SSM3J305
Download Hi Res Image (JPG 770KB)
applications, providing a wide selection of LCDs for customers to choose from among seven main screen sizes from 8.9-inch to 13.3-inch.
TMD has been expanding its lineup of LED-backlit LCD products for notebook applications, combined with proprietary low-temperature poly-silicon (LTPS) technology, beginning with the world's first commercialization of an LED-backlit 11.1-inch WXGA+ resolution LCD panel for notebook PCs in October 2005.

Compared with a conventional cold cathode fluorescent lamp (CCFL) backlighting system, the LED backlighting has distinct advantages such as reduced thickness, reduced weight, increased brightness, and decreased power consumption. In addition, it is Mercury-Free1 and RoHS- Compatible2 . It also features lower operating voltages, which provides another advantage in design and safety aspects. Moreover, an LED backlighting system contributes to increased durability against impacts and vibration.

Including the two newly developed panels, TMD's lineup of LED-backlit TFT LCD panels now offers screen sizes from 8.9-inch to 13.3-inch and pixel resolutions of XGA, WXGA, and WXGA+. This lineup may contribute to further reduction of weight and thickness in portable notebook PCs for mobile applications, while at the same time extending their battery-driven operation.

In these notebook PC panels, in addition to the adoption of an LED-backlight system, TMD has also adopted thinner glass substrates of 0.3 mm or less, reduced the number of component parts to the minimum requirement and optimized layout design for weight reduction. For example, TMD has succeeded in decreasing the weights to 120g for a 10.4-inch XGA module and to 135g for a 12.1-inch XGA module. These improvements have helped to reduce overall module thickness to only 2.5mm for several of TMD's notebook PC LCD products. In conjunction with the successful reduction of weight and thickness, TMD has also achieved a high brightness of level up to 300 candelas per sq. meter (cd/m2 ) in certain products in this family.

TMD foresees strong growth in this area, and these types of LED-backlit panels will exceed 50 percent of TMD's production in late 2007.

TMD will continue to reinforce this product lineup by offering low-profile, lightweight and low-power consumption modules to precisely meet customer needs, and will actively support the enhancement of the usability of mobile notebook PCs.

TAEC Lineup of LED Backlit LCD Products for Notebook PCs
Screen size
Number of pixels
and resolution format
Weight
(g)
Luminance
(cd/m2)
Power consumption (W)
26 cm (10.4-inch)
1024 x 768 / XGA
120
240
2.4
31 cm (12.1-inch)
1024 x 768 / XGA
135
300
3.1
23 cm (8.9-inch)
1280 x 768 / WXGA
130
200
2.9
27 cm (10.6-inch)
1280 x 768 / WXGA
150
300
2.8
28 cm (11.1-inch)
1366 x 768 / WXGA
146
240
3.7
31 cm (12.1-inch)
1280 x 800 / WXGA
183
300
3.5
34 cm (13.3-inch)
1280 x 800 / WXGA
225
300
4.0
Pricing and Availability
The new 10.4-inch and 10.6-inch LCD displays are available now from TAEC. Pricing in sample quantities is $350 each for both models.
RoHS-Compatible Displays

The RoHS Directive restricts the use of cadmium, hexavalent chromium, lead, mercury, polybrominated biphenyl (PBB), and polybrominated diphenyl ether (PBDE) in a wide range of electrical and electronic products as of July 2006, in the European Union. In addition, China , California , and several other U.S. states have passed regulations with similar phase-outs of these substances in certain electrical and electronic products. Initially, LCDs with cold cathode fluorescent lamp (CCFL) backlight systems must contain less than 5mg of mercury per lamp, under one of the exemptions listed in the Annex to the RoHS Directive.4 TMD is committed to offering a broad selection of RoHS-Compatible displays, and will continue to develop products intended to meet various global environmental regulations. During a transition period, TMD will supply its original non-RoHS-Compatible modules to existing customers as demand warrants.

*About TAEC

Combining quality and flexibility with design engineering expertise, TAEC brings a breadth of advanced, next-generation technologies to its customers. This broad offering includes semiconductors, flash memory-based storage solutions, and displays for the computing, wireless, networking, automotive and digital consumer markets

TAEC is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corp. (Toshiba), Japan 's second largest semiconductor manufacturer and the world's ninth largest integrated manufacturer of electric and electronic equipment. In more than 130 years of operation, Toshiba has recorded numerous firsts and made many valuable contributions to technology and society. For additional company and product information, please visit TAEC's website at chips.toshiba.com.  For technical inquiries, please e-mail Tech.Questions@taec.toshiba.com.

**About Toshiba Matsushita Display Technology Co., Ltd
In April 2002, Toshiba Corporation and Matsushita Electric Industrial Co., Ltd. merged their LCD businesses into a new joint venture company, Toshiba Matsushita Display Technology Co., Ltd, now known as TMDisplay. The new company brings together each company's strengths and capabilities in LCD technology to satisfy a broad range of customer requirements and market segments. Today, Toshiba Matsushita Display Technology Co., Ltd. is a worldwide leader in the field of TFT LCD modules for mobile use. For further information, please visit the TMD home page at http://www.tmdisplay.com/tm_dsp/index.htm.

1 Mercury-Free: Toshiba Matsushita Display Technology Co. Ltd. defines “Mercury-Free” products as those containing no more than a maximum concentration value of 0.1 percent mercury(Hg) by weight in Homogeneous Materials 3 . This does not mean that Mercury-Free products are entirely free of mercury(Hg).

2 RoHS-Compatible – Toshiba Matsushita Display Technology Co. Ltd. defines “RoHS-Compatible” LCD products as products that either (i) contain no more than a maximum concentration value of 0.1% by weight in Homogeneous Materials 3 for lead, mercury, hexavalent chromium, polybrominated biphenyls (PBBs), and polybrominated diphenyl ethers (PBDEs) and no more than 0.01% by weight in Homogeneous Materials for cadmium, or (ii) fall within one of the stated exemptions set forth in the Annex to the RoHS Directive4.

3 Homogeneous Materials – Toshiba Matsushita Display Technology Co. Ltd. defines “Homogeneous Materials” to mean a material that cannot be mechanically disjointed into different materials. The term “homogeneous” is understood as “of uniform composition throughout,” so examples of “Homogeneous Materials” would be individual types of plastics, ceramics, glass, metals, alloys, paper, board, resins and coatings. Toshiba Matsushita Display Technology Co., Ltd. defines the term “mechanically disjointed” to mean that the materials can, in principle, be separated by mechanical actions such as unscrewing, cutting, crushing, grinding or abrasive processes.

4 RoHS Directive – Toshiba Matsushita Display Technology Co. Ltd. defines the “RoHS Directive” as the Directive 2002/95/EC of the European Parliament and of the Council of 27 January 2003 on the restriction of the use of certain hazardous substances in electrical and electronic equipment.

Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice. Technical and application information contained here is subject to the most recent applicable Toshiba product specifications. In developing designs, please ensure that Toshiba products are used within specified operating ranges as set forth in the most recent Toshiba product specifications and the information set forth in Toshiba’s "Handling Guide for Semiconductor Devices," or "Toshiba Semiconductor Reliability Handbook." This information is available at chips.toshiba.com or from your TAEC representative.

All trademarks and tradenames held within are the properties of their respective holders.

Legal Note. These definitions are not intended to interpret the RoHS Directive and/or any other applicable law or regulation and do not constitute legal advice. The RoHS Directive itself and/or any other applicable law or regulation should always be read and understood (as they constitute the law), in contrast with the information contained herein, which is intended to be informative but has no legal authority. You should refer to the RoHS Directive itself and/or any other applicable law or regulation for a full statement of the legal requirements and in the case of any doubt take independent advice, including your own legal advice. The RoHS Directive itself and/or any other applicable law or regulation may be revised from time to time, so users should take care to keep themselves informed.

 
LCDB 07 468