|
| |
| TOSHIBA AMERICA ELECTRONIC COMPONENTS
TO SHOWCASE ADVANCED LCD AND OLED PRODUCTS AND TECHNOLOGIES
AT SID 2007 |
| Innovative Display Products and Prototypes
for Mobile Phones and Portable Electronics, Automotive, Mobile
Computing, and Industrial Markets to be Featured |
 |
| IRVINE, Calif., May 22, 2007 — Toshiba America Electronic Components, Inc. (TAEC)* will demonstrate an extensive array of next-generation displays and display technologies developed by Toshiba Matsushita Display Technology Co., Ltd. (TMD)** for mobile phone and portable electronics, automotive, mobile computing, and industrial markets in booth #1149 at the 2007 Society for Information Display (SID) International Symposium, Seminar & Exhibition in Long Beach, CA, May 22 to 24, 2007.
Featured technologies in TAEC’s booth this year include optically compensated bend (OCB), low temperature poly-silicon (LTPS), System-on-Glass (SOG), and Organic Light-Emitting Diode (OLED) displays.
|
 |
| OCB
Technology |
- TMD’s latest 32-inch OCB LTPS thin-film transistor (TFT) active-matrix LCD features 1,000,000:1 contrast ratio, an ultra-fast 2.0ms Motion Picture Response Time (MPRT) and ultra-wide viewing angles (to 176 degrees) in all directions, surpassing cathode ray tube (CRT) front-of-screen performance1. For comparison, the 32-inch OCB panel will be shown adjacent to a 32-inch CRT TV.
- A 12.1-inch SVGA (800 x 600) OCB LCD that also features 1,000,000:1 contrast ratio, ultra-fast 2.0ms response time, and ultra-wide 176-degree viewing angles in all directions will be displayed side-by-side with a conventional twisted nematic (TN) mode LCD to show the improvement in motion picture legibility that is possible with OCB technology, as well as the ultra-wide viewing angles and fast response time that enable OCB displays to provide image quality superior to conventional TN mode LCDs2.
- Two 9.0-inch WVGA (800 x 480) LCD displays, one in OCB mode and the other in conventional TN mode, will be shown operating at -20oC to demonstrate the benefits of OCB’s fast response time, even at the extreme temperatures that can be encountered in automotive video and navigation applications.
- A 4.3-inch prototype WQVGA (480 x 272) display combines OCB liquid crystal technology, which offers both a wide viewing angle and a fast response time, and transflective technology, which assures high viewability both indoors and outdoors. The development of this combination is a first in the LCD industry. The module features very high brightness for a transflective module of 400 candelas per sq. meter (cd/m2), with 2.4ms response time in reflective mode and 5.3ms response time in transmissive mode. The innovative panel is targeted for use in portable media players and will be displayed in the Mobile section of the booth.
- A 4.13-inch prototype high-resolution transmissive WVGA (800 x 480) OCB module will also be shown in the Mobile section. Like the ultra-high contrast 32- and 12.1-inch modules noted above, this LTPS module features 1,000,000:1 contrast ratio, 2.0ms ultra-fast MPRT response time and 176-degree ultra-wide viewing angles in all directions. The improvement in contrast ratio was achieved by optimizing the backlight performance relative to the display image, to obtain deeper blacks, thus increasing contrast and visual depth perception.
|
 |
| System-on-Glass
Technology |
| To demonstrate
the potential that TMD’s LTPS SOG technology offers
for integration of additional functions and circuitry,
two prototypes will be shown that integrate input functionality
into the substrate glass. This enables brighter, more
vivid images by eliminating an external touch panel,
which typically degrades optical performance. In addition,
the reduction in number of components and connections
enhances reliability and contributes to a thinner, lighter
weight design. |
- A switchable-mode, finger-shadow-sensing or light-pen-sensing input 2.8-inch WQVGA (240 X 400) LCD panel will be featured in the booth. It operates across a significantly increased range of ambient light intensities compared to previous generation SOG input displays. Booth visitors will be encouraged to test the display, which supports input to the LCD screen by directly touching an icon or button on the LCD screen with a finger, or by directly writing onto the LCD screen with a light pen. The finger-shadow-sensing technology could be used in a touch panel application, while the light-pen-sensing technology could provide functionality similar to today’s digitizer applications.
- A second 2.8-inch WQVGA (240 x 400) finger-sensing input display, which can sense input without external devices, will be the subject of a conference presentation and will be shown in the booth. This input display operates in any ambient lighting condition by recognizing a finger’s reflection from an internal backlight when in dark lighting conditions, and recognizes a finger’s shadow from ambient lighting when in outdoor lighting conditions. Advanced performance compared to earlier input display prototypes was achieved through improved high-speed driving circuitry, increased sensitivity of the photo sensors embedded in the glass substrate, and more sophisticated signal processing.
- In addition, three highly integrated mobile phone displays, including 2.2- and 2.4-inch QVGA (240 x 320) modules and a 2.6-inch WQVGA (240 x 400) prototype module will be exhibited. They each achieve improved durability and reliability through integration of analog circuits (D-A converter and amplifier), driving and power supply circuits, and an integrated control circuit, thus reducing external components, simplifying the assembly process, and contributing to reduced weight.
|
 |
| OLED
Technology |
| TMD is demonstrating
the excellent color reproduction and true black performance
of its new top-emission OLED technology with a 2.8-inch
WQVGA (240 x 400) active matrix module with an ultra-fast
response time of less than 1.0msec, high brightness of
400cd/m2 and color gamut greater than 90 percent. Top-emission
OLEDs emit light away from the substrate to achieve higher
brightness with lower power consumption, compared to
bottom-emission OLEDs, thereby extending the life of
the panel. An OLED panel reproduces images from light
emitted by the fine organic electroluminescent film formed
on the glass substrate, thus it can provide high-contrast,
clear images with ultra-fast response time for remarkable
moving picture performance. In addition, the OLED panel
features an ultra-wide viewing angle, and is thinner
and lighter than an LCD, since no backlighting system
is required. |
 |
| New Displays |
| In addition
to the technology demonstrations noted above, a diverse
line-up of commercially available displays and prototypes
for mobile phones and portable electronics, mobile computing,
industrial and automotive applications will also be featured. |
 |
| Mobile
Phones/Portable Electronics: TMD’s broad line of displays for mobile
phones, handheld GPS, portable media players and more
will be represented by 2.4- and 2.6-inch QVGA (240 x
320), 2.8-inch wide WQVGA (240 x 400), and 3.0-inch WVGA
(800 x 480) LTPS TFT LCD modules. The 2.4-, 2.6- and
2.8-inch prototype modules incorporate thin glass and
are only 0.99mm thick, including the backlight, to enable
even thinner and lighter weight mobile phones. The high-resolution
3.0-inch WVGA display features five times the number
of pixels as available in the QVGA format, and a pixel
density of 313 pixels per inch to support greater information
content and superior image quality for web and mapping
applications. |
 |
| Automotive: Displays for automotive entertainment and navigation
applications will be featured, including a 15-inch class
ultra-wide 1280 x 390 concept display for instrument
clusters that can switch among multiple views as required,
such as speedometer and tachometer, navigation guides,
meters and gauges, and from rear-view camera systems.
In addition, representative technology prototypes from
TMD’s extensive product line-up of 5.8- to 9.0-inch
modules for both automotive entertainment and navigation
applications will be showcased. One noteworthy prototype
is an 8.0-inch WVGA (800x480) color active-matrix automotive
display for navigation applications that uses a new LED
backlight, instead of the conventional cold cathode fluorescent
lamp (CCFL) backlight system, to achieve color gamut
performance of approximately 90 percent. The high-resolution
WVGA format provides excellent image quality for video
and/or mapping applications, while the LED backlight
enables quick start-up at low temperatures typically
required in automotive applications. In addition to the 8.0-inch WVGA display, a 7.0-inch WVGA (800 x 480) display featuring a wide viewing angle, "normally black" display mode and LED backlight system will also be shown. |
 |
| Mobile
Computing: TMD’s recently expanded (March 20, 2007) series
of notebook PC LCD displays feature a thin, lightweight
structure achieved through poly-silicon technology, glass
thinning and LED backlighting. Combining 0.3mm or thinner
glass and LED backlighting in LTPS-based TFT LCD modules
enables and enhances even higher portability in the mobile
PC segment of the marketplace. An 8.9-inch WXGA (1280
x 768) transflective mobile PC module with 0.3mm glass
provides excellent image quality in a variety of ambient
lighting conditions. In addition, a 12.1-inch module
with 0.2mm glass, and a 13.3-inch module with 0.3mm glass,
both in wide-format WXGA (1280 x 800) resolution, will
represent TMD’s diverse line-up of ultra-lightweight
transmissive TFT LCD panels. Mobile PCs from leading
manufacturers demonstrate various TMD display modules
in commercially available notebook applications, including
a 14.1-inch SXGA+ (1400 x 1050) notebook, as well as
wide-format models featuring the 8.9-inch, 12.1-inch
and 13.3-inch WXGA displays described above. |
 |
| Industrial: Featured LCD modules for the industrial market range
from a 3.5-inch QVGA (320 x 240) display with replaceable
LED backlight to a very high brightness, 1000cd/m2, 12.1-inch
SVGA (800 x 600) module with improved viewability for
vending machines, ticket dispensers, or other equipment
installed outdoors. Additional new industrial-use modules
at SID include a 5.7-inch QVGA (320 x 240) module with
enhanced resolution and replaceable LED backlight for
use in measuring instruments and handheld computing devices;
high-brightness 10.4-inch and lightweight 8.4-inch modules
to expand TMD’s popular SVGA line; and a new 7.0-inch
module to expand TMD’s WVGA (800 x 480) wide-screen
lineup. Each of the new LCD modules has been designed
so that it could be equipped with an optional resistive
touch panel. (See separate announcement dated May 9,
2007.) Additional modules on display from TMD’s
broad industrial line include an 8.5-inch WVGA (800 x
400) module ideally suited for use in multi-function
printers, and a 5.0-inch WQVGA (400 x 234) AV panel with
analog video interface and LED backlighting. |
|
 |
| *About
TAEC |
| Combining quality
and flexibility with design engineering expertise, TAEC
brings a breadth of advanced, next-generation technologies
to its customers. This broad offering includes memory
and flash memory-based storage solutions, a broad range
of discrete devices, displays, medical tubes, ASICs,
custom SOCs, microprocessors, microcontrollers and wireless
components for the computing, wireless, networking, automotive
and digital consumer markets. TAEC is an independent
operating company owned by Toshiba America, Inc., a subsidiary
of Toshiba Corp. (Toshiba), Japan’s largest semiconductor
manufacturer and the world’s fourth largest semiconductor
manufacturer. In more than 130 years of operation, Toshiba
has recorded numerous firsts and made many valuable contributions
to technology and society. For additional company and
product information, please visit TAEC’s website
at chips.toshiba.com. For
technical inquiries, please e-mail Tech.Questions@taec.toshiba.com. |
|
 |
| **About Toshiba Matsushita Display
Technology Co., Ltd |
| In April 2002, Toshiba Corporation
and Matsushita Electric Industrial Co., Ltd. merged their LCD
businesses into a new joint venture company, Toshiba Matsushita
Display Technology Co., Ltd, now known as TMDisplay. The new
company brings together each company's strengths and capabilities
in LCD technology to satisfy a broad range of customer requirements
and market segments. Today, Toshiba Matsushita Display Technology
Co., Ltd. is a worldwide leader in the field of TFT LCD modules
for mobile use. For further information, please visit the TMD
home page at http://www.tmdisplay.com/tm_dsp/index.htm. |
| |
 |
| Information in this press release,
including product pricing and specifications, content
of services and contact information, is current and believed
to be accurate on the date of the announcement, but is
subject to change without prior notice. Technical and
application information contained here is subject to
the most recent applicable Toshiba product specifications.
In developing designs, please ensure that Toshiba products
are used within specified operating ranges as set forth
in the most recent Toshiba product specifications and
the information set forth in Toshiba’s "Handling
Guide for Semiconductor Devices," or "Toshiba
Semiconductor Reliability Handbook." This information
is available at chips.toshiba.com or
from your TAEC representative. |
|
| |
| LCDB 07 474 |
 |
|
|