|
| |
| TOSHIBA LAUNCHES LARGEST DENSITY EMBEDDED NAND FLASH MEMORY DEVICES |
| eMMC and eSD Embedded Memories Combine Up To 32GB NAND and Controller in a
Single Package
|
 |
|
IRVINE,
Calif., and TOKYO, August 7, 2008 — Toshiba Corp. (Toshiba) and Toshiba America Electronic Components, Inc. (TAEC)*, its subsidiary in the Americas, today announced the launch of 32GB1 embedded NAND flash memory devices that offer the largest density yet announced2 plus full compliance with the eMMC™ and eSD™ standards. The embedded devices are designed for application in digital consumer products, including mobile phones, video cameras, HDTV, personal navigation devices, POS terminals, printers, and set-top boxes. Samples will be available in September 2008, and mass production will start in the fourth quarter.
The new 32GB embedded devices combine eight 32Gbit (= 4GB) NAND chips fabricated with Toshiba's cutting-edge 43nm process technology and also integrate a dedicated controller. Full compliance with
JEDEC/MMCA Ver. 4.3 and SDA Ver. 2.0 high-speed memory standards for memory cards as defined by the MultiMediaCard Association and SD Card Association, respectively, supports standard interfacing and simplified embedding in products, reducing development burdens on product manufacturers.
Toshiba offers a line-up of single-package embedded NAND Flash memories which include a controller to manage basic control functions for NAND applications: LBA-NAND™ memory, which has a NAND interface; eSD large capacity chips with SD interface; and e MMC with an HS-MMC interface. This comprehensive line-up, available in densities ranging from 1GB to 32GB, supports applications in a very wide range of products.
There is growing demand for memories with a controller function that minimizes development requirements and eases integration into system designs. Toshiba has already taken steps to secure leadership in this expanding market, and the addition of higher density modules will reinforce the company's position. |
|
 |
New Product Lineup:
eMMC |
| Product Number |
Capacity |
Package |
Sample Shipment |
Mass Production |
Production Scale |
| THGBM1G8D8EBAI2 |
32GB |
169Ball FBGA
14x18x1.4mm |
Oct., 08 |
4Q, 08
(Oct.~Dec.) |
1 million/ month
(Total) |
| THGBM1G7D8EBAI0 |
16GB |
169Ball FBGA
12x18x1.4mm |
Sept., 08 |
4Q, 08
(Oct.~Dec.) |
| THGBM1G7D4EBAI2 |
16GB |
169Ball FBGA
14x18x1.4mm |
4Q, 08
(Oct.~Dec.) |
4Q, 08
(Oct.~Dec.) |
| THGBM1G6D4EBAI4 |
8GB |
169Ball FBGA
12x18x1.3mm |
Sept., 08 |
4Q, 08
(Oct.~Dec.) |
| THGBM1G5D2EBAI7 |
4GB |
169Ball FBGA
12x16x1.3mm |
Sept., 08 |
4Q, 08
(Oct.~Dec.) |
| THGBM1G4D1EBAI7 |
2GB |
169Ball FBGA
12x16x1.3mm |
4Q, 08
(Oct.~Dec.) |
1Q, 09
(Jan. –Mar.) |
| THGBM1G3D1EBAI8 |
1GB |
169Ball FBGA
11.5x13x1.2mm |
4Q, 08
(Oct.~Dec.) |
1Q, 09
(Jan. –Mar.) |
|
|
 |
| eSD |
| Product Number |
Capacity |
Package |
Sample Shipment |
Mass Production |
Production Scale |
| THGVS4G8D8EBAI2 |
32GB |
169Ball FBGA
14x18x1.4mm |
Sept., 08 |
4Q, 08
(Oct.~Dec.) |
500K/ month
(Total) |
| THGVS4G7D8EBAI0 |
16GB |
169Ball FBGA
12x18x1.4mm |
Sept., 08 |
4Q, 08
(Oct.~Dec.) |
| THGVS4G7D4EBAI2 |
16GB |
169Ball FBGA
14x18x1.4mm |
4Q, 08
(Oct.~Dec.) |
4Q, 08
(Oct.~Dec.) |
| THGVS4G6D4EBAI4 |
8GB |
169Ball FBGA
12x18x1.3mm |
Sept., 08 |
4Q, 08
(Oct.~Dec.) |
| THGVS4G5D2EBAI4 |
4GB |
169Ball FBGA
12x18x1.3mm |
4Q, 08
(Oct.~Dec.) |
4Q, 08
(Oct.~Dec.) |
| THGVS4G4D1EBAI4 |
2GB |
169Ball FBGA
12x18x1.3mm |
4Q, 08
(Oct.~Dec.) |
1Q, 09
(Jan. –Mar.) |
| THGVS4G3D1EBAI8 |
1GB |
169Ball FBGA
11.5x13x1.2mm |
1Q, 09
(Jan. –Mar.) |
1Q, 09
(Jan. –Mar.) |
|
|
|
 |
| Key Features |
- The integrated controller, compliant with
JEDEC/MMCA Ver. 4.3 and SDA Ver. 2.0, handles essential functions, including writing block management, error correction (ECC) and driver software. It simplifies system development, allowing manufacturers to minimize development costs and to improve time to market for new and upgraded products.
- A wide product line-up supports capacities from 1 to 32GB. The high-capacity 32GB device can record up to 560 hours of data at a bit rate of 128Kbps3 and can record4 hours of full spec high definition video and 7.3 hours of standard definition video 4.
- The 32GB device stacks eight 32Gbit (=4GB) chips fabricated with leading-edge 43nm process technology.

SEM Photograph of 32GB device structure
|
 |
| Specifications eMMC |
| Interface |
JEDEC/MMCA Ver. 4.3 standard HS-MMC interface |
| Power Supply Voltage |
2.7 to 3.6V(memory core)/ 1.7V to 1.95V (interface) |
| Bus width |
x1 / x4 / x8 |
| Writing Speed |
Target 10 MB per sec/ minimum (Sequential Mode)
Target 18 MB per sec/ minimum (Sequential/Interleave Mode)** |
| Reading Speed |
Target 20 MB per sec/minimum (Sequential Mode) |
| Temperature |
-25 degrees to +85 degrees Celsius |
| Package |
153Ball FBGA (+16 support Ball) |
|
|
 |
| Specifications eSD |
| Interface |
SDA Ver. 2.0 standard SD interface |
| Power Supply Voltage |
2.7 to 3.6V |
| Bus width |
x1 / x4 |
| Writing Speed |
SDA Standard Class 4 |
| Reading Speed |
SDA standard Class 4 |
| Temperature |
-25 degrees to +85 degrees Celsius |
| Package |
153Ball FBGA (+16 support Ball) |
|
 |
| *About Toshiba Corp. and
TAEC |
| Through proven commitment, lasting relationships and advanced, reliable electronic components, Toshiba enables its customers to create market-leading designs. Toshiba is the heartbeat within product breakthroughs from OEMs, ODMs, CMs, distributions and fabless chip companies worldwide. A committed electronic components leader, Toshiba designs and manufactures high-quality flash memory-based storage solutions, discrete devices, displays, advanced materials, medical tubes, custom SoCs/ASICs, digital multimedia and imaging products, microcontrollers and wireless components that make possible today's leading cell phones, MP3 players, cameras, medical devices, automotive electronics and more.
Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation, Japan 's largest semiconductor manufacturer and the world's third largest semiconductor manufacturer ( Gartner, 2007 WW Semiconductor Revenue, April 2008). For additional company and product information, please visit http://www.toshiba.com/taec/. |
|
| |
 |
| Information in this press release,
including product pricing and specifications, content
of services and contact information, is current and believed
to be accurate on the date of the announcement, but is
subject to change without prior notice. Technical and
application information contained here is subject to
the most recent applicable Toshiba product specifications.
In developing designs, please ensure that Toshiba products
are used within specified operating ranges as set forth
in the most recent Toshiba product specifications and
the information set forth in Toshiba’s "Handling
Guide for Semiconductor Devices," or "Toshiba
Semiconductor Reliability Handbook." This information
is available at chips.toshiba.com or
from your TAEC representative.
eMMC is a trademark of the MultiMediaCard Association. LBA-NAND and eSD are trademarks of TOSHIBA Corporation All other trademarks and tradenames held within are the properties of their respective holders. |
|
| |
| MEMY 08 536 |
 |
|
|