Toshiba  
 News/Media Resources | Photo Gallery  
Print This Page   Close Window
 
Toshiba Introduces Super Speed USB 3.0-Compliant USB Flash Memory
Transfer Rate 22 Times Faster than Previous Models
Osumi 64GB
Download Larger Image (JPG 188KB)

LAS Vegas, NV, January 9, 2012— This week at International CES 2012, Toshiba America Electronic Components, Inc. (TAEC)*, will be demonstrating the latest additions to its lineup of flash memory offerings - the TransMemory-EX™ series of USB flash memory products. The new drives are compliant with the new USB 3.0 standards - known as Super Speed USB*1 . Initial storage capacities include a 32GB model and a 64GB model.

Utilizing Toshiba's Double Data Rate (DDR) NAND , the new products offer maximum data transfer rates of 220 MB/sec*4 for reading and 94 MB/sec for writing*2 - or 22 times and 18 times faster transfer rates, respectively, when compared with Toshiba's previous models*3 . Additionally, Toshiba achieved this level of performance with low power consumption of 300 mA or less - one of the lowest in the industry. Toshiba's new drives are fully backward-compatible with the USB 2.0 standard.

The new products can transfer 25GB of video content in approximately five minutes*5 , which would take the previous model about 30 minutes. The new devices meet user needs for portability of video content and other large data and for high-speed data transfer between digital products. "Today's consumers have a need for speed, and they want a truly interactive experience," noted Brian Kumagai, senior business development manager, NAND flash memory products for TAEC. "Devices and peripherals are becoming faster and faster, and the USB transfer speed needs to increase in order to keep up. Eventually, all motherboards and laptops will be designed with USB 3.0 ports, allowing for consumers to take advantage of the increased speed and improved performance it offers."

In order to meet the needs of consumers looking for faster transfer rates and higher capacities, Toshiba will continue to promote innovations that widen the horizons of the NAND flash market and support the company's continued leadership in that market - including the introduction of new USB flash drives and memory cards.

Key Features:
  1. Compliant with the USB 3.0 Super Speed USB standard
    Compliant with the USB 3.0 Super Speed USB standard established in 2008, maximum transfer rates of 220 MB/sec for reading and 94 MB/sec for writing are achieved. Also connectable to computers equipped with USB 2.0 hosts, maximum transfer rates of 34 MB/sec for reading and 30 MB/sec for writing are achieved.
  2. One of the lowest power consumptions in the industry
    Low power consumption is achieved thanks to Toshiba's original technology, such as multi-layering of high-speed NAND flash memory and a dedicated low-power-consumption ASIC controller. As a result, power consumption of notebook PCs is minimized even when using a USB flash memory.
  3. Windows® ReadyBoost® capability
    The new products support Windows ReadyBoost that allows use of external memory storage as a cache for a hard disk drive of a PC. Windows ReadyBoost capability contributes to enhanced PC performance, such as reduced time required for starting up PC software. This function is available for computers incorporating Windows® 7 or Vista.
  4. Toshiba's original security software
    The new products incorporate application software that allows protection of a particular block with a password lock so that data and files stored in that block cannot be accessed without the password.
Main Specifications:
Product Name TransMemory-EX™
Capacity 64GB 32GB
ReadyBoost ® Function Available for computers incorporating Windows®7 or Vista
Interface USB 1.1/ Hi Speed USB 2.0 *, Super Speed USB 3.0 *
Power Supply Voltage Powered through USB port
Exterior Dimensions 68.8 (L) × 21 (W) × 10.5 (H) mm
Weight Approx. 14 g (main unit only)
Operating Environment Operating temperature: 0-50°C
Storage temperature: -20-60° C
Operating and storage humidity: 5-95 %RH (no condensation)
Compatible Devices

Computers with USB Interface (A type) and equipped with one of the following operating systems:

  • Windows®7
  • Windows®XP
  • Windows®Vista
  • Mac OS 10.0.2 or later (Only support USB 2.0)

* The terms USB 1.1/ Hi Speed USB 2.0 and Super Speed USB 3.0 used herein are the names of specifications upon which these products are based; they do not guarantee the speed of their operation.
* TransMemory-EX™ and TransMemory™ are trademarks of Toshiba Corporation.
* Specifications are subject to change.

*About Toshiba Corp. and TAEC

Through proven commitment, lasting relationships and advanced, reliable electronic components, Toshiba enables its customers to create market-leading designs. Toshiba is the heartbeat within product breakthroughs from OEMs, ODMs, CMs, VARs, distributors and fabless chip companies worldwide. A committed electronic components leader, Toshiba designs and manufactures high-quality flash memory-based storage solutions, solid state drives (SSDs), hard disk drives (HDDs), discrete devices, LCD displays, advanced materials, medical tubes, custom SoCs/ASICs, imaging products, microcontrollers and wireless components that make possible today's leading cell phones, MP3 players, cameras, medical devices, automotive electronics, enterprise solutions and more.

Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation, Japan's largest semiconductor manufacturer and the world's third largest semiconductor manufacturer (Gartner, 2010 WW Semiconductor Revenue, April 2011). Toshiba was founded in 1875 and today has over 490 subsidiaries and affiliates, with 203,000 employees worldwide and annual sales of $77 billion. Visit Toshiba's web site at www.toshiba.co.jp/index.htm.

For additional company and product information, please visit http://www.toshiba.com/taec/.

1 USB 3.0 (Super Speed USB) is a new standard established in 2008 by USB Implementers Forum.

2 Maximum data transfer rates for reading and writing were verified in Toshiba's PC testing environment.

3 Maximum transfer rates of the previous TransMemory model compliant with the USB 2.0 standard are 10 MB/sec for reading and 5 MB/sec for writing.

4In the case of a model with maximum transfer rates of 220 MB/sec for reading and 94 MB/sec for writing. As of January 09, 2011. Survey by Toshiba.

5 The data for full HD video (1920 x 1080, 16:9) verified in Toshiba's PC testing environment

6 Product density is identified based on the maximum density of memory chip(s) within the Product, not the amount of memory capacity available for data storage by the end user. Consumer-usable capacity will be less due to overhead data areas, formatting, bad blocks, and other constraints, and may also vary based on the host device and application.

Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice. Technical and application information contained here is subject to the most recent applicable Toshiba product specifications. In developing designs, please ensure that Toshiba products are used within specified operating ranges as set forth in the most recent Toshiba product specifications and the information set forth in Toshiba'’s "Handling Guide for Semiconductor Devices," or "Toshiba Semiconductor Reliability Handbook." This information is available at www.chips.toshiba.com, or from your TAEC representative.

 
MEMY 12 626