Toshiba  
 News/Media Resources | Photo Gallery  
Print This Page   Close Window
 
Toshiba Introduces New Line of Photocouplers
Provide Guaranteed Performance at Temperatures up to 125 Degrees Celsius

IRVINE, Calif., Nov. 15, 2012 Toshiba America Electronic Components, Inc., (TAEC)*, a committed leader that collaborates with technology companies to create breakthrough designs, has announced the addition of the TLP350H and TLP352 to its family of photocouplers. The new photocouplers utilize a new long-life LED for a guaranteed operating temperature of up to 125°C . The Toshiba TLP350H and TLP352 consist of a GaAIAs infrared light-emitting diode (LED) optically coupled to an integrated high-gain, high-speed photodetector IC chip.

Toshiba's TLP350H is a DIP8-package IC coupler that can directly drive a small to medium capacity IGBT and power MOSFET. This product is suitable for use in home appliances or devices that are required to operate in high temperature environments, including PV converters for solar applications, consumer applications including refrigeration and air conditioning, and factory automation applications such as motion control. Recently, there has been an increased use of bootstrap power supplies to drive photocouplers in order to achieve simplified design, thus increasing demand for lower current consumption in photocouplers. With a power supply current of 3.0 mA (maximum), the TLP350H offers the best power consumption in the industry.

Housed in a DIP8-package, the TLP352 can directly drive a middle-capacity IGBT or power MOSFET, and helps reduce dead time and improve efficiency in inverter circuits. Toshiba's TLP352 can be used in a wide range of products, including industrial devices used in environments of severe heat, home photo voltaic power systems, digital home appliances, measurement devices, and control devices.

According to Joseph Tso, business development manager for Toshiba's optoelectronics discrete business unit , "We designed this new family of chips to withstand extreme temperatures in order to meet the needs of a wide variety of applications, and give customers a high efficiency end product."

Features include:
  • Wide guaranteed operating temperature range: Topr = -40ºC to 125ºC
  • Totem pole output
  • Peak output current: IOP = ±2.5A (Max.)
  • Power supply current: ICC = 3mA (Max.)
  • Low threshold input current: IFLH = 5mA (Max.)
  • Withstand voltage: BVs = 3750Vrms
  • Transmission delay time (TLP350H): tpLH, tpHL = 500ns (Max.)
  • Transmission delay time (TLP352): tpLH,tpHL=200ns (max.)
  • Transmission delay time difference between products (PDD) (TLP352):= ±80ns (Max.)
Availability

The Toshiba TLP350H and TLP352 are available now. For datasheets, samples and pricing, please contact your Toshiba representative.

*About Toshiba Corp. and TAEC

Through proven commitment, lasting relationships and advanced, reliable electronic components, Toshiba enables its customers to create market-leading designs. Toshiba is the heartbeat within product breakthroughs from OEMs, ODMs, CMs, VARs, distributors and fabless chip companies worldwide. A committed electronic components leader, Toshiba designs and manufactures high-quality flash memory-based storage solutions, solid state drives (SSDs), hard disk drives (HDDs), discrete devices, advanced materials, medical tubes, custom SoCs/ASICs, imaging products, microcontrollers and wireless components that make possible today's leading smartphones, tablets, MP3 players, cameras, medical devices, automotive electronics, enterprise solutions and more.

Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation, Japan's largest semiconductor manufacturer and the world's third largest semiconductor manufacturer (Gartner, 2011 Worldwide Semiconductor Revenue, March, 2012). Toshiba Corporation was founded in 1875 and today has over 554 subsidiaries and affiliates, with 210,000 employees worldwide. Visit Toshiba's web site at www.toshiba.co.jp/index.htm.

 

© 2012 Toshiba America Electronic Components, Inc. All rights reserved.
Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice. Technical and application information contained here is subject to the most recent applicable Toshiba product specifications.

 

Editors Note: Reader inquiries please publish: Tech.Questions@taec.toshiba.com.

Photos available for download at Photo Gallery http://www.toshiba.com/taec/news/media_resources/news_mr_gallery.jsp

 
OPTO 12 652