News/Media Resources | Photo Gallery  
Print This Page   Close Window
Toshiba Extends Family of 650V SiC Power Devices
6, 8 and 10A Devices Added to Silicon Carbide Schottky Barrier Diode Range

IRVINE, Calif., Oct. 24, 2013 Toshiba America Electronic Components, (TAEC)*, a committed leader that collaborates with technology companies to create breakthrough designs, today announced that it has extended its family of 650V silicon carbide (SiC) Schottky Barrier Diodes (SBD). The TRS6E65C, TRS8E65C and TRS10E65C are 6, 8, and 10A devices, respectively. These SBDs join Toshiba’s 12A device, the TRS12E65C, which entered volume production in 2Q 2013. With analysts predicting significant growth in the SiC power device market, Toshiba is expanding its SBD line-up to meet an anticipated spike in demand.

Part Number VRRM(V) IF (A) Electric Specifications Package


typ. / max
typ. / max
TRS6E65C 650 6 1.5 / 1.7 0.3 / 90

TO-220 (2pin)

TO-220 (2pin)

TRS8E65C 650 8 1.5 / 1.7 0.4 / 90
TRS10E65C 650 10 1.5 / 1.7 0.42 / 90
TRS12E65C 650 12 1.5 / 1.7 0.45 / 90

Low forward voltage drop and a very fast switching action make SBDs well-suited to applications including power conditioners for photovoltaic power generation systems, solar inverters, uninterruptible power supplies and DC-DC converters. SBDs can also act as replacements for silicon diodes in switching power supplies, where they are much more efficient.

SiC power devices offer more stable operation than current silicon devices - even at high voltages and currents - as they significantly reduce heat dissipation during operation. They meet diverse industry needs for smaller, more effective communications devices and suit industrial applications ranging from servers to inverters and trains to automotive systems.

The Toshiba SBD range features a maximum reverse recovery current (IRRM ) of 90µA @ 650V. All devices are housed in TO-220 packages, with additional packages scheduled to be added at a future date.

Pricing and Availability

Toshiba's new 650v SBDs are available now. Budgetary pricing begins at $3.00(6A device) with volume discounts available.

*About Toshiba Corp. and TAEC

Through proven commitment, lasting relationships and advanced, reliable electronic components, Toshiba enables its customers to create market-leading designs.  Toshiba is the heartbeat within product breakthroughs from OEMs, ODMs, CMs, VARs, distributors and fabless chip companies worldwide.  A committed electronic components leader, Toshiba designs and manufactures high-quality flash memory-based storage solutions, solid state drives (SSDs), hard disk drives (HDDs), discrete devices, advanced materials, medical tubes, custom SoCs/ASICs, imaging products, microcontrollers and wireless components that make possible today's leading smartphones, tablets, cameras, medical devices, automotive electronics, enterprise solutions and more.

Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation, Japan's largest semiconductor manufacturer and the world's fifth largest semiconductor manufacturer (Gartner, 2012 Worldwide Semiconductor Revenue, April, 2013). Toshiba Corporation was founded in 1875 and today has over 554 subsidiaries and affiliates, with 210,000 employees worldwide. Visit Toshiba's web site at


Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice. Technical and application information contained here is subject to the most recent applicable Toshiba product specifications.

POWR 13 691