United States
Toshiba USA   Toshiba Americas   Toshiba Worldwide
Enter Search Term
Stock Check
Home  News  2014 Press Releases


New High-Current Photorelay from Toshiba Suited for Testing, Control Applications

Enhances Performance; Reduces Mounting Area

IRVINE, Calif., April 29, 2014 Toshiba America Electronic Components, Inc., (TAEC)*, a committed leader that collaborates with technology companies to create breakthrough designs, today announced a new small package size, high-current (3.3A max.) photorelay - the TLP3107. Housed in a small 2.54SOP6 package, the low on-state resistance and high permissible on-state current of the TLP3107 make it suited to testing applications, including power-line switching, feedback resistance switching and measuring-line switching.

Photorelays provide design engineers with fast switching speed, high reliability, lower power consumption, and noise-free operation in a space-saving package, making them an alternative to mechanical relays. Consisting of a photo MOSFET optically coupled to an infrared light emitting diode, the new photorelay utilizes the latest generation trench MOSFET to realize an approximately 1.4 times higher on-state current than Toshiba's existing product, the TLP3103. This performance, combined with a 3.3A (max.) output, will accelerate the replacement of mechanical relays in applications that require high density assembly. Replacing a 3A-capable DIP package with the 2.54SOP6 package reduces the assembly area by 40 percent, and the overall product height by half.

  • Normally off (1-Form-A)
  • Off-state output terminal voltage: 60V (min)
  • Trigger LED current: 3mA (max)
  • On-state current: 3.3A (max) (A connection)
  • Isolation voltage: 1500Vrms (min)
  • Meets safety standards
Additional Applications
  • Mechanical relay replacements
  • Security systems
  • Measuring instruments
  • Factory automation (FA)
  • Amusement equipment

Main Specifications
Part Number TLP3107
Package 2.54SOP6
Body size: 6.3 x 4.4mm
(Including lead: 6.3 x 7.0mm)
On-state Current 3.3A (max.)
On-state Resistance 0.04Ω (typ), 0.07Ω (max.)
Off-state Voltage 60V (min.)
Off-state Current (Photo Side) 10nA (max.)
Trigger LED Current 3mA (max.)
Isolation Voltage 1500Vrms (min.)
Pricing and Availability

Mass production of the new photorelay has begun. Please contact your local Toshiba Sales Office for samples and pricing.

*About TAEC

Through proven commitment, lasting relationships and advanced, reliable electronic components, Toshiba enables its customers to create market-leading designs. Toshiba is the heartbeat within product breakthroughs from OEMs, ODMs, CMs, VARs, distributors and fabless chip companies worldwide. A committed electronic components leader, Toshiba designs and manufactures high-quality flash memory-based storage solutions, solid state drives (SSDs), hard disk drives (HDDs), solid state hybrid drives (SSHDs), discrete devices, custom SoCs/ASICs, imaging products, microcontrollers, wireless components, mobile peripheral devices, advanced materials and medical tubes that make possible today's leading smartphones, tablets, cameras, medical devices, automotive electronics, industrial applications, enterprise solutions and more.

Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation, Japan's largest semiconductor manufacturer and the world's sixth largest semiconductor manufacturer (Gartner, 2013 Worldwide Semiconductor Revenue, December 2013). Toshiba Corporation was founded in 1875 and today has over 554 subsidiaries and affiliates, with 206,087 employees worldwide. Visit Toshiba's web site at

For additional company and product information, please visit

Product density is identified based on the density of memory chip(s) within the Product, not the amount of memory capacity available for data storage by the end user. Consumer-usable capacity will be less due to overhead data areas, formatting, bad blocks, and other constraints, and may also vary based on the host device and application. For details, please refer to applicable product specifications

2014 Toshiba America Electronic Components, Inc. All rights reserved. Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice. Technical and application information contained here is subject to the most recent applicable Toshiba product specifications.

OPTO 14 709