Rewire Your Wireless Thinking

Learn how Toshiba connectivity ICs provide fast, low power and flexible solutions



Toshiba is connectivity-focused

Look inside our family of wireless technologies. No question, they’re seeing rapid adoption in a range of uses from point-to-point connections to the Internet of Things (IoT) – to the Internet of Everything (IoE). With wireless sensor networks on the rise, Toshiba wireless ICs are driving the next wave of connectivity.

Hundreds of millions of ICs sold

Toshiba offers wireless connectivity solutions for many applications, across all primary standards and technologies. These ICs enable high-speed, low-power media sharing, HD video streaming, data transfer between mobile and stationary devices, and easy Internet connectivity. Hundreds of millions of Toshiba wireless ICs are in use.

Designing a wireless product?

Designing for smartphones, tablets, NFC readers/writers, wearables, cameras, automotive applications, handheld medical products, home appliances with wireless functions, or other industrial applications? Join the forward thinkers who rely on Toshiba for wireless connectivity ICs.

© 2015-2017 Toshiba America Electronic Components, Inc.
All Rights Reserved. Legal. Trademarks.
*Effective data transfer rate. **As of 1/15/2015.

Enter to Win Free! Panasonic Place and
Play Bluetooth® Module Evaluation Kit.

15 kits to be awarded. It’s a no-brainer drawing.

> Evaluation Kit Promotion Entry Form
> Promotion Rules

> Panasonic PAN1026 Series Place and Play Bluetooth module
> Toshiba TC35661 Dual Mode BT Controller Chip Family
> Toshiba TC35661-502 IC features
> Guidelines on when to purchase module hardware or a discrete solution

The Panasonic EVAL PAN1026 Series dual mode Place and Play Bluetooth® Module Evaluation kit consists of two PAN1026ETU development SMD modules and enables you to do simple prototyping and testing of the Toshiba TC35661-502 Bluetooth IC with the help of the EasyDualMode software under Related Information (Easy SPP, Bluetooth Demo Software and Quick Start). For greater levels of testing, Toshiba also offers the Toshiba starter kits.

The Bluetooth IC can later be purchased as a discrete IC or as part of the ready-to-use Panasonic PAN1026 Place and Play Bluetooth Module.

Panasonic Module

The Panasonic PAN1026 Series Place and Play Bluetooth module features Toshiba TC35661-502 Bluetooth 4.0 IC, with embedded ARM® processor, embedded Bluetooth protocol stack, serial port profile (SPP), command set API , integrated EEPROM and antenna. Bluetooth 4.0 combines the legacy of Bluetooth Classic and the ultra-fast connection set up time and flexibility of Bluetooth Low Energy. Bluetooth Low Energy is designed to create low data rate networks using a minimum amount of power. The embedded serial port profile (SPP) and BLE-GATT profile frees application resources while the command set API creates a simple but flexible firmware interface. An onboard antenna does away with 2.4GHz RF circuit complexity.

Product design cycles may be reduced using Panasonic’s reference design and design review services. PCB layouts are simplified using available Gerber files and minimized with Panasonic’s small footprint technology. The module is just 15.6mm x 8.7mm x 1.9mm and fully shielded to improve immunity.  Panasonic Bluetooth RF module carries FCC, IC, CE and Bluetooth certifications.

PAN1026 Series Documentation.

Join the forward thinkers who rely on Toshiba for wireless connectivity ICs and wireless insight to design fast, low-power RF products.

As one of the world’s leading suppliers of semi- conductor products, Toshiba offers wireless
connectivity solutions for many applications, ensuring
that its products are compliant with global standards. From true, one-chip multi-technology "combo" solutions to the market’s smallest touch-transfer chip, Toshiba helps customers deliver fully connected platforms with reduced constraints on speed, power and space.  > Wireless Brochure 

Toshiba Wireless Technologies:

Toshiba Bluetooth® solutions support sharing small amounts of data and digital/audio and include a one-chip, multi-mode low-energy device.

Toshiba offers a true, one-chip integrated solution for both single and dual mode that supports a variety of Bluetooth features including Bluetooth Low Energy (BLE), effectively reducing costs associated with incorporating two wireless technologies.

Bluetooth product family highlights:

Toshiba Bluetooth products:

Toshiba Wi-Fi® long distance solutions make connectivity for Internet of Things and integration of WLAN deployments reliable.

Toshiba Wi-Fi solutions can handle RF interference in the unlicensed 2.4GHz band in a highly efficient manner using novel approaches for antenna sharing and interference mitigation.

Wi-Fi product family highlights:

Toshiba Wi-Fi products:

Toshiba TransferJet™ enables close proximity wireless touch-transfer at 375* Mbps using the market’s smallest one-chip TransferJet LSI.

Toshiba TransferJet, IC modules and accessories enable high-speed communication between two devices positioned next to each other. This wireless technology allows large volumes of data, media or video to be shared securely and quickly. There is no need for complex setup, device pairing or the use of access points. Simply touching together two TransferJet-enabled devices can transfer large files.

TransferJet product family highlights:

Toshiba TransferJet products:

Toshiba Near Field Communication solutions offer short-range, highly secure, bi-directional data transfer with no set up required.

Toshiba Near Field Communication (NFC) solutions are designed to facilitate easy connections, quick transactions, and simple data sharing with very short-range, highly secure communication. Toshiba’s NFC controller chip enables small amounts of data to be shared confidentially between two electronic devices and supports multiple identities by interfacing with 3 Secure Elements. This technology enables seamless interaction with the mobile user for endless applications including cashless payment, access management, point-of-sale, and ticketing.

Near Field product family highlights:

Toshiba Near Field products:

Toshiba Wireless Power Charging solutions enable up to 15-Watt power transfer for mobile devices with high-power density batteries.

Toshiba Wireless Charging solutions enable wireless mobile device charging without the use of a cable. No exact alignment of the device(s) being charged is necessary. The devices effectively manage up to 15-Watt power transfer necessary for wireless charging of tablets, phablets or smartphones.

Wireless Charging product family highlights:

Toshiba Wireless Charging products:

Receiver ICs: Transmitter ICs:

Ask a question about Toshiba wireless ICs.

First Name*

Last Name*

Title*

Company*

Email Address*

Required Fields*

Question(s):


Trademarks used on this site.

Wi-Fi is a registered trademark of the Wi-Fi Alliance. Bluetooth is a trademark of the Bluetooth SIG and is used under license by Toshiba. TransferJet is a trademark of the TransferJet Consortium. iOS is a trademark of Apple Inc. Android is a trademark of Google Inc. Qi is a trademark of the Wireless Power Consortium. ARM is a trademark of ARM Ltd. Windows is a registered trademark of Microsoft Corporation.

Trademarks used on this site.

Wi-Fi is a registered trademark of the Wi-Fi Alliance. Bluetooth is a trademark of the Bluetooth SIG and is used under license by Toshiba. TransferJet is a trademark of the TransferJet Consortium. iOS is a trademark of Apple Inc. Android is a trademark of Google Inc. Qi is a trademark of the Wireless Power Consortium. ARM is a trademark of ARM Ltd. Windows is a registered trademark of Microsoft Corporation.