...
...
  
...

  Site Menu

..

Index

  NiMH Batteries
  Clean Power
  Monster Cables

  Connect DLP / DVD

  Connect Computer

  Connect Nokia

----
Where to Buy
  SmarterMall

  Herman's

  Shop Toshiba
----
Digital Members
  Registration
  Extended Warranty
  Lost & Found

----

  Reference
Buyers Guide
----
Careers at Toshiba
----
----
----
----
Toshiba recognizes that this is the era of Digital Convergence and Personal Mobility.

As a leader in Superior Performance Technology Products, we recommend that you connect and power your advanced devices with the highest quality and most reliable brand in the industry -
Monster Cable / Monster Power.

MB4DCRC: AA Size NiMH Digital Power.
This is the best solution for enjoyment and cost savings. NiMH batteries last longer than alkaline batteries. NiMH batteries are rechargeable batteries, so they can be used several times and thereby reduce the expense of continually purchasing new batteries. NiMH batteries are sold with a power adapter for charging. Monster Digital Power batteries are 1800mAh! NiMH batteries do not have the memory effect associated with NiCd batteries, which means that these batteries can be recharged at any time and at your convenience, you do not have to wait for batteries to drain between charges.

MB4MP3AAA: AAA Size NiMH Digital Power.
Monster PowerCells provide maximum usage time on all your electronics that require AAA batteries. PowerCells can hold up to 100% more battery power than disposable alkaline batteries, and as much as 30% more than ordinary rechargeable batteries. Monster PowerCells feature the latest Nickel Metal Hydride (NiMH) technology, which lets you safely recharge and refresh the PowerCells any time that you want to in the Monster Digital Power Charger. Your electronic equipment can be ready to go when you are! High capacity 750mAh AAA size PowerCells and Monster Digital Charger included.

MB4DCRC:
AA Size are great for Toshiba Digital Cameras.
Use these in any device that requires AA batteries.

MB4MP3AAA:
AAA Size are great for Toshiba MP3 Players.
Use these in any device that requires AAA batteries.

The Monster Difference

Monster PowerCells can be recharged 1,000 times or more with the Monster Digital Charger, saving thousands of dollars in equivalent replacement cost for disposable alkaline batteries.

Monster 1800mAh PowerCells last longer than other 1300-1600mAh rechargeable batteries.

You will experience longer lasting performance per charge because of higher capacity batteries.

4AA Size NiMH Batteries equals more than $21,133 of Alkaline Batteries.

By using rechargeable batteries you save money from continually buying alkaline. You are also protecting the environment by reducing the number of 'throw away' batteries.

Equals $21 Thousand Alkaline Batteries.
Recharge faster with the intelligent charger. Spend less time waiting and more time using your equipment.

Intelligent charger quickly charges up to 1600mAh, then does 'trickle charge' to full 1800mAh, so batteries do not overheat (cook) in the charger. This is better for long battery life and more safe for you.

Recharge Faster!
Digital Cameras
Toshiba Digital Cameras

... ..

.

.. Contact Toshiba Privacy Statement Terms of Use .. .. ..

  Copyright© 2001 Toshiba America Information Systems, Inc. All rights reserved.