![]() | |||||||||||||||||
|
News & EventsToshiba Security Debuts New “Fault Tolerant” Digital Video RecordersIRVINE, CA, NOVEMBER 18, 2004 – Once again raising the bar for digital video recorder (DVR) performance, Toshiba Security & Network Video today debuted its new EVR (“Extreme Video Recorder”) Series of DVRs boasting one of the the industry’s most fault tolerant designs with redundant, field replaceable dual power supplies, maximum air flow dynamics, internal RAID 5 compatibility and field-upgradeable hard drives. “As the security industry migrates towards digital video surveillance, DVR reliability has become an overriding concern for network administrators,” said Sergio Collazo, National Sales & Marketing Manager, Toshiba Security & Network Video. “Our EVR Series recorders put these concerns to rest with their unequaled fault tolerant engineering, advanced feature package and the very latest in networking technologies.” Available in 8, 16, 32 and 64 channel configurations, Toshiba EVR Series DVRs are capable of recording at up to 480 pictures per second (up to 30 PPS per camera) at resolutions as high as 720x480 with up to 16 channels of audio. This capacity to support a large volume of cameras while delivering excellent image quality qualifies EVR recorders for enterprise class organizations, government agencies, multi-site businesses and other high-security recording applications. Representing the latest evolution in Toshiba’s continually growing line of digital and networked systems devices, the EVR Series of DVRs offer a wide range of sophisticated features: For more information and the name of a local Toshiba Security & Network Video distributor, call 1-877-696-3822. Or visit www.cctv.toshiba.com. ABOUT TOSHIBA AMERICA INFORMATION SYSTEMS, INC. ©2004 Toshiba America Information Systems, Inc. All product names and trademarks belong to their respective owners. Information in press releases, including without limitation product prices, specifications, and contact information, is current on date of the release, and is subject to change without notice. Reseller prices may vary.
| ||||||||||||||||