layout.gif




   
 Notify me about future
    product information


 

 

 

 

FOR IMMEDIATE RELEASE

November 9, 1994

Toshiba Introduces a 540MB 0.5-inch High, 2.5-inch Hard Disk Drive; New Drive Targets Slimline Notebook, Sub-Notebook and Portable Computers


IRVINE, Calif., November 9, 1994 -- Toshiba America Information Systems, Inc., Disk Products Division (TAIS, DPD) today introduced the MK-1924 Series drives which offer a 540MB capacity and a fast 13ms average seek time in a 0.5-inch high (12.7mm), 2.5-inch form factor.

"A dramatic increase in the use of portable computers for graphics and multimedia presentations has driven the demand for larger storage capacities and enhanced performance at a substantially reduced price point," said Jeffrey Greenwald, director of hard disk drive marketing, TAIS, DPD. The new MK-1924 Series drives meet these requirements by delivering high capacity and fast performance in a 2.5-inch drive.

According to Greenwald, the MK-1924 Series drives, with Fast ATA and SCSI-2 interface support, take advantage of the latest technology and a high level of integration to provide today's smaller, slimmer sub-notebook and portable computers with higher capacity, performance and low power requirements at a reduced cost. "Such innovations as the predictive read-channel technology of PRML (Partial Response Maximum Likelihood) and aerial density improvements, are key developments to these high-performing drives," said Greenwald.

The MK-1924 Series drives also feature a 128K cache memory including write-cache, and use a two-platter design offering a rapid spin rate of 4200rpm.

The MK-1924 Series drives are available with either Fast ATA or SCSI-2 interfaces to allow for compatibility with a wide range of systems. The MK-1924FCV Fast ATA interface drive supports multiword DMA mode 2 at a data transfer rate of 16.6MB/sec, and PIO mode 4 with 16.6MB/sec data transfer rate. The MK-1924FBV provides a SCSI-2 interface and features a 10MB/sec data transfer rate.

In addition to providing high performance regardless of interface type, the new MK-1924 Series drives were developed specifically to meet the ever increasing demands of the portable and sub-notebook market for small size, high capacity, low weight and low power requirements. The new 2.5-inch drives weigh only 5.6 ounces (160 grams) and consume an average of only one watt from a single 5-volt supply while spinning up to operational speed in a fast five seconds.

The MK-1924 Series drives are part of a complete product offering of 2.5-inch disk drives which now allow Toshiba to offer the most complete range of products ever. Toshiba's complete line of 2.5-inch drives spans from 86MB up to 1080MB, including the new MK-2728 1GB 2.5-inch drive. Recent additions to Toshiba's 2.5-inch line also include the MK-2526, MK-2528 and MK-2628 Series drives which offer capacities of 528MB, 704MB and 810MB respectively, and the MK-1824 slimline drive with a 352MB capacity.

The MK-1924 Series drives weigh only 5.6 ounces and measure a slim 12.7mm high. These new drives are also extremely reliable, demonstrating a 300,000 hour MTBF.

The MK-1924 Series drives are available in first quarter 1995 in OEM production quantities at a suggested list price of only $435.

Headquartered in Irvine, California, TAIS is comprised of seven divisions which manufacture and market a wide range of business and information-oriented products in the United States. Products include portable computers, disk drives, CD-ROM drives, plain paper copiers, facsimile systems, digital key telephones and PBX systems, voice mail systems and toner products.

TAIS is an independent operating company, owned by Toshiba America Inc., a subsidiary of the $44.9 billion Toshiba Corporation, a world leader in high-technology products with 138 major consolidated subsidiaries worldwide.

The TAIS Disk Products Division markets a wide range of industry-standard Winchester and CD-ROM disk drives in the United States. For additional product information, contact Toshiba America Information Systems, Inc., Disk Products Division, 9740 Irvine Blvd., Irvine, CA 92713; telephone (714) 457-0777.

Agency Contact:

Colleen Raley

The Benjamin Group Inc.

(714) 245-7500

colleen_raley@benjamingroup.com

Back to top

  © 2003 Toshiba America Inc. | Terms of Use | Privacy Statement