layout.gif




   
 Notify me about future
    product information


 

 

 
FOR IMMEDIATE RELEASE

April 10, 1995

Toshiba Introduces 815MB 0.5-inch High Hard Disk Drive -- Highest Capacity Slimline

New Drive Targets Slimline Notebook, Sub-Notebook and Portable Computers


IRVINE, Calif., April 10, 1995 -- Toshiba America Information Systems, Inc., Disk Products Division (TAIS DPD) today introduced the MK-1926F Series drives which offer a 815MB capacity -- the worldís highest capacity slimline drive, and a fast 13ms average seek time in a small 0.5-inch high (12.7mm), 2.5-inch form factor.

"Todayís notebook users require more from their portable systems than ever before," said Scott Smith, vice president of marketing, TAIS, DPD. "The MK-1926F Series is ideal for Pentium-class notebook users who require high performance and reliability and who rely on their portable systems for highly demanding database, multimedia and graphics applications. The new MK-1926F Series drives meet these requirements by delivering fast performance in the highest capacity slimline drive on the market."

The new MK-1926F Series offers superior performance. The three platter drive offers an internal data transfer rate of up to 44.9Mbits/sec, a 128KB write cache buffer, and a rapid spin rate of 4200rpm.

The MK-1926F Series drives are available with either Fast ATA or SCSI-2 interfaces to allow for compatibility with a wide range of systems. The MK-1926FBV provides a SCSI-2 interface and features a synchronous data transfer rate of 10MB/sec and an asynchronous data transfer rate of 6MB/sec. The MK-1926FCV Fast ATA interface drive supports multiword DMA mode 2 at a data transfer rate of 16.6MB/sec, and PIO mode 4 with 16.6MB/sec data transfer rate.

In addition to its high performance capabilities, the new MK-1926F Series drives were developed specifically to meet the demands of the portable and sub-notebook market for small size, high-capacity, low weight and low power requirements. The new 2.5-inch drives consume less than one watt from a single 5-volt supply while spinning up to operational speed in a fast 5 seconds.

The MK-1926F Series drives weigh only 150 grams and measure a slim 0.5-inches high, 2.76-inches wide and 3.94-inches deep. These new drives are also extremely reliable, demonstrating a 300,000 hour MTBF.

The MK-1926F Series drives are available in the second quarter of 1995 in quantities at a price of $275.

Headquartered in Irvine, California, TAIS is comprised of seven divisions which manufacture and market a wide range of business and information-oriented products in the United States. Products include portable computers, disk drives, CD-ROM drives, plain paper copiers, facsimile systems, digital key telephones and PBX systems, voice mail systems and toner products.

TAIS is an independent operating company, owned by Toshiba America Inc., a subsidiary of the $44.9 billion Toshiba Corporation, a world leader in high-technology products with 138 major consolidated subsidiaries worldwide.

The TAIS Disk Products Division markets a wide range of industry-standard Winchester and CD-ROM disk drives in the United States. For additional product information, contact Toshiba America Information Systems, Inc., Disk Products Division, 9740 Irvine Blvd., Irvine

Agency Contact:

Colleen Raley

The Benjamin Group Inc.

(714) 245-7500

colleen_raley@benjamingroup.com

Back to top

  © 2003 Toshiba America Inc. | Terms of Use | Privacy Statement