layout.gif




   
 Notify me about future
    product information


 

 

 
FOR IMMEDIATE RELEASE

February 28, 1996

Toshiba Introduces First Slimline Six-Speed CD-ROM Drive, New Drive Targeted to Notebook Computer Manufacturers


IRVINE, Calif., February 28, 1996 -- Toshiba America Information Systems, Inc., Disk Products Division (TAIS DPD) today announced the industry’s fastest slimline CD-ROM drive. Toshiba’s new XM-1402B offers leading six-speed performance in a slimline format measuring only 17mm (H) x 128mm (W) x 136.4mm (D) and weighing only 380 grams.

The new six-speed XM-1402B internal CD-ROM drive boasts a 900KB/sec transfer rate and a fast 160ms random seek and 190ms average access. The drive’s fast performance is attributable to its high rotation speed, which was accomplished by accelerating the processing speed of the digital signal processor used in error correction and by improving the pick-up motor to support higher speed data accessing.

Designed for notebook computers, the drive has a low 3.7W average power consumption. The drive incorporates a power-saving function that cuts consumption to 85 milliwatts when the drive is in a wait state. The drive operates with a 5V power supply.

"This new drive packs tremendous performance into a very small package," said Jerry Higgins, vice president of CD-ROM marketing, TAIS DPD. "With this new drive, OEMs can now design fast six-speed performance plus proven Toshiba CD-ROM reliability into their notebook computers."

"It is critical when developing a drive for the notebook computer market that you do not sacrifice reliability," said Higgins. To that end, Toshiba designed the new XM-1402B drive in a fully-sealed enclosure to prevent contamination and ensure reliability. Through these efforts, the drive has a 60,000 hour MTBF.

While engineering the XM-1402B to meet minimal size requirements, Toshiba developed the drive to support multimedia; the drive fully meets MPC-3 specifications while supporting Kodak multi-session Photo CD and CD EXTRA.

Toshiba designed the drive for optimum performance using Toshiba's proven variable speed playback system and digital servo control. The variable speed playback system allows the drive to read data before the disc rotational speed reaches any of 1, 4 or 6 times standard rotational speeds. The digital servo control, which offers greater precision in tracking and head positioning, further contributes to performance and reliability.

The XM-1402B features a drawer-type disk loading system. The drawer holds an inserted disk firmly and securely, allowing disks to be left in a PC when it is being carried, or even if the PC is stood on end.

The new XM-1402B is designed for use in notebook computers and features an ATAPI interface that eases integration.

Toshiba's XM-1402B internal CD-ROM drive is priced from $195 in OEM quantities and samples are now available.

Headquartered in Irvine, Calif., TAIS is comprised of seven divisions which manufacture and market a wide range of business and information-oriented products in the United States. Products include portable computers, disk drives, CD-ROM drives, plain paper copiers, facsimile systems, digital key telephones and PBX systems, voice mail systems and toner products.

TAIS is an independent operating company, owned by Toshiba America Inc., a subsidiary of the $53.8 billion Toshiba Corp., the second largest computer and office equipment manufacturer and the world’s 20th largest corporation in terms of sales. Toshiba Corp. is a world leader in high technology products with 134 major consolidated subsidiaries worldwide.

The TAIS Disk Products Division markets a wide range of industry-standard Winchester and CD-ROM drives in the United States. For additional product information, contact Toshiba America Information Systems, Inc., Disk Products Division, 9740 Irvine Blvd., Irvine, CA 92618; telephone (714) 457-0777.

Photos available upon request.

Agency Contact:

Colleen Raley

The Benjamin Group Inc.

(714) 245-7500

colleen_raley@benjamingroup.com

Back to top

  © 2003 Toshiba America Inc. | Terms of Use | Privacy Statement