Tiny Toshiba Drives To Offer Storage Aplenty
January 16, 2002
By John G. Spooner, Staff Writer, CNET News.com
http://news.cnet.com/news/0-1006-200-8501503.html?tag=mn_hd
Toshiba
is promising big things for small packages with a pair of new hard drives.
The diminutive 10GB and 20GB drives, announced
Wednesday, will mean cavernous storage for a range of mobile-computing
devices, including music players, personal digital assistants, wearable
computers and even laptops. Their capacities are well above those of most
gadget-sized devices, including Apple Computer’s well-endowed new iPod.
Based on the design of the company’s 2.5-inch notebook
PC drives, the new 1.8-inch designs are smaller than a credit card in
width and length and, at 5 millimeters and 8 millimeters, respectively,
only slightly thicker than a credit card.
Most PDAs, such as Compaq Computer’s iPaq,
offer between 16MB and 64MB of internal storage in the form of flash memory
or RAM and also can use external compact flash cards, such as Sony’s Memory
Stick, with capacities up to 1GB. IBM offers the 1-inch Microdrive,
a tiny hard drive with capacities ranging from 170MB to 1GB. It is designed
to fit inside the compact flash ports used by PDAs and other devices.
Larger hard drive-based music players and notebook
PCs typically offer drives with capacities between 10GB and 40GB. New
60GB hard drives are just coming on the market for notebooks.
Toshiba says that its new drives, with tens of gigabytes
on hand, will support manufacturers’ desire to add more complex applications
or more storage space for music or photos in new products.
Those manufacturers are likely to follow the example
of Apple and its PDA-sized iPod
portable music player, which uses a 5GB hard drive. Apple says the drive
can store up to 1,000 songs and can also be used as a portable hard drive
to store other files or transfer them between machines.
The new drives from Toshiba’s Storage Systems Division
should roughly double and quadruple those figures, though actual storage
figures will depend on the device each drive is used for.
Toshiba said it would begin shipping the 10GB drive,
dubbed the MK1003GAL, in February and the 20GB unit, known as the MK2003GAH,
in March. The company did not announce pricing for the new drives.
|