Toshiba Fits 20GB Onto 1.8-Inch Disk - Tiny,
High-Capacity Drives Are Headed For MP3 Players, Handhelds, And Elsewhere.
January 16, 2002
Sean Captain, PCWorld.com
http://www.pcworld.com/news/article/0,aid,79727,00.asp
Toshiba's tiny high-capacity hard drives are hitting new highs: The company
is announcing 10GB and 20GB versions of the series.
Measuring 1.8 inches across--about the diameter of silver dollar coin--the
double-sided, single-platter drives premiered at 2GB in May 2000 and expanded
to 5GB in June 2001.
Toshiba has doubled the capacity in the 10GB model, and quadrupled it
for the 20GB model, by adding a second double-sided platter. At last week's
Consumer Electronics Show in Las Vegas, several companies including Creative,
RCA, and SonicBlue unveiled handheld music players that use 2.5-inch laptop-style
10GB and 20GB hard drives in paperback-size devices weighing about 10
ounces.
The new Toshiba drives could match that storage in players about half
as large. Drives of 1.8 inches are the optimum size, says Toshiba spokesperson
Amy Dalphy. "There are a lot of [players with] 2.5-inch hard drives
out there, but they're big."
The most notable application of Toshiba's 5GB drive is probably the Apple
iPod MP3 player, which can store upward of 1000 songs. Though neither
company will confirm that the iPod uses Toshiba's drive, representatives
of both companies acknowledge Toshiba is the only one producing a 5GB
drive small enough to fit in Apple's music player.
Beyond MP3 Players
Music players are only one application Toshiba is banking on. Gigabytes
of storage would also allow handheld devices to contain video files, for
example. While she can't name customers, Dalphy says Toshiba is working
with a number of companies--many of them startups--on a variety of product
ideas that could use Toshiba's tiny drives.
"If they do make it to market, they will change the way we do things,"
she says of the unannounced projects in development. Dalphy expects products
should start appearing between the middle and the end of 2002, or possibly
earlier. Toshiba will ship its new 20GB drive in volume in February, and
the 10GB version will follow in March.
Toshiba currently makes versions of its 2GB and 5GB drives embedded in
Type II notebook PC cards. The 5GB MK5002MPL hard disk drive is priced
at $399, while the 2GB version costs $299. Dalphy expects Toshiba will
eventually incorporate at least the new 10GB drive into a PC card, although
she says the company is unsure whether there is much demand for a larger
capacity in that product.
|