layout.gif




   
 Notify me about future
    product information


 

 

 
FOR IMMEDIATE RELEASE

April 7, 1997

Toshiba Introduces 16-Speed ATAPI CD-ROM Drive

High Performance and Reliability at a Competitive Price


IRVINE, Calif., April 7, 1997 -- Toshiba America Information Systems Inc., Disk Products Division today introduced its max-16-speed ATAPI CD-ROM drive. The XM-6002B internal drive offers high performance at a competitive price for PC manufacturers integrating the drive into their PCs and for users who want to upgrade their systems.

"This competitively priced drive meets the industry's current demand for the fastest, highest-performance products on the market," said Maciek Brzeski, director of marketing, CD-ROM, TAIS DPD. "Also, this new drive continues Toshiba's tradition of offering the industry's most-reliable, high-quality CD-ROM products."

PC OEMs and end-users wanting to upgrade their lower-speed CD-ROM drives with the fastest ATAPI interfaced-drive available can choose the XM-6002B. The new 16X drive speeds through data on a CD-ROM at a 2,400KB/sec. maximum data transfer rate supported by a 90ms random seek and 100ms random access.

To achieve its industry-leading performance specifications, the drive features a 256KB buffer and Partial Constant Angular Velocity (PCAV). PCAV combines the best of Constant Angular Velocity (CAV) and Constant Linear Velocity (CLV) to obtain the highest transfer rates while reading data from anywhere on the disk. The new drive is designed with an ATAPI interface and supports PIO mode 3 and DMA mode 1. PIO mode 3 provides a burst mode data transfer rate of 11.1 MB per second, while DMA multiword mode 1 supports a burst data transfer rate of 13.3MB per second and reduces the burden on the main CPU.

The XM-6002B fully meets the demands of today's multimedia applications. The drive is MPC-3 compliant and supports both multisession Photo CD and CD-EXTRA. The drive can also read CD-RW CD-DA, CD-ROM XA, CD-I, CD-I Ready and CD-I Bridge disc formats. In addition, the new XM-6002B sets another industry milestone with its ability to read CD-RW (Erasable) media.

Toshiba designed the drive for optimum performance. The XM-6002B employs Toshiba's proven Active Wide Range playback system and digital servo control. The Active Wide Range playback system allows the drive to read data at +/- 80 percent of a specific rotational speed -- allowing the drive to access data on the disc at almost any time. The digital servo control, which offers greater precision in tracking and head positioning, further contributes to performance and reliability.

For user convenience, the XM-6002B drive was designed with a tray-loading mechanism. A media-removal prevention function ensures that CDs cannot be ejected during read operations. For integration and set-up flexibility, the drive may be mounted horizontally or vertically. The XM-6002B was designed based on Toshiba's highly reliable, award-winning 12X CD-ROM drives to ensure reliability; as a result XM-6002B features a 100,000 hour MTBF.

The new XM-6002B internal drive measures only 1.62(h) x 5.69(w) x 7.41(d) inches and weighs only 1.98 pounds. The drive's power consumption is a low 0.5 watts standby and 4.6 watts average. The drive may be used in temperatures ranging from 41-122 degrees Fahrenheit.

The XM-6002B ATAPI drive has a suggested list price of $185 and is available now.

TAIS is headquartered in Irvine, Calif., with annual sales of approximately $4 billion. TAIS is comprised of nine divisions which manufacture and market a wide range of business and information-oriented products in the United States. Products include notebook and desktop computers, disk drives, CD-ROM drives, DVD drives, plain-paper copiers, facsimile systems, digital business telephone systems, voice mail, security imaging systems, industrial video products, medical, digital and PC cameras, systems solutions for the cable industry, and toner products. TAIS is an independent operating company, owned by Toshiba America, Inc., a subsidiary of the $53 billion Toshiba Corp., a world leader in high-technology products with 207 major subsidiaries and affiliates worldwide.

The TAIS Disk Products Division markets a wide range of industry-standard Winchester, CD-ROM and DVD-ROM drives in the United States. For additional product information, contact Toshiba America Information Systems, Inc., Disk Products Division, 9740 Irvine Blvd., Irvine, CA 92618-1697; telephone (714) 457-0777, or on the World Wide Web at: http://www.tais.com/taisdpd/ or http://www.toshiba.com.

Agency Contact:

Colleen Raley

The Benjamin Group Inc.
(714) 245-7500

colleen_raley@benjamingroup.com

Back to top

  © 2003 Toshiba America Inc. | Terms of Use | Privacy Statement