layout.gif




   
 Notify me about future
    product information


 

 

 
FOR IMMEDIATE RELEASE

November 17-21, 1997

Toshiba Introduces Two New Mainstream Capacity 2.5-Inch Hard Disk Drives for Notebooks and Mini-Notebooks


New Products Summary:
Model Number Capacity Height Platters
MK3205MAV 3.25GB 12.7mm 3
MK2104MAV 2.16GB 12.7mm 2

LAS VEGAS, Nev., November 17-21, 1997 " Toshiba America Information Systems, Inc., Disk Products Division (TAIS DPD) today introduced two new 2.5-inch hard disk drives, one of which is the inaugural product of a new class of super-slim form factor drives. Toshiba's new slimline MK3205MAV 2.5-inch drive meets current mainstream market demand with its 3.25GB capacity, while the new MK2104MAV slimline 2.5-inch drive delivers a 2.16GB capacity for entry-level notebook computers. Toshiba's new hard disk drives will be on display at COMDEX/Fall, Las Vegas Convention Center, South Hall, booth # L1214.

New Drives Meet Customer Demands
"Toshiba is bringing to market exactly what our customers have asked for " competitive products at key capacities available in volume," said Amy Lian, director, Hard Disk Drive Business Unit, TAIS DPD. "The mainstream notebook computer user, in both the consumer and commercial markets, is demanding their systems come equipped with increased capacities of 2-3GB for midrange notebooks. As a result, these products will be the hard disk drives of choice for this season's leading notebook computers."

High Areal Density
Toshiba's drives are available with an ATA-3 interface to meet OEM, VAR/VAD and system integrator needs. This new family of 2.5-inch disk drives combines PRML data channels with advanced magneto resistive (AMR) head technology to yield higher areal density allowing up to 1.08GB of storage per platter. This high per-platter storage capacity allows increased overall capacity, while maintaining a slim form-factor. "Because today's software applications are so capacity-hungry, notebook computer consumers in every segment of the market are demanding higher-capacity hard disk drives," added Lian.

Reliability Critical for Portable Computing
Toshiba's two new hard disk drives were designed and engineered to result in high performance for portable computing environments. Developed to meet Toshiba-renowned reliability specifications, the drives offer an industry-high MTTF of 300,000 hours. Also, to combat the consequences of a dropped or shaken notebook computer, the drives all adhere to a high operating shock rating of 100G, and a non-operating shock rating of 350G.

3.25GB MK3205MAV Specifications
Toshiba's new 3.25GB MK3205MAV was developed to offer notebook manufacturers a product that would meet their mainstream volume demands. The 12.7mm-high MK3205MAV drive offers a 4,200 rpm rotational speed which contributes to a fast 13ms average seek time. The drive provides a peak internal data transfer rate of up to 88.2 Mbit/sec and data transfer rates of 16.6MB/sec in PIO mode 4 and 33.3MB/sec in Ultra DMA mode 2. The 512KB cache contributes to the drive's overall performance specifications. MK3205MAV weighs only 5.29 ounces and measures 0.49"/12.7mm (h) x 2.75" (w) x 3.94" (d).

2.16GB MK2104MAV Specifications
Perfectly suited for integration into leading entry-level notebook computers, the MK2104MAV hard disk drive offers 2.16GB of storage space. The drive's fast internal data transfer rate of 81.1Mb/sec is supported by fast buffer-to-host transfer rates of 16.6Mb/sec in DMA mode 2 and PIO mode 4. With a 128KB buffer, the drive provides a fast average seek time of 13ms and a rotational speed of 4,200rpm. Adhering to the size and weight restrictions dictated by today's notebook computers, the new MK2104MAV weighs only 5.29 ounces and measures 0.49"/12.7 mm (h) x 2.75" (w) x 3.94" (d).

Power Requirements
To meet the low-power demands of today's notebook computers, the two new drives use a 5 volt charge and consume a low 0.3 watts on standby.

Availability
The new MK3205MAV and MK2104MAV 2.5-inch hard disk drives are available now.

About Toshiba
Headquartered in Irvine, Calif., with annual sales of approximately $4 billion, TAIS is comprised of nine divisions which manufacture and market a wide range of business and information-oriented products in the United States and Latin America and one wholly owned subsidiary which operates a network of copier/fax dealers. Products include portable and desktop computers; hard disk, CD-ROM and DVD drives; plain-paper copiers; facsimile systems; voice mail systems; digital business telephone systems; toner products; systems solutions for the cable industry; digital cameras and network systems. TAIS is an independent operating company, owned by Toshiba America, Inc., a subsidiary of the $48 billion Toshiba Corp., the sixth largest electronics and electrical equipment manufacturer, and the world's 37th largest corporation in terms of sales. Toshiba Corporation is a world leader in high-technology products with 303 major subsidiaries and affiliates worldwide.

The TAIS Disk Products Division markets a wide range of industry-standard 2.5-inch hard disk drives, CD-ROM drives and DVD-ROM drives in the United States. For additional product information, contact Toshiba America Information Systems, Inc., Disk Products Division, 9740 Irvine Blvd., Irvine, CA 92618-1697; telephone (714) 457-0777, or on the World Wide Web at: http://www.tais.com/taedpd/ or http://www.toshiba.com.

Agency Contact:

Colleen Raley

The Benjamin Group Inc.

(714) 245-7500

colleen_raley@benjamingroup.com

Back to top

  © 2003 Toshiba America Inc. | Terms of Use | Privacy Statement