layout.gif




   
 Notify me about future
    product information


 

 

 
FOR IMMEDIATE RELEASE

November 16, 1998

Toshiba Introduces 40X CD-ROM Drive With SCSI Interface

For multi-tasking environments such as workstations and servers, the new XM-6401B provides the right combination of performance, reliability and features


FOR IMMEDIATE RELEASE

LAS VEGAS, Nev., November 16, 1998-Toshiba America Electronic Components, Inc. (TAEC), Disk Products today announced the XM-6401B 40X CD-ROM with SCSI-2 interface, continuing the company's commitment to delivering the right optical product to meet customers' demands. With the introduction of the XM-6401B, Toshiba provides a high-quality, highly reliable optical solution for SCSI users. The drive will be displayed in Toshiba's booth during COMDEX/Fall, November 16-20 in the Las Vegas Convention Center, Booth #L1814.

"There is a definite need for SCSI CD-ROM drives that fulfill the immediate and long-term computing needs for industries that run high-end applications, such as banking and government," said Maciek Brzeski, vice president, marketing, TAEC Disk Products. "Toshiba's XM-6401B 40X SCSI CD-ROM drive provides these companies with the high performance and reliability needed to maximize their technology investment."

Traditional SCSI markets, such as workstation and servers, also require peripherals that will provide stability in the marketplace while meeting their high-end computing demands. The Toshiba XM-6401B meets these demands with Toshiba renowned quality, reliability and innovation.

The XM-6401B features the fastest performance on the market today, by increasing the drive speed over previous generations. To provide the fastest immediate access to data and smooth branching between scenes, the drive has a fast random access time of only 79ms and an average random seek of 85ms. For fast data transfers of software loads from CD-ROM to hard disk drives, the XM-6401B boasts a 6MB/sec. maximum sustained transfer rate and supports burst interface transfer rates of 20MB/sec. Data transfer is further optimized through the use of Constant Angular Velocity technology and a 256KB cache.

Toshiba designed the XM-6401B with Active Wide Range playback system to deliver optimum performance. The company-developed Active Wide Range playback system enables the drive to read data at +/- 80 percent of a specific rotational speed - allowing the drive to access data almost instantly.

The drive's efficient power consumption average of 10 watts and ability to operate in a range of temperatures from 41 to 122 degrees Fahrenheit further contribute to performance and reliability, and ultimately, to the drive's highly-dependable 100,000 MTBF rate.

For industry compatibility, the XM-6401B is Plug-and-Play SCCI compatible and can read CD-ROM XA, CD-I, CD-I Ready, CD-I Bridge, Video CD, CD-G, CD-RW, and CD-R disc formats.

Availability
Toshiba is now shipping the XM-6401B through distribution channels.

About Toshiba
TAEC brings to market the industry's most comprehensive offering of components for the manufacturing of desktop and portable computers. As the North American manufacturing, sales and marketing arm of one of the world's largest suppliers of semiconductors, integrated circuits, storage devices and electronic components, TAEC's product offerings account for more than 30 percent of the total possible components used in desktop and portable computers. This broad product offering positions TAEC as the ideal business partner for system manufactures that want to consolidate suppliers without sacrificing quality and performance. TAEC's products include industry-leading semiconductors, integrated circuits, hard disk drives, CD-ROM drives, DVD-ROM and DVD-RAM drives, color picture tubes, display monitor tubes, liquid crystal displays, medical tubes, rechargeable batteries, microwave components, laser diodes and optical transmission devices.

TAEC Disk Products is a technology and market leader with a well established reputation for delivering high performance, highly reliable 2.5-inch hard disk drives, CD-ROM drives, DVD-ROM drives and DVD-RAM drives. For additional product information, contact Toshiba America Electronic Components, Inc., Disk Products, 35 Hammond, Irvine, CA 92618; telephone (714) 457-0777, or on the World Wide Web at: http://www.toshiba.com/taissdd/.

Agency Contact:

Lisa Landry
The Benjamin Group Inc.
(714) 245-7500
lisa_landry@benjamingroup.com

Back to top

  © 2003 Toshiba America Inc. | Terms of Use | Privacy Statement