layout.gif




   
 Notify me about future
    product information


 

 

 
Revised on 11/12/99

FOR IMMEDIATE RELEASE

July 30, 1999

TOSHIBA BRINGS THE BEST OF ALL WORLDS TOGETHER WITH FIRST COMBINATION CD-RW/DVD-ROM DRIVE

Leader in Optical Technology Gives Users Exceptional Functionality and Smooth Transition from CD to DVD


IRVINE, Calif., July 30, 1999 ‚ The Disk Products Division of Toshiba America Electronic Components (TAEC), continues to be at the forefront of optical storage innovation with the introduction of the first CD-RW drive with DVD-ROM readability. The first drive to combine these two technologies, the SD-R1002 drive is the ideal upgrade product, providing the rewritability of a CD-RW drive with the high-capacity storage of DVD-ROM. Because of its backward compatibility and low cost media, the SD-R1002 drive also provides customers with a sound investment and an effortless transition from CD to DVD.

"Our customers wanted a solution that would give them the multimedia and storage capabilities of DVD-ROM as well as CD rewritability," said Maciek Brzeski, vice president, marketing, TAEC Disk Products Division. "The SD-R1002 CD-RW/DVD-ROM drive is the first of its kind to meet all of those needs, and underscores Toshiba's ability to deliver innovative, tailored solutions to our customers."

Brought Together Through Toshiba Innovation
As a leader in optical storage products, Toshiba leverages its technology expertise to bring the SD-R1002 drive to market. The drive combines key technologies from CD-RW and DVD-ROM including lasers and LSIs from both, as well as a combination pick-up head. For easy set up and compatibility, the SD-R1002 drive has an ATAPI interface.

The SD-R1002 drive is built to give the best performance for data, multimedia and storage environments. The drive reads CD-RW/CD-R media, which has a capacity of 650MB and can also read DVD-ROM software, which has a maximum capacity of 17GB per disc. The drive also features a fast writing speed of 4X for CD-R and CD-RW, and employs a full 24X speed maximum playback for CD-ROM and 4X for DVD-ROM.

Designed to Satisfy Today's Needs and Tomorrow's Demands
Toshiba's new CD-RW/DVD-ROM drive was designed to provide customers with an easy way to transition from CD to DVD while satisfying the demand for local backup, cost-effective data archiving and data interchange. Because the SD-R1002 drive uses universal technology, it is compatible across portable computers, desktop systems, workstations and servers. In addition, optical recording offers a low cost per megabyte, the longest archive life of any media and is highly durable. Also, it adheres to the DVD Forum's DVD-ROM specifications.

"CD-RW and DVD-ROM are poised to be two of the fastest growing technologies over the next few years," said John Freeman, president, Strategic Marketing Decisions. "Today, users have to choose between CD-RW writability or DVD-ROM compatibility. A product that gives them the functionality of both technologies should be very well received by the market."

For increased storage capacities, heightened video and audio playback and faster access to data, DVD-ROM is the obvious choice. Some of the most popular applications for DVD-ROM are gaming, interactive software, software distribution and data storage. DVD-ROM drives are backward compatible with all CD technology and have a planned growth path that will lead to future generations of DVD products to support users' needs well into the future.

CD-RW provides users with a cost-effective way to record and playback digital quality sound and video, or to rewrite and backup data onto CD-RW or CD-R media. These drives satisfy many individual and business needs such as software distribution, back-up, recording or playing personalized CD-audio disks and running CD-ROM applications. Like DVD-ROM, CD-RW is a sound investment because of its compatibility with CD-R and CD-ROM. CD-RW and CD-R media can also be read by other CD-ROM drives, making it a viable replacement for floppy drives.

The SD-R1002 is a half-height drive that fits into all standard desktop computer drive bays. The drive measures 146mm (w) x 41.5mm (h) x 193mm (d).

Pricing and Availability
The SD-R1002 drive will be sold primarily to value-added resellers, system integrators and distributors. The drives are available now in sample quantities and will begin shipping in volume in February. Pricing is not available at this time.

The drive will also be available as part of a kit which will include supporting hardware and software. The kit will be available in February. Suggested list price of the SD-R1002 kit will be less than $400.

Disk Products Division
TAEC Disk Products Division leads the market in the development, design and manufacturing of DVD-RAM, DVD-ROM and CD-ROM and CD-RW drives and 2.5-inch hard disk drives. The Disk Products Division markets high quality peripherals to original equipment manufacturers, value-added resellers, value-added dealers, systems integrators and distributors in the United States. Inherent in the company's product line is the high-quality engineering and manufacturing which has established Toshiba products as worldwide leaders.

About Toshiba
Toshiba America Electronic Components, Inc. (TAEC) is the North American design, manufacturing, marketing and sales arm of Toshiba Corporation, a global technology innovator. TAEC is recognized as a leading supplier of semiconductor, electronic component and storage solutions. The company delivers technology solutions that enable OEMs to develop advanced integrated products for the computing, networking, communications and digital consumer markets. In fact, its technology offerings account for more than 30 percent of the total possible components used in desktop and portable computers. By continuing to develop leading-edge solutions that cost-effectively meet the emerging needs of the design engineering community, TAEC keeps its customers in touch with tomorrow. For additional information, please visit TAEC's web site at, http://www.diskproducts.toshiba.com

Agency Contact:

Lisa Landry
The Benjamin Group Inc.
(714) 245-7500
lisa_landry@benjamingroup.com

Back to top

  © 2003 Toshiba America Inc. | Terms of Use | Privacy Statement