layout.gif




   
 Notify me about future
    product information


 

 

 
FOR IMMEDIATE RELEASE

January 22, 2001 

TOSHIBA INTRODUCES 2.5-INCH HDD FAMILY WITH INDUSTRY'S HIGHEST AREAL DENSITY AND 15GB PER PLATTER CAPACITY

New HDD Family Brings the Ideal Storage Capacities at the Right Time for Consumer, Commercial and Non-PC Applications


IRVINE, Calif, Toshiba America Electronics Components (TAEC), Storage Device Division today announced its newest family of industry-leading 2.5-inch hard disk drives (HDDs) in 15GB and 30GB capacities, offering the industry's highest areal density per platter at 26.7 gigabits per square inch. The new line of HDDs provides higher-capacity storage options for a range of mobile PC and non-PC applications.

"Our new generation of super-slim 2.5-inch HDDs enables computer users to keep pace with the latest applications and computer functionality, while maintaining portability," said Amy Lian, director of Toshiba's HDD business unit. "Today's market requires 2.5-inch HDD technology that offers an increasingly mobile society the ability to use complex data, business graphics and audio visual applications, as well as digital photos, music and video in a mobile environment."

Storage Products for the New Economy
Toshiba's new 30GB (MK3017GAP) and 15GB (MK1517GAP) HDDs are 9.5mm high with interfaces that are ATA-5 compliant to support high transfer rates of 100 megabytes per second. Both the 15GB and 30GB HDDs can withstand an operational shock of up to 175g and non-operating shock of up to 800g.

At 30GB, Toshiba's new family offers enough capacity for portable video recording and editing, with lower power consumption compared to traditional 3.5-inch HDDs. This functionality provides ideal storage for a range of commercial and consumer notebooks, as well as non-PC applications such as PDAs, printers, copiers, GPS systems and MP3 players.

Toshiba achieved this industry-leading per platter areal density using proprietary technology that provides greater capability for reading information on the drive. This rugged design and reliability has enabled Toshiba to deliver the right capacities to meet today's diverse range of storage needs for both commercial and consumer PC applications, as well as the full range of non-PC applications.

Toshiba SDD will begin shipping samples of the 30GB MK3017GAP and 15GB MK1517GAP HDDs in February.

Product outlines: 2.5 -inch HDD
Model No.
MK3017GAP
MK1517GAP
Capacity
30.0GB
15.1GB
No. of disks
2
1
No. of heads
4
2
Average seek time
13ms
Data transfer rate
100MB/sec
Rotational speed
4,200 rpm
Buffer memory
2,048 KB
Interface
ATA-5
Dimensions(WxDxH)
69.85x100 x 9.5mm
Weight
99g (Max.)
94g (Max.)
Shock resistance
Operating:1,715 m/2 (175g)
Non-operating:7,840 m/s2 (800g)

Storage Device Division
TAEC Storage Device Division leads the market in the development, design and manufacturing of DVD-RAM, DVD-ROM, combination CD-RW/DVD-ROM and CD-ROM drives and 1.8- and 2.5-inch hard disk drives. Toshiba SDD markets high-quality peripherals to original equipment manufacturers, value-added resellers, value-added dealers, systems integrators and distributors in the United States. Inherent in the company's product line is the high-quality engineering and manufacturing that has established Toshiba products as worldwide leaders.

About Toshiba
Toshiba America Electronic Components (TAEC), recognized as one of the largest suppliers of semiconductor, electronic component and storage solutions, is the North American engineering, manufacturing, marketing and sales arm of Japan's Toshiba Semiconductor Company and Toshiba Display Devices and Components Company. The Toshiba Semiconductor Company is one of the world's leading manufacturers and suppliers of semiconductor products including LSIs, microprocessors and controllers, and advanced memory products, in addition to discrete and analog peripheral components. TAEC is also responsible for sales and marketing of other major electronic components including liquid crystal displays, color display and picture tubes, lithium-ion and other secondary batteries. For additional information, please visit TAEC's web site at http://www.toshiba.com/taec


Back to top

  © 2003 Toshiba America Inc. | Terms of Use | Privacy Statement