|
FOR IMMEDIATE RELEASE
August 22, 2001
TOSHIBA INTRODUCES MULTI-READ OPTICAL STORAGE PRODUCTS TO MEET
DIVERSE RANGE OF CONSUMER AND BUSINESS MOBILE COMPUTING NEEDS
Storage
technology leader increases mobile computer functionality with new
slim-line drives that read multiple formats
IRVINE, Calif,
Toshiba America Electronic Components (TAEC), Storage Device Division
(SDD) today announced the upgrade of its industry leading slim-line
combination CD-RW/DVD-ROM product and the introduction of DVD-ROM
drives with DVD-RAM media read capabilities. These new optical introductions
are designed to meet the array of consumer and business storage
applications required for today's multimedia computing environment.
Toshiba was
the first storage supplier to introduce a slim-line combination
CD-RW/DVD-ROM product, which is now available with a fast-writing
speed of 8X for CD-R/CD-RW when high-speed CD-RW media is used and
8X read for DVD-ROM. With the addition of DVD-RAM media read to
its line of DVD-ROM drives, Toshiba is providing its customers with
drives that read multiple DVD media types to best meet the needs
of the mobile computer user .
“Ultimately
computer users will decide which storage medium works for their
unique applications," said Maciek Brzeski, vice president of marketing
at Toshiba SDD. "Since consumer and business users have very different
requirements, our focus is to furnish mobile computer manufacturers
with the right storage solutions to meet their customers' diverse
needs.”
Toshiba's DVD-ROM
with DVD-RAM media read drives enable the business user to access
large DVD-RAM back-up files on their mobile systems, while the slim
combination drive creates the benefits of both rewritable CD and
the ability to read DVD media in a mobile environment. Given the
space constraints in a notebook computer, the combination drive
provides a cost-effective option to write and share CD files, while
also allowing users to enjoy DVD movies or access large DVD data
files and resource software.
The SD-R2102
slim-line combination drive begins shipping in August. The SD-C2512
slim-line DVD-ROM with DVD-RAM media read is currently available
in volume production to mobile PC manufacturers .
Toshiba SDD will begin mass production of the new HDD family in July.
Product
outline: SD-R2102
(CD-R 8X; CD-RW 8X when high-speed CD-RW media is used; CD-ROM 24X;
DVD 8X)
| Applicable
Disc Formats |
Applicable
Write Disc CD-R, CD-RW: CD-DA, CD+(E)G, CD-MIDI, CD-ROM,
CD-ROM, XA, CD-TEXT, MIXED MODE CD, CD-I, CD-1 Bridge (Photo-CD,
Video-CD), Multisession CD (Photo-CD, CD-EXTRA, Portfolio)
Applicable
Read Disc DVD: DVD-ROM (DVD-5, DVD-9, DVD-10, DVD-18),
DVD-R*
Applicable
Read Disc CD: CD-DA, CD+(E)G, CD-MIDI, CD-TEXT, CD-ROM,
CD-ROM XA, MIXED MODE CD, CD-I, CD-I Bridge (Photo-CD, Video
CD), Multisession CD (Photo-CD,CD-EXTRA, Portfolio, CD-R,
CD-RW), CD-R, CD-RW
*does
not support CPRM
|
| Interface |
ATAPI |
| ATAPI
|
DVD-ROM:
115ms
CD-ROM:
105ms
|
| Continuous
Data Transfer Rate |
CD-R/RW
(write): 1,200KB/sec max (8X)
DVD-ROM: 10,820KB/sec max (8X)
CD-ROM: 3,600KB/sec max (24X) |
| Buffer
Capacity |
2MB |
| MTBF |
60,000
hours |
Product
outline: SD-C2512
8X DVD-ROM with DVD-RAM Media Read (DVD-ROM 8X; DVD-RAM 2X; CD-ROM
24X)
| Applicable
Disc Formats |
DVD:
DVD-ROM (DVD-5, DVD-9, DVD-10, DVD-18), DVD-R*, DVD-RAM (Supports
12 cm 2.6GB/4.7GB and 8 cm 1.4GB DVD-RAM media)
CD:
CD-DA, CD+(E)G, CD-MIDI, CD-TEXT, CD-ROM, CD-ROM XA, CD-I,
CD-I Bridge (Photo-CD, Video-CD), Multisession CD (Photo-CD,
CD-EXTRA, CD-R, CD-RW)CD-R (read), CD-RW (read)
*does
not support CPRM
|
| Interface |
ATAPI |
| ATAPI
|
DVD-ROM:
95ms
CD-ROM:
90ms
DVD-RAM:
120ms
|
| Continuous
Data Transfer Rate |
DVD-ROM
: 10,820KB/sec max (8X)
CD-ROM: 3,600KB/sec max (24X)
DVD-RAM: 2,704KB/sec max (2X) |
| Buffer
Capacity |
512KB |
| MTBF |
60,000
hours |
Toshiba Storage
Device Division
TAEC Storage
Device Division (SDD) leads the market in the development, design
and manufacturing of DVD-RAM, DVD-ROM, slim CD-R/RW, combination
CD-RW/ DVD-ROM, 1.8-inch hard disk drives and 2.5-inch hard disk
drives. Toshiba SDD markets high-quality peripherals to original
equipment manufacturers, value-added resellers, value-added dealers,
systems integrators and distributors in the United States. Inherent
in the company's product line is the high-quality engineering and
manufacturing that has established Toshiba products as worldwide
leade.
About TAEC
TAEC offers the
industry's broadest line-up of semiconductor, display and storage
solutions for the computing, wireless, networking and digital consumer
markets. Combining quality and flexibility with design engineering
expertise, TAEC brings advanced next-generation technologies to
its OEM customers.
TAEC is an independent
operating company owned by Toshiba America Inc., a subsidiary of
the $54 billion (FY 1999 recorded sales) Toshiba Corp., the second
largest semiconductor company worldwide in terms of global sales
for the year 2000. Toshiba Corp. is a world leader in high-technology
products with more than 300 major subsidiaries and affiliates worldwide.
For additional company and product information, please visit TAEC's
Web site at chips.toshiba.com.
For technical inquiries, please email Tech.Questions@taec.toshiba.com.
Back to top
|