|
FOR IMMEDIATE RELEASE
Released: November 12, 2001
Updated: February 11, 2002
TOSHIBA UPGRADES PERFORMANCE OF ITS POPULAR DESKTOP COMBINATION
CD-RW/DVD-ROM AND MOBILE CD-R/RW DRIVES Increased
speeds provide customers with new storage capabilities for today’s
demanding computing applications
IRVINE, Calif,
Toshiba Storage Device Division (SDD) today announced performance
upgrades for its popular desktop combination CD-RW/DVD-ROM drive as
well as its super-slim CD-R/RW drive for mobile computer systems.
The enhanced capabilities provide OEM customers and end users with
greater functionality for the growing range of computer applications
that require solid storage solutions.
The SD-R1202 combination drive, ideally suited for integration in
or as an upgrade to desktop PCs, increases PC functionality with the
faster speeds for file sharing, CD writing and DVD playback. The new
combination drive provides maximum write speeds of 16x for
CD-R and 10x for CD-RW, with maximum read speeds of 12x for DVD-ROM
and 40x for CD-ROM.
"Because Toshiba’s combination drive allows end users to
determine their choice of media, they can experience the benefits of
both CD writing and DVD playback technologies," said Maciek
Brzeski, vice president of marketing at Toshiba SDD. "The drive’s
improved performance enables users to access, read and write files
faster than ever before."
Toshiba also has upgraded one of its newest slim-line family
members, a mobile CD-RW offering. The new SR-C8102 CD-R/RW drive
weighs only 197g, measures 12.7mm high and achieves a maximum 16x
write speed for CD-R – the highest rate yet achieved in a built-in
super-slim CD-R/RW drive. The drive offers a maximum 10x write speed
for CD-RW and a maximum 24x read speed for CD-ROM.
"People are using their mobile computers more often for
advanced applications, from editing video to recording music – a
trend that demands high-speed storage performance," Brzeski
said. "This upgraded drive provides the speed users need to
keep up with their multimedia applications."
Toshiba will begin shipping the SD-R1202 desktop combination
drive in March and the SR-C8102 slim-line CD-R/RW drive in
mid-December.
Specification
Outline
| Model |
CD-R
Write |
CD-RW
Write |
CD-ROM
Read |
DVD-ROM
Read |
Interface |
|
SD-R1202 |
Max
16X |
Max
10X |
Max
40X |
Max
12X |
ATAPI |
| SR-C8102 |
Max
16X |
Max
10X |
Max
24X |
-- |
ATAPI |
Product Specification
Details
| Model Name |
SD-R1202 |
SR-C8102 |
| Supported Disc
Formats |
Read:
DVD-ROM, DVD-R, DVD-RW, DVD-DA, CD+(E)G, CD-MIDI, CD-TEXT,
CD-ROM XA, MIXED MODE CD, CD-I, CD-I Bridge (Photo-CD,
Video-CD), Multi-session CD (Photo-CD, CD-EXTRA, Portfolio,
CD-R, CD-RW, High Speed CD-RW)
Write:
CD-R, CD-RW, High-Speed CD-RW
|
Read:
CD-DA, CD+(E)G, CD-MIDI, CD-TEXT, CD-ROM, CD-ROM XA, MIXED
MODE CD, CD-I, CD-I Bridge (Photo-CD, Video-CD), Multi-session
CD (Photo-CD, CD-EXTRA, Portfolio, CD-R, CD-RW, High Speed CD-RW)
Write:
CD-R, CD-RW, High-Speed CD-RW
|
| Interface |
ATAPI |
| Average Random
Seek Time |
DVD-ROM:
140ms (Typ)
CD-ROM: 105ms (Typ) |
105ms
(Typ) |
| Data
Transfer Rate |
Read:
DVD-ROM: 16,200KB/sec Max (12X)
CD-ROM: 6,000KB/sec Max (40X)
Write:
CD-R: 2,400KB/sec Max (16X)
High-Speed CD-RW: 1,500KB/sec Max (10X)
|
Read:
CD-ROM: 3,600KB/sec Max (24X)
Write:
CD-R: 2,400KB/sec Max (16X)
High-Speed CD-RW: 1,500KB/sec Max (10X)
|
| Buffer Capacity |
2MB |
| Power
Consumption |
DVD-ROM: 7.4W
CD-ROM: 8.8W |
4.2W |
| Power Source |
+5V, +12V |
+5V |
| MTBF |
100,000 hours |
60,000 hours |
| Operating Temperature |
5
- 50°C (excluding media) |
External
Dimensions
(W x H x D) |
5.7"
x 1.6" x 7.6"
(146mm x 41.5mm x
193mm) |
5.04"
X 0.5" X 4.96"
(128mm x 12.7mm x 126.1mm) |
| Weight |
2.03lbs
(0.92kg) |
6.95
ounces (197g) |
About
Toshiba Storage Device Division
Toshiba SDD, a division of Toshiba America Information Systems,
Inc., leads the market in the development, design and manufacturing
of DVD-ROM, DVD-RAM, slim CD-R/RW, combination CD-RW/DVD-ROM,
1.8-inch hard disk drives and 2.5-inch hard disk drives. Toshiba SDD
markets high-quality peripherals to original equipment
manufacturers, value-added resellers, value-added dealers, systems
integrators and distributors in the United States. Inherent in the
company’s product line is the high-quality engineering and
manufacturing that has established Toshiba products as worldwide
leaders. For more information, visit www.sdd.toshiba.com.
About Toshiba America Information Systems, Inc.
Headquartered in Irvine, Calif., with annual sales of
approximately $2.5 billion, Toshiba America Information Systems,
Inc. is comprised of six divisions organized into two business
groups, which manufacture, market and service a wide range of
business and information-oriented products in the United States and
Latin America. Products include portable and desktop computers, PC
servers and storage subsystems; voice-mail systems; digital business
telephone systems; interactive voice-response systems; network
systems and digital cameras. TAIS is an independent operating
company owned by Toshiba America Inc., a subsidiary of the $52
billion Toshiba Corp., the eighth-largest computer and electronics
company and the world’s 26th largest industrial corporation in
terms of sales. Toshiba Corp. is a world leader in high-technology
products with more than 300 major subsidiaries and affiliates
worldwide.
Back to top
|