|
FOR IMMEDIATE RELEASE
Initial Release: January 16, 2002
Revised: September 13, 2002
TOSHIBA INTRODUCES WORLD’S HIGHEST CAPACITY
1.8-INCH HARD DISK DRIVES
10GB And 20GB Embedded Drives Power Consumer, Commercial And PC Applications
IRVINE,
Calif, Toshiba Storage Device Division (SDD) continues its
leadership in the hard drive industry by today announcing its newest
family of 1.8-inch embedded hard disk drives (HDDs) available in
10GB and 20GB capacities. The new mini drives offer consumer
electronics and PC manufacturers the right combination of
high-capacity storage with a compact, lightweight footprint for
design into a wide variety of mobile and handheld products that
require reliable storage solutions.
The tiny storage giants measure
54 mm wide and 78.5 mm deep, and weigh 51 and 62 grams respectively.
Toshiba’s new 10GB (MK1003GAL) and 20GB (MK2003GAH) HDDs are
smaller than a credit card and lighter than a traditional pager. The
low-profile, lightweight drives offer data transfer rates of
100MB/sec, providing high-speed performance for both consumer
electronics devices and notebook PCs.
"Our latest 1.8-inch HDD
technology is enabling some of today’s most exciting, new small
form factor mobile devices," said Amy Dalphy, manager, HDD
business unit, Toshiba SDD. "Toshiba’s 1.8-inch HDDs have the
right mix of power consumption, shock tolerance and compact size for
today’s capacity-hungry ‘biz-sumer’ mobile computing and
digital gadgets – such as music players, handheld PCs, PDAs,
wearable computers and laptops."
Built on Toshiba’s proven
2.5-inch HDD technology platform, the rugged design and reliability
of Toshiba’s new 1.8-inch HDDs meets today’s increasingly
diverse range of storage needs for a variety of new applications and
environments. The drives can be easily designed and integrated into
portable PCs, handheld mobile terminals, wearable computers, digital
video cameras, automotive applications and audio/video players. In
addition, Toshiba’s 1.8-inch HDD technology enables the use of
complex data, business graphics and audio/visual applications for
the growing mobile market, and enables PDA manufacturers to provide
substantial photo archiving capabilities in their products.
Offering the industry’s highest
areal density per platter in this form factor at 35.26 gigabits per
square inch – and withstanding operational shock of up to 200g and
non-operating shock of up to 1000g – the 20GB HDD will begin
shipping in early February, while the 10GB will ship in early March.
Toshiba’s HDD products can be ordered through industrial
distributors, or for additional information please visit http://www.harddrives.toshiba.com.
Product Outlines: 1.8-inch 10GB
and 20GB HDDs
|
Model no. |
MK1003GAL |
MK2003GAH |
|
Capacity |
10GB |
20GB |
|
No. of platters |
1 |
2 |
|
No. of heads |
2 |
4 |
|
Average seek time |
15ms |
15ms |
|
Data transfer rate |
100MB/sec |
100 MB/sec |
|
Rotational speed |
4,200rpm |
4,200rpm |
|
Voltage |
3.3V |
3.3V |
|
Power consumption |
1.4W |
1.4W |
|
Energy consumption efficiency |
.04W/GB |
.02W/GB |
Dimensions
(WxDxH)
|
54 x 78.5 x 5 mm |
54 x 78.5 x 8 mm |
|
Weight |
51g |
62g |
|
Buffer memory |
512KB |
512KB |
|
Interface |
ATA-5 |
ATA-5 |
|
Shock
Operating
Non-Operating |
1,960 m/s2
(200g)
9,800 m/s2 (1000g)
|
1,960 m/s2
(200g)
9,800 m/s2 (1000g)
|
About
Toshiba Storage Device Division
Toshiba
SDD, a division of Toshiba America Information Systems, Inc., leads
the market in the development, design and manufacturing of DVD-ROM,
DVD-RAM, slim CD-R/RW, combination CD-RW/DVD-ROM, 1.8-inch hard
disk drives and 2.5-inch hard disk drives. Toshiba SDD markets high-quality
peripherals to original equipment manufacturers, value-added resellers,
value-added dealers, systems integrators and distributors in the
United States. Inherent in the company’s product line is the high-quality
engineering and manufacturing that has established Toshiba products
as worldwide leaders. For more information, visit www.sdd.toshiba.com.
About Toshiba
America Information Systems, Inc.
Headquartered
in Irvine, Calif., with annual sales of approximately $2.5 billion,
Toshiba America Information Systems, Inc. is comprised of six divisions,
organized into two business groups, which manufacture, market and
service a wide range of business and information-oriented products
in the United States and Latin America. Products include portable
and desktop computers, PC servers and storage subsystems; voice-mail
systems; digital business telephone systems; interactive voice-response
systems; network systems and digital cameras. TAIS is an independent
operating company owned by Toshiba America Inc., a subsidiary of
the $52 billion Toshiba Corp., the eighth-largest computer and electronics
company and the world’s 26th largest industrial corporation in terms
of sales. Toshiba Corp. is a world leader in high-technology products
with more than 300 major subsidiaries and affiliates worldwide.
Back to top
|