|
FOR IMMEDIATE RELEASE
February 6, 2002
Revised: March 14, 2002
Revised: June 12, 2002
TOSHIBA INTRODUCES THE FIRST 5400 RPM 2.5-INCH HDD FAMILY WITH INDUSTRY-LEADING
AREAL DENSITY IN 9.5mm
High-Capacity
HDDs Feature FDB Technology In 30GB And 40GB Capacities
IRVINE,
Calif, Toshiba's Storage Device Division (SDD), the industry pioneer
in small form factor, high-capacity hard disk drives (HDDs), today
announced the industry's first 9.5mm 5400 RPM drive family. This
new family offers high-speed 2.5-inch HDDs in 30GB and 40GB
capacities. Featuring the industry's highest areal density at 34.7
gigabits per square inch, the new drives provide 5400 RPM motor
speed, which improves system-level performance by as much as 12
percent* when compared to 4200 RPM drives.
The 2.5-inch
hard disk drives are 9.5mm high and support fast data transfer rates
and seek times allowing users to access more data in less time.
Their high capacity and technical performance capabilities are well
suited to accommodate a spectrum of storage applications, including
portable video recording and editing, large graphics files and other
multimedia applications.
These drives are
also ideal for multi-functional mobile PCs and non-PC applications
such as telecommunications, printers, copiers, GPS systems and MP3
players. For example, at 40GB, Toshiba's HDD offers enough capacity
and performance for portable video recording and editing, with lower
power consumption when compared to traditional 3.5-inch HDDs.
Toshiba's new
drives also feature fluid dynamic bearing (FDB) motor technology,
which has been especially popular with PC OEMs looking to reduce
ambient drive noise in mobile computing applications. This technology
combined with the 5400 RPM rotational speed noticeably improves
mobile computing system performance. Toshiba also offers a line
of 2.5-inch 4200 RPM hard drives - first introduced last June -
with both FDB and ball bearing motors. The range of offerings within
a single HDD family means Toshiba customers enjoy the most secure
supply source and latest technologies available in the 2.5-inch
form factor.
"These exciting
new products offer a real performance boost that will be very noticeable
to the end customer," said Amy Dalphy, manager, HDD business unit,
Toshiba SDD. "Higher rotational speeds deliver a significant computing
improvement by reducing the amount of wait time the user experiences.
These drives also contribute more value to our direct customers
by offering a full family that provides performance differentiation
at the system level."
Toshiba's new
HDD family offers capacities in 40GB (MK4019GAX)
and 30GB (MK3019GAX) in an ATA-5 compliant interface to support
high transfer rates of 100MB/sec. The robust HDDs can withstand
operational shock of up to 200g and non-operating shock of up to
800g, and will begin shipping in May.
Toshiba's HDD
products can be ordered through industrial distributors, or for
additional information please visit www.harddrives.toshiba.com.
Product Outline:
2.5-Inch HDD
|
MK3019GAX
|
MK4019GAX
|
| Capacity |
30GB
|
40GB
|
| Platters |
2
|
2
|
| Heads |
3
|
4
|
| Average
seek time |
12ms
|
| Data
transfer rate |
Ultra
DMA/100
|
| Rotational
speed |
5,400
RPM
|
| TPI |
57.1K
|
| BPI |
607K
(max)
|
| Voltage |
5V
|
| Power
consumption |
R/W:
2.5W
Low Power Idle: 0.85W
|
| Energy
consumption |
0.028
W/GB
|
0.021
W/GB
|
| Buffer
memory |
16MB
|
| Interface
|
ATA-5
|
| Dimensions
(WxDxH) |
70
x 100 x 9.5 (mm)
|
| Weight |
102g |
102g |
| Shock
resistance |
Operating:
1,960 m/s2 (200G)
Non-operating: 7,840 m/s2 (800G)
|
| Acoustic
noise |
Idle:
27 dB
Seek: 33 dB
|
About
Toshiba Storage Device Division
Toshiba SDD, a division of Toshiba America Information
Systems, Inc., leads the market in the development, design and
manufacturing of DVD-ROM, DVD-RAM, slim CD-R/RW, combination CD-RW/DVD-ROM,
1.8-inch hard disk drives and 2.5-inch hard disk drives. Toshiba
SDD markets high-quality peripherals to original equipment manufacturers,
value-added resellers, value-added dealers, systems integrators
and distributors in the United States. Inherent in the company's
product line is the high-quality engineering and manufacturing
that has established Toshiba products as worldwide leaders. For
more information, visit www.sdd.toshiba.com.
About Toshiba
America Information Systems, Inc.
Headquartered
in Irvine, Calif., Toshiba America Information Systems, Inc. (TAIS)
is comprised of multiple divisions that provide computer, communications
and imaging products and services. Products include industry leading
portable computers, PDAs, mobile computing accessories, servers,
including communications and portable servers, storage subsystems,
cable modems, digital business telephone systems, voice-mail, digital
cameras, security systems, and projectors. TAIS provides sales,
marketing, services and manufacturing for its wide range of information
products in the United States and Latin America. TAIS is an independent
operating company owned by Toshiba America, Inc., a subsidiary of
Toshiba Corporation, which is a world leader in high technology
and integrated manufacturing of electrical and electronic components,
products and systems. Toshiba has global sales of over $50 billion
and more than 300 subsidiaries and affiliates worldwide.
Back to top
|