|
FOR IMMEDIATE RELEASE
April 09, 2002
TOSHIBA INTRODUCES INDUSTRY'S FIRST 30GB PER PLATTER 2.5-INCH HARD
DISK DRIVE FAMILY
Technology
Leader Further Demonstrates Storage Expertise, Advancing Areal Density
To Deliver 60GB HDD
IRVINE, Calif,
Toshiba's Storage Device Division (SDD), the industry pioneer in
small form factor, high-capacity hard disk drives (HDDs), today
announced a 60GB 2.5-inch drive - the first 2.5-inch HDD product
based on a 30GB per platter design. Toshiba was first to market
for the past three generations with 10GB, 15GB and 20GB per platter
products. The new 30GB per platter product marks the fourth generation
of areal density leadership in the 2.5-inch 9.5mm form factor, delivering
the industry's highest areal density at 48.8 gigabits per square
inch.
The new drive
supports fast transfer rates and seek times, allowing users to access
more data in less time. Ideal for multi-functional mobile PCs and
non-PC applications such as telecommunications, printers, copiers,
GPS systems and MP3 players, the new 60GB dual platter drive provides
manufacturers with an abundance of capacity and performance in a
compact form factor.
"Toshiba's
customers have come to rely on our consistency, reliability and
first-to-market delivery," said Amy Dalphy, manager, HDD business
unit, Toshiba SDD. "Market-leading areal density and overall product
leadership is what customers expect and receive from Toshiba's storage
portfolio."
The new HDD
line offers 60GB (MK6021GAS) capacity in an ATA-5 compliant interface,
supporting high transfer rates of 100MB/sec. The robust HDD can
withstand operational shock of up to 200g and non-operating shock
of up to 800g, and will begin shipping in late May.
With the introduction
of lead-free soldering and halogen-free printed circuit boards on
all new hard disk drives produced by Toshiba, the environmentally
conscious can be reassured of Toshiba's commitment to the global
environment.
Toshiba's HDD
products can be ordered through industrial distributors, or for
additional information please visit www.harddrives.toshiba.com.
| Model |
MK6021GAS
|
| Capacity |
60GB
|
| Platters |
2
|
| Heads |
4
|
| Average
seek time |
12ms
|
| Data
transfer rate |
Ultra
DMA/100
|
| Rotational
speed |
4,200
RPM
|
| TPI |
78.9K
|
| BPI |
618K
(max)
|
| Voltage |
5V
|
| Power
consumption |
R/W:
2.3W
Low Power Idle: 0.70W
|
| Energy
consumption |
0.012
W/GB
|
| Buffer
memory |
2MB
|
| Interface
|
ATA-5
|
| Dimensions
(WxDxH) |
70
x 100 x 9.5 (mm)
|
| Weight |
99g
|
| Shock
resistance |
Operating:
1,960 m/s2 (200G)
Non-operating: 7,840 m/s2 (800G)
|
| Acoustic
noise |
Idle:
24 dB
Seek: 31 dB
|
About Toshiba
Storage Device Division
Toshiba
SDD, a division of Toshiba America Information Systems, Inc., leads
the market in the development, design and manufacturing of DVD-ROM,
DVD-RAM, slim CD-R/RW, combination CD-RW/DVD-ROM, 1.8-inch hard
disk drives and 2.5-inch hard disk drives. Toshiba SDD markets high-quality
peripherals to original equipment manufacturers, value-added resellers,
value-added dealers, systems integrators and distributors in the
United States. Inherent in the company's product line is the high-quality
engineering and manufacturing that has established Toshiba products
as worldwide leaders. For more information, visit www.sdd.toshiba.com.
About Toshiba
America Information Systems, Inc.
Headquartered in Irvine, Calif., Toshiba America Information Systems,
Inc. (TAIS) is comprised of multiple divisions that provide computer,
communications and imaging products and services. Products include
industry leading portable computers, PDAs, mobile computing accessories,
servers, including communications and portable servers, storage
subsystems, cable modems, digital business telephone systems, voice-mail,
digital cameras, security systems, and projectors. TAIS provides
sales, marketing, services and manufacturing for its wide range
of information products in the United States and Latin America.
TAIS is an independent operating company owned by Toshiba America,
Inc., a subsidiary of Toshiba Corporation, which is a world leader
in high technology and integrated manufacturing of electrical and
electronic components, products and systems. Toshiba has global
sales of over $50 billion and more than 300 subsidiaries and affiliates
worldwide.
Back to top
|