layout.gif




   
 Notify me about future
    product information


 

 

 
FOR IMMEDIATE RELEASE

September 30, 2002
Revised: October 11, 2002

TOSHIBA INTRODUCES INDUSTRY’S FIRST MOBILE PC DRIVE WITH BOTH DVD AND CD RECORDING CAPABILITIES

Mobile PC Users Can Create DVD Videos And CD Audio Files All With The Same Drive


IRVINE, Calif, Extending its leadership in developing optical storage products to meet evolving needs, Toshiba’s Storage Device Division (SDD) today announced two new combination drives that deliver DVD/CD recordability to notebook and desktop computers. Based on the DVD-R/RW format, Toshiba’s combination drives support the most widely compatible DVD standard, giving consumers the highest level of compatibility with legacy DVD devices.

Toshiba’s SD-R6012 slim combination drive – the industry’s first DVD/CD recordable drive for mobile computers – allows PC manufacturers to deliver unprecedented functionality to mobile computer users, providing both DVD and CD read and write capabilities. Until now, only desktop computers have had the luxury of DVD recordability for applications such as audio/video editing and personal digital compilations.

"Consumers are looking to create, edit, and burn both work-related and personal digital productions – on the fly and on the go," said Maciek Brzeski, vice president of marketing at Toshiba SDD. "Our new lightweight combination drive brings DVD recording to the mobile world, providing users with a stepping stone to move from CD to DVD technology for creating and storing family photos, files, videos and other memories people don’t want to lose."

The SD-R6012 slim drive supports writing DVD-R/RW at 1X, writing CD-R/RW at 16x/10x, and reads 8X DVD and 24X CD.

Toshiba Also Introduces Its First Desktop DVD Recordable Drive
Increasing the functionality of its popular desktop combination drive with the addition of DVD recording technology, Toshiba also introduced the SD-R5002 recordable drive today. Supporting read and write functionality for the DVD-R/DVD-RW/CD-R/CD-RW formats, the new desktop drive is compatible with the majority of legacy DVD players – enabling PC OEMs to build products that assure consumers of media compatibility when used with other DVD/CD systems.

The SD-R5002 desktop drive is also available as an upgrade kit, allowing consumers with existing desktop computers to add DVD recording functionality. The included industry-leading software provides for theater-quality movie viewing and burning of DVDs that contain personal videos and digital still image slide-shows. The software compilation includes:

  • Cyberlink PowerDVD – The leading software DVD player
  • Cyberlink PowerDirector Pro – Integrated personal movie-making solution
  • VOB Instant CD/DVD (InstantDisc, InstantBackup, InstantCopy, InstantWrite, InstantMusic, InstantVideo)

About Toshiba’s DVD Recordable Technology
Given the popularity of DVD and the evolution of recordable/rewritable formats for entertainment content, Toshiba’s new SD-R6012 slim drive and SD-R5002 desktop drive support two of the hottest trends driving the convergence of consumer electronics and computing – video and audio recording/editing. The combination drives are also a great stepping stone for users to dabble between CD and DVD media – all while providing the safety net of CD read and write technology.

Both DVD-R and DVD-RW formats are sanctioned by the DVD Forum. In addition, they are compatible with most legacy DVD players, while other formats may have compatibility issues with existing players. DVD-R/RW media is affordably priced at $5 and $10/disc respectively.

"DVD is expected to replace audio CD, videotape, laser disc and CD-ROM/RW technology, becoming the de facto standard for home entertainment and lifestyle computing," Brzeksi said. "Toshiba’s new combination drives provide customers with a sound investment to make an effortless transition from CD to DVD technology."

Availability
Toshiba’s slimline combination drive, SD-R6012, is an OEM product available to PC manufacturers now. In addition, the desktop combination drive upgrade kit (TSDR5002BK00000) is available through distribution or on www.shoptoshiba.com for $349. For additional information, please visit www.sdd.toshiba.com.

Specification Outline

Model

DVD-R
Read/Write

DVD-RW
Read/Write

DVD-ROM
Read

CD-R
Read/Write

CD-RW
Read/Write

CD-ROM
Read

SD-R5002

2x

1x

12x

16x

10x

40x

SD-R6012

1x

1x

8x

16x

10x

24x

 

Product Specification Details

Model name

SD-R5002 Desktop

SD-R6012 Slim

Supported Disc Formats

Read:
DVD-ROM, DVD-R, DVD-RW,
CD-DA, CD+(E)G, CD-MIDI, CD-TEXT, CD-ROM XA, MIXED MODE CD, CD-I, CD-I Bridge (Photo-CD, Video-CD),
Multi-session CD (Photo-CD, CD-EXTRA, Portfolio, CD-R, CD-RW), CD-R, CD-RW, High-Speed CD-RW

Write:
CD-ROM, CD-R, CD-RW, High-Speed CD-RW, DVD-ROM, DVD-R, DVD-RW

 

Interface

ATAPI

Average Random Seek Time

DVD: 130ms (Typ)
CD: 110ms (Typ)

DVD: 100ms (Typ)
CD: 95ms (Typ)

Write Performance

DVD-R (Ver. 2.0): 2X (CLV)
DVD-RW (Ver. 1.0): 1X (CLV)
CD-R : 16X (ZCLV)
CD-RW (High Speed): 10X (CLV)

DVD-R (Ver. 2.0): 1X (CLV)
DVD-RW (Ver. 1.0): 1X (CLV)
CD-R : 16X (ZCLV)
CD-RW (High Speed): 10X (CLV)

Read Performance

DVD-ROM (Single): 12X (CAV)
DVD-ROM (Dual): 8X (CAV)
DVD-R, DVD-RW: 4.8X (CAV)
CD-ROM, CD-R : 40X (CAV)
CD-RW: 20X (CAV)
CD-Audio Extraction: 16X (CAV)
Video-CD: 6X (PCAV)

DVD-ROM (Single): 8X (CAV)
DVD-ROM (Dual): 6X (CAV)
DVD-R, DVD-RW: 4X (CAV)
CD-ROM, CD-R : 24X (CAV)
CD-RW: 12X (CAV)
CD-Audio Extraction: 12X (CAV)
Video-CD: 6X (PCAV)

Buffer Capacity

2 MB

2 MB

MTBF

100,000 hours

60,000 hours

Mounting Orientation

Horizontal and Vertical

External Dimensions
(W x H x D)

146mm x 41.5mm x 193mm

128mm x 12.7mm x 126mm

Weight

1.0 kg

0. 2 kg

About Toshiba Storage Device Division
Toshiba SDD, a division of Toshiba America Information Systems, Inc., leads the market in the development, design and manufacturing of DVD-ROM, slim CD-R/CD-RW/DVD-R/DVD-RW, combination CD-R/CD-RW/DVD-R/DVD-RW, 1.8-inch hard disk drives and 2.5-inch hard disk drives. Toshiba SDD markets high-quality peripherals to original equipment manufacturers, value-added resellers, value-added dealers, systems integrators and distributors in the United States. Inherent in the company’s product line is the high-quality engineering and manufacturing that has established Toshiba products as worldwide leaders. For more information, visit www.sdd.toshiba.com.

 

About Toshiba America Information Systems, Inc.
Headquartered in Irvine, Calif., Toshiba America Information Systems, Inc. (TAIS) is comprised of multiple divisions that provide computer, communications and imaging products and services. Products include industry leading portable computers, PDAs, mobile computing accessories, servers, including communications and portable servers, storage subsystems, cable modems, digital business telephone systems, voice-mail, digital cameras, security systems, and digital projectors. TAIS provides sales, marketing, services and manufacturing for its wide range of information products in the United States and Latin America. TAIS is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation, which is a world leader in high technology and integrated manufacturing of electrical and electronic components, products and systems. Toshiba has global sales of over $40 billion and more than 300 subsidiaries and affiliates worldwide.

Back to top

  © 2003 Toshiba America Inc. | Terms of Use | Privacy Statement