| FOR IMMEDIATE RELEASE
Initial Release: October 3, 2002
TOSHIBA INTRODUCES INDUSTRY’S FIRST 60GB 5400 RPM SUPER SLIM 2.5-INCH HARD DRIVE
Mobile
Technology Leader Leverages Storage Expertise to Offer Higher RPM 60GB in 9.5mm
IRVINE, Calif,
Toshiba’s Storage Device Division (SDD), the industry pioneer in small form factor hard disk drives (HDDs), continued it’s leadership position today announcing the industry’s first 60GB, 5400 RPM drive in a 9.5mm form factor. Providing this level of performance and capacity in a slim design enables mobile manufacturers to upgrade their customers’ usage experience with faster and thinner computing and entertainment devices.
Toshiba’s 5400 RPM 60GB hard drive allows users to access more data in less time – significantly improving system level performance. With an areal density of 49.8 gigabits per square inch, 60GB is achieved with two platters in the 9.5mm package. Toshiba’s hard drive family is well suited to accommodate the storage needs of multi-functional mobile PCs and non-PC applications – such as telecommunications, printers, copiers and MP3 players.
“Toshiba continues to power the mobile revolution, raising the bar again for storage performance,” said Amy Dalphy, manager, HDD business unit, Toshiba SDD. “For PC and consumer electronics manufacturers, this drive unleashes optimized performance, capacity and form factor for the next generation of mobile computers and other small digital devices.”
Toshiba’s new 60GB
(MK6022GAX) contains an ATA-5 compliant interface to support high transfer rates
of 100MB/second and can withstand operational shock of up to 200G and
non-operating shock of up to 800G. The new HDDs are shipping now.
Toshiba’s HDD products
can be ordered through distribution, or for additional information, please visit
www.harddrives.toshiba.com.
Product
Outline: 2.5-Inch HDD
| |
MK6022GAX |
| Capacity |
60GB |
| Platters |
2 |
| Heads |
4 |
| Average
Seek Time |
12ms |
| Data
Transfer Rate |
Ultra
DMA/100 |
| Rotational
Speed |
5400
RPM |
| TPI |
78.9K |
| BPI |
632K
(max) |
| Voltage |
5V |
| Power
Consumption |
R/W:
2.5W
Low Power Idle: 0.85W |
| Energy
Consumption |
0.014
W/GB |
| Motor
technology |
Fluid
Dynamic Bearing (FDB) |
| Buffer
memory |
16MB |
| Interface |
ATA-5 |
| Dimensions
(WxDxH) |
69.85
x 100 x 9.5 (mm) |
| Weight |
102g |
| Shock
resistance |
Operating:
1,960 m/s2 (200G)
Non-operating: 7,840 m/s2 (800G) |
| Acoustic
noise |
Idle:
26 dB
Seek: 33 dB |
About Toshiba Storage Device Division
Toshiba SDD, a division of Toshiba America Information Systems, Inc., leads the market in the development, design and manufacturing of DVD-ROM, slim CD-R/RW, combination CD-RW/DVD-ROM, 1.8-inch hard disk drives and 2.5-inch hard disk drives. Toshiba SDD markets high-quality peripherals to original equipment manufacturers, value-added resellers, value-added dealers, systems integrators and distributors in the United States. Inherent in the company’s product line is the high-quality engineering and manufacturing that has established Toshiba products as worldwide leaders. For more information, visit
www.sdd.toshiba.com.
About Toshiba America Information Systems, Inc.
Headquartered in Irvine, Calif., Toshiba America Information Systems, Inc. (TAIS) is comprised of multiple divisions that provide computer, communications and imaging products and services. Products include industry leading portable computers, PDAs, mobile computing accessories, servers, including communications and portable servers, storage subsystems, cable modems, digital business telephone systems, voice-mail, digital cameras, security systems, and digital projectors. TAIS provides sales, marketing, services and manufacturing for its wide range of information products in the United States and Latin America. TAIS is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation, which is a world leader in high technology and integrated manufacturing of electrical and electronic components, products and systems. Toshiba has global sales of over $40 billion and more than 300 subsidiaries and affiliates worldwide.
Back to top
|