IRVINE, Calif., November 4, 1996 -- Toshiba America Information Systems, Inc., Disk Products Division (TAIS DPD) today introduced the industry's highest-capacity 2.5-inch disk drive and the industry's highest-capacity 2.5-inch slimline disk drive. Toshiba's new MK3303MAN 2.5-inch drive offers an unprecedented 3.3GB capacity and the new MK2103MAV slimline 2.5-inch drive delivers an industry high 2.16GB capacity.
"The new MK3303MAN and MK2103MAV drives set new capacity levels in their class," said Chris Norman, director of marketing, hard disk drives, TAIS DPD. "Toshiba developed these drives to meet the needs of today's notebook computer manufacturers for the highest possible storage capacity without sacrificing performance and reliability."
This new family of 2.5-inch disk drives combines PRML data channels with enhanced MR head technology to yield higher areal density allowing up to 720MB of storage per platter.
According to Norman, notebook computer users continue to demand the functionality and performance comparable to desktop PCs. " These new drives , offer the performance and capacity levels that make them top performers for not only text and data applications, but also multimedia applications that combine text and data with audio and full-motion video," said Norman.
The two new drives were developed with leading-edge performance and reliability. Featuring an ATA-3 interface, the MK3303MAN and MK2103MAV provide a fast 13ms average seek time and data transfer rates of 16.6MB/sec. in PIO mode 4 and DMA mode 2. The drives offer an industry-high MTTF of 300,000 hours.
The 3.3GB MK3303MAN, the industry's highest-capacity 2.5-inch disk drive, is the premier drive for notebook computer manufacturers. This drive features a fast 4852rpm rotational speed that provides an internal data rate of up to 76.4Mbits/sec. The MK3303MAN measures .75 (h) x 2.76 (w) x 3.94 (d) inches and weighs 7.7 ounces.
Toshiba's new MK2103MAV was developed to offer notebook manufacturers the highest capacity available in a slimline (12.7mm) profile, coupled with maximum performance and reliability. The 12.7mm-high MK2103MAV drive offers a fast 4,200rpm rotational speed which contributes to a peak internal data rate of up to 69.8Mbits/sec. The new slimline drive conforms to the demanding size, weight and power restrictions dictated by today's notebook computers. The new MK2103MAV weighs only 5.3 ounces and measures .5 (h) x 2.76 (w) x 3.94 (d) inches.
Samples of the MK2103MAV are available now with volume production scheduled for later this month. Sample pricing for the MK2103MAV begins at $595.
Sample units of the MK3303MAN will be available in December 1996 with volume production beginning in January 1997. Sample pricing for the MK3303MAN starts at $795.
Headquartered in Irvine, Calif., with approximate annual sales of $3 billion, TAIS is comprised of seven divisions which manufacture and market a wide range of business and information-oriented products in the United States. Products include portable and desktop computers, disk drives, CD-ROM drives, plain paper copiers, facsimile systems, digital key telephones and PBX systems, voice mail systems and toner products.
TAIS is an independent operating company, owned by Toshiba America Inc., a subsidiary of the $53.8 billion Toshiba Corporation, the fifth largest computer and electronics manufacturer, and the world's 36th largest corporation in terms of sales. Toshiba Corporation is a world leader in high-technology products with 173 major consolidated subsidiaries worldwide.
The TAIS Disk Products Division markets a wide range of industry-standard Winchester and CD-ROM disk drives in the United States. For additional product information, contact Toshiba America Information Systems, Inc., Disk Products Division, 9740 Irvine Blvd., Irvine, CA 92618; telephone (714) 457-0777, or on the World Wide Web at: http://www.tais.com/taisdpd/ or http://www.toshiba.com.