Toshiba Satellite C55-A5195 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

good laptop

POSTED BY: Pot , Dallas,PA
Overall rating: 5 out of 5 5 out of 5

easy to use

Good Workhorse Computer!

POSTED BY: Special K , Coupeville, WA
Overall rating: 5 out of 5 5 out of 5

I was compelled to purchase a computer to replace an aging Windows XP computer that was not going to be supported by Microsoft any longer. This was going to be an office computer; not an entertainment source. I have not been disappointed. When I needed a reconfiguration of the keyboard, Toshiba technical support came to my rescue with excellent service. I am not familiar with all the features of which this computer is capable and it's always plugged into a power source, but so far I am very pleased and have no complaints.

Great Laptop

POSTED BY: Papaw
Overall rating: 5 out of 5 5 out of 5

The C55 has been a great laptop so far. I really enjoy the long battery life.

great laptop at a reasonable price

POSTED BY: stach , jackson, nj
Overall rating: 5 out of 5 5 out of 5

the review title says it all with one exception. Easy to use.

First Laptop Purchase

POSTED BY: DanO , Long Beach, CA
Overall rating: 5 out of 5 5 out of 5

This laptop seems to be doing the trick so far. It allows me to be mobile as I still use by desktop PC. It is fast, efficient and sleek in design. I only wish it came loaded with more classic card games like backgammon, hearts, etc. to compliment the solitaire. Very pleased overall so far with this C55-A5195 laptop.

Love this laptop

POSTED BY: Matme , TN
Overall rating: 5 out of 5 5 out of 5

This is a great laptop. The price was so reasonable and it is so easy to use.

Awesome! I love it!

POSTED BY: Cheerful Musician , Tempe AZ
Overall rating: 5 out of 5 5 out of 5

Extremely delightful! Awesome! Best I've ever had!

Smooth as silk

POSTED BY: SavvyGranny , Home
Overall rating: 5 out of 5 5 out of 5

Love my new Toshiba. It glides from app to app without a hitch. Thank you.

Good buy for the money

POSTED BY: swdizzy , Colorado
Overall rating: 4 out of 5 4 out of 5

a bit slow

POSTED BY: Arnie , hawaii
Overall rating: 4 out of 5 4 out of 5

a bit slow but otherwise a good computer. got it with Windows 7 which I still think was a good move.

Not so much

POSTED BY: Pat , Castle Rock, CO
Overall rating: 3 out of 5 3 out of 5

This laptop okay in most things, but the keyboard is not very sensitive at all. You have to hit the keys fairly hard to make the keystrokes register. And, it's not terribly fast considering the amount of memory.

MSRP: $509.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i3-3110M Processor
  • Windows 7 Home Premium (64-bit)
  • 6GB DDR3 1600MHz memory
  • Intel® Integrated Graphics
  • 1.0TB (5400 RPM, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

build your own C50 shop for accessories