Toshiba Satellite C55-A5245 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

my laptop

POSTED BY: stan , Oscoda ,Mi
Overall rating: 5 out of 5 5 out of 5

I am joying my new laptop.

Best Laptop I have ever had.

POSTED BY: Les , Granbury, TX
Overall rating: 5 out of 5 5 out of 5

When I was working (presently retired), I traveled world wide and for 20+ years always carried a laptop computer. I replaced my computer every two years and with the exception of one replacement, I always purchased a Toshiba. I never had a problem with any Toshiba. The one time that I purchased a different laptop, the display died at the two year mark. Needless to say I went back to Toshiba and would not have any other brand. My model C55-A5245 Toshiba is the best and cheapest laptop I have ever had.

Good laptop, cheaper than tablet

POSTED BY: Vicki , Saginaw, MI
Overall rating: 5 out of 5 5 out of 5

This is my second Toshiba laptop. I thought the price was very reasonable. I had absolutely no problems with my first laptop purchased five years ago, so decided to go for another Toshiba. I've been very satisfied and would recommend this laptop to anyone, even folks looking for a tablet. Much cheaper and it does more than a tablet.

Very Good Machine for the Money

POSTED BY: Tom , Bird Island, Oklahoma
Overall rating: 5 out of 5 5 out of 5

Good gaming laptop

POSTED BY: UltimateFisher , Trenton, MO
Overall rating: 5 out of 5 5 out of 5

I got this laptop to use for mainly gaming. I'm able to run some high graphics game with no problems. Outside of the battery not lasting very long for some games, it's a really good laptop.

very smart tool!

POSTED BY: don dino
Overall rating: 5 out of 5 5 out of 5

Just upgraded from a old Dell this baby is a piece of work-beautiful styling performance.

Great improvement

POSTED BY: Retired , Roseville, Ca
Overall rating: 5 out of 5 5 out of 5

Used older laptop with very little memory or speed. The Toshiba works great, and easy to set up and use. Excellent definition and tone.

Very nice laptop

POSTED BY: Sasquatch7 , Concord, CA
Overall rating: 4 out of 5 4 out of 5

Been using this for a month. I like it. The only complaints I have, is about the position of the network jack (too close to the front of the unit, interferes with my wireless mouse) and the SD card should seat farther inside the front ( so it can be left in the computer--- SAFELY )

I Like My Laptop - There Is One Annoying Thing

POSTED BY: Ms Lady , Upper Marlboro, MD
Overall rating: 4 out of 5 4 out of 5

Overall, I like my Toshiba Satellite C55-A5245 Laptop. However, the factory installed Internet Explorer is very annoying, it constantly pops-up, and interrupts while I am on other sites

POSTED BY: Duffy , Temecula, CA
Overall rating: 4 out of 5 4 out of 5

Nice laptop

POSTED BY: ROC , Royal Oaks, CA
Overall rating: 4 out of 5 4 out of 5

My old dell laptop has windows XP on it which I was really used to. Since mirosoft quit supporting XP I decided it was time for a new one. After looking around for awhile I chose this one. I heard many bad things about windows 8 and only good things about windows 7. This laptop has windows 7 and it took me all of about 10 seconds to get familiar with it. I've had it for about a month now and really like it. The only negative thing about it is I wish a better owners manual would have came with it. Not enough info about the laptop. Especially if you are a beginner. Over all for the money this is a really good laptop.

Satellite C55-A5245

POSTED BY: apollo97 , Springfield, OH
Overall rating: 3 out of 5 3 out of 5

I wish I had gone with a Intel i5 instead of i3 and 8gb memory. I bought this with 4gb. I have purchased another 4gb to add. It's not near as fast as my desktop and speed is what I'm all about but this laptop is for my wife and she's satisfied with it. She had it reboot once unexpectedly but it has not happened again. It's decent for the price.

Disappointing

POSTED BY: MorganStreetArcher , Tucson, AZ
Overall rating: 2 out of 5 2 out of 5

It is insane to ship a new computer without a hard copy manual, a list containing all INCLUDED features and how to access and use them as well as a diagram of all keys, input and output plugs and other physical features. And worst of all; the keyboard. It is too small, the keys are too close together and are MUCH too sensitive.

MSRP: $449.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i3-3110M Processor
  • Windows 7 Home Premium (64-bit)
  • 4GB DDR3 1333MHz memory
  • Intel® Integrated Graphics
  • 500GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

build your own C50 shop for accessories