Toshiba Satellite C55-A5281 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Great laptop for the price

POSTED BY: TW , Kansas City
Overall rating: 5 out of 5 5 out of 5

I have been using this laptop for about a month now and the performance has been very solid for the price paid. The speed of navigating web pages is great and the battery life is excellent. Still trying to get used to Windows 8 but it should get easier to use over time.

new laptop

POSTED BY: andy , Hughson,Ca
Overall rating: 5 out of 5 5 out of 5

convenient perfect size optimal learning time to master windows 8 able to transfer old computer data onto new one.

Great Laptop

POSTED BY: ptmickey , Stockton, NJ
Overall rating: 5 out of 5 5 out of 5

Love this laptop, replaced an old XP based clunker and what a difference. This is lighter, faster, easier to use than my 5 year old Dell. I had trouble getting used to Windows 8 but after a week got used to it. Still dont like the Toshiba software shell though; it seems to battle with Windows 8 when loading software. Had a very hard time loading MS Office because of the Toshiba window blocking Windows, but after a few days got it working. Still overall would buy this again.

Working Well So Far

POSTED BY: Rick , Catskills of New York
Overall rating: 5 out of 5 5 out of 5

Satisfied with performance of computer, but still struggling getting used to Windows 8. This is not a bad reflection on the computer, just the operating system.

Great

POSTED BY: BabyGirl , Escanaba Mi
Overall rating: 5 out of 5 5 out of 5

i love windows 8.1 i dont have a problem with it yet and i hope i dont

awesome Laptop

POSTED BY: Jewels , Pompano Beach, Fl
Overall rating: 5 out of 5 5 out of 5

I really like this laptop. I'm still learning it but overall it's awesome :)

Great computer

POSTED BY: FlaminNinja
Overall rating: 4 out of 5 4 out of 5

I had bought this computer for a cheaper price. But besides the price it is an amazing laptop. This is my first windows 8 laptop and I'm happy with it

Good machine

POSTED BY: Pici
Overall rating: 4 out of 5 4 out of 5

The machine is good and offers excellent value for the price. It's a bit heavy but I knew that from the beginning. My biggest critique does not concern your product but the misguided product called Windows 8.1. it has made my life difficult and having to be subjected to Microsofts product development proved to be frustrating. I wish Toshiba would join HP to give us the opportunity to use Windows 7 as the operating software. I really will turn to Apple next time if Microsoft doesn't figure out that we are in business and cannot waste valuable time learning their absurd OS changes. This is not a reflection on Toshiba. I have purchased your products in the past with success. But you need to take a firm stand with Mircrosoft like HP has.

A nice piece of equipment

POSTED BY: My first laptop purchase , Caledonia, NY
Overall rating: 4 out of 5 4 out of 5

Quite happy with the equipment for having it a little over 30 days Wondering if I can change the sensitivity of the touch pad, for sometimes it just doesn't want to move I do not have enough knowledge to change the laptop settings. I fuddled around a bit to get it where it is. Though it has nothing to do with the equipment, I strongly do not like the right side task bar opening up with the date showing up in huge font every time I use the scroll bar..for the life of me can not change the settings on that!! Love the number keyboard on the right side Starts up and shuts down quickly

A good choice

POSTED BY: Willameister , Logan, UT
Overall rating: 4 out of 5 4 out of 5

I've had this computer for over a month now and am happy with it. It's basic and not as compact as more expensive models, but the speed is fine and it's been dependable. Good value.

Good value

POSTED BY: Schwartzdogs
Overall rating: 4 out of 5 4 out of 5

Units boots up fast, and screen has great resolution. Speakers could be better and Windows 8 blows, but overall a great value

Satisfied-Except for poor speakers

POSTED BY: Deebesmart , North Carolina
Overall rating: 4 out of 5 4 out of 5

I'm satisfied with my new C55-A Toshiba EXCEPT the speakers are terrible. I Skype quite often, the speakers have very low tones even when the volume is turned up to maximum. Very Disappointing!

Toshiba Satellite C55-A5281 Laptop

POSTED BY: Facebook Nut . , Ma.
Overall rating: 4 out of 5 4 out of 5

To be Honest ! I, Was very Surprised that with a brand new Computer You get no Literature . Espically when most of these new computers these days are running Windows 8 or 8.1 they should really provide people with at least the basics to get them started !

GOOD FOR PRICE.

POSTED BY: Consumer
Overall rating: 4 out of 5 4 out of 5

Easy to set up. Fast for my basic needs. Streams fine. I'll never get used to Windows 8/8.1 and the charm bar and all the other unnecessary change for the sake of change. Seems like this is meant to be a touch-screen but it's easy enough to customize and bypass the Apps start page. Also have constant usb mouse recognition problems but that may be the mouse for all I know. I only use this laptop to surf and stream and it works fine.

Great laptop

POSTED BY: delray , Jefferson City Mo
Overall rating: 4 out of 5 4 out of 5

Good value, so has met my expectations and working well with windows 8.1

Love it!

POSTED BY: Grandmacheryl , Haltom City, TX
Overall rating: 4 out of 5 4 out of 5

My laptop was a birthday gift from my brother and sister-in-law. It is very user-friendly, and that is definitely a plus for me. The superb resolution is really a bonus for watching movies.

My second Toshiba

POSTED BY: Jack , Northridge
Overall rating: 4 out of 5 4 out of 5

It is good in every aspect except for Windows 8 and during typing, the P letter requires more pressure than the others. Without that extra pressure P might not come out

Good laptop

POSTED BY: arkiegal , Paris, AR
Overall rating: 4 out of 5 4 out of 5

I like the Toshiba Laptop. The mouse plug in and the power cord plugs into awkward places on the laptop. They always seem to be in the way, especially the mouse connection. It is right where the mouse sits.

Great Support

POSTED BY: RK , Flagstaff, AZ
Overall rating: 4 out of 5 4 out of 5

Love the LapTop, Hate Windows 8. This Laptop is not a touch screen system and I find it very hard to navigate from one screen to another. One problem, I could not load windows one day. I tried the on line support to no avail, then I called Toshiba support and she had me up and running again within 5 min. Thanks, Toshiba !!

Great Laptop

POSTED BY: 3Bear , Sparks, NV
Overall rating: 4 out of 5 4 out of 5

The Toshiba Laptop is a great piece of equipment. Just don't care for the Windows 8 operating system.

Enjoying this laptop

POSTED BY: GiGi , GA
Overall rating: 4 out of 5 4 out of 5

I am enjoying this laptop, it is light weight and easy to use as I am learning the Windofws 8 Love the longer battery life.

nice computer

POSTED BY: JIM , Florida
Overall rating: 4 out of 5 4 out of 5

I am not use to windows 8.1. There is a lot of differnce from XP. The sound is poor. Everything else seems OK. J

satellite

POSTED BY: gpaul , Cape Cod
Overall rating: 4 out of 5 4 out of 5

I like the machine. It is lighter than my last laptop. I especially like the numeric keypad on the side. I use it often. Windows 8 tiles seem more useful for touch screen and I am most often inclined to go to the desktop. Also, I don't find apps useful on a laptop. Opening the browser is slowed by the fact 2 tabs open at the same time, Toshiba and Microsoft. I don't use either as I already enjoy another home page. I just want the search engine when I open.

Setting up the laptop is difficult for nontechies

POSTED BY: Sally , newark, de
Overall rating: 4 out of 5 4 out of 5

I like the laptop but found it impossible to set up on my own. Also having trouble negotiating the little sidebar that pops up to turn the computer off along with other stuff. Having trouble with other odds and ends. Just difficult for nontechy old people like me.

Satellite C55 A

POSTED BY: Spanky of AZ , Glendale, AZ
Overall rating: 3 out of 5 3 out of 5

The sound/speakers on this computer sounds like a 1960 transistor radio.

Horrible Sound

POSTED BY: jaljsocal , Los Angeles, CA
Overall rating: 3 out of 5 3 out of 5

The general specs of this product are decent for the price. However, the sound is beyond horrible. Fisher Price toys have higher sound quality. I will be debating about returning this computer solely upon the disgusting sound quality. You can't even connect external speakers and get better sound...it's simply the computer's bad hardware which is incapable of producing quality sound.

Ok Laptop

POSTED BY: VGM911 , Bridgeport,CT
Overall rating: 3 out of 5 3 out of 5

The Laptop is okay for the price.

Problem with bottom left of laptop

POSTED BY: Rollingstone
Overall rating: 3 out of 5 3 out of 5

Very frequently when I am typing my left hand sleeve hits something (I have no idea what it is) and will cause everything that I have been typing to be erased. This is extremely obnoxious and should not be happening but it does over and over and over and over.

I hate Windows 8!

POSTED BY: CJ , Cincinnati, OH
Overall rating: 3 out of 5 3 out of 5

The laptop is a bit on the heavy side for traveling. I absolutely hate Windows 8! You should be able to still get Windows 7.

Ok machine

POSTED BY: beaclan , Tulsa, Ok
Overall rating: 3 out of 5 3 out of 5

I don't have any real dislikes about the Toshiba except two items. First, I would like another USB port. Second, I would like for it to have blue tooth. Since it doesn't, I have to use a USB device and it uses one of my blue tooth ports. I didn't like Windows 8 so I got a copy of Windows 7 and replaced it with it. Luckily, you had all the drivers I needed but your website was fairly cryptic about which ones I needed to use. I was finally able to figure it out but it took me a couple of days to get it right. I'm still not sure if I got the graphics driver correct but it seems to be working ok. It is not as high a resolution as I would like it though. Speed and battery life are fine. The only other gripe is that plastic seems a little brittle to me. Not sure if it can adequately protect the devices.

No scroll

POSTED BY: Matty , Klamath Falls, Or
Overall rating: 3 out of 5 3 out of 5

There is no scroll on the touch pad and it is not a touch screen.

Toshiba C55 A5281

POSTED BY: ljj
Overall rating: 2 out of 5 2 out of 5

This was a good computer for the money but the on-board speakers were horrible which influenced my performance and features rating!!!

awlful

POSTED BY: do not have one , Manteo,NC
Overall rating: 2 out of 5 2 out of 5

I have one and I purchased a new one that I DO NOT like at all.

my opinion

POSTED BY: emr , kcmo
Overall rating: 2 out of 5 2 out of 5

Had I known the pc required 8.0 or 8.1 I would not have purchased. the speed has not increased and there is little support

POSTED BY: charlie
Overall rating: 2 out of 5 2 out of 5

I don't know if it is the computer or the apps. but I would never have bought this product if I had know that using and adding things would be this much of a problem.

Hard to use

POSTED BY: Mormor , Duarte, CA
Overall rating: 2 out of 5 2 out of 5

I have a hard time using this lap-top. I expected it to be easier than it is. Did not come with a handbook, which I feel is necessary on this model..

This is the worst laptop I have ever had!!

POSTED BY: birdie , Covington, Ohio
Overall rating: 1 out of 5 1 out of 5

I have never had a computer that every time the arrow even gets close to the edge, the tool bar comes in and sometimes it pulls up the desktop page or the date and time show up. This is so frustrating especially when you`re playing solitaire, etc.

unhappy with laptop

POSTED BY: annie , New York City
Overall rating: 1 out of 5 1 out of 5

bigger than I wanted; haven't used it yet. all I have done is register it. I cant return because I have it too long

a great disappointment

POSTED BY: beauciel , Pittsburg, CA
Overall rating: 1 out of 5 1 out of 5

I've had this laptop since Christmas, but I'm sorry to say it has been a great disappointment. I can;t get in to the Internet. I have a terrible time disconnecting or terminating a session. Plus the battery never tells me how much charge I have or don't have Who can I contact for help with these basic issues?

MSRP: $499.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Pentium® Processor 2020M
  • Windows 8
  • 6GB DDR3 1600MHz memory
  • Intel® Integrated Graphics
  • 750GB (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

build your own C50 shop for accessories