Toshiba Satellite C55-A5286 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

first laptop

POSTED BY: golfnut , valrico,florida
Overall rating: 5 out of 5 5 out of 5

great product, easy to use, great price, awesome.

Worth the money!

POSTED BY: Rose
Overall rating: 5 out of 5 5 out of 5

my uncle got this for me for christmas and it is amazing! For my first laptop, it is so worth it~

So Far So Good!

POSTED BY: rnbksm3 , denver, colorado
Overall rating: 5 out of 5 5 out of 5

The computer is still new. I have been using it for 2 months and LOVE it! For me, its all about the long run...If it still functions like this in 2 years, I will be exstatic.

Breath of Fresh Air

POSTED BY: phil h , Burbank, CA
Overall rating: 5 out of 5 5 out of 5

I am astonished on how this Toshiba laptop is so user-friendly. I am older than most first time buyers and not very familiar with the bells and whistles available in the computer world, but Toshiba has made it very easy for me. Highly recommended

Toshiba Loyalty

POSTED BY: Cosmo , Los Angeles, CA
Overall rating: 5 out of 5 5 out of 5

I have had Toshiba laptops forever. I have been nothing but pleased the quality of all Toshiba products. The prices are always fair and have great offers. Toshiba has my total loyalty. I will buy and recommend Toshiba always.

Very Happy!

POSTED BY: Guin , Florida
Overall rating: 4 out of 5 4 out of 5

This is an excellent laptop. Great value for the price. The only downside is the sound card isn't great. It's good enough for YouTube and various quick videos or TV shows. But my priorities for this were speed and RAM for running multiple programs, which it does very well. It is a beautiful machine, well made, and doesn't feel cheap or too plastic-y. Yet another satisfied purchase from Toshiba.

good prize

POSTED BY: sapon
Overall rating: 4 out of 5 4 out of 5

Its a giood lap whith actually standard, has a great prize

So Glad I Picked a Good Laptop!

POSTED BY: savannah , Gassville, AR
Overall rating: 4 out of 5 4 out of 5

I have only had desktop computers; this is my first laptop. So far it is very easy to use. The battery life is great, slower when streaming, but even decent then. The keyboard is very comfortable if a full sized keyboard is what you want. Made it easy to transition from the desktop. I have even found that Windows 8, while very different, is not that difficult to learn. The screen picture is incredible. It is also very light considering the size. All in all this was a smart purchase!

Good Value

POSTED BY: Hawaii50
Overall rating: 4 out of 5 4 out of 5

This is a good product for people who don't need the extensive capabilities that more expensive models/brands offer.

Great laptop for the price

POSTED BY: Cher , Baltimore, MD
Overall rating: 4 out of 5 4 out of 5

The only thing that I did not like is windows 8

Great product, bad OS

POSTED BY: dont have one
Overall rating: 4 out of 5 4 out of 5

This is a great laptop, I love it. The operating system, Windows 8, is pitiful. I would recommend this product but not with this OS.

Newest Laptop-Keep Toshiba, Lose Windows 8

POSTED BY: pat , Jonesboro, AR
Overall rating: 4 out of 5 4 out of 5

Love this laptop--its size, color, performance. Toshiba is a name I trust for durable, long-term performance. Windows 8 is insane, unwieldy, and a colossal mess, without which, I would have submitted a perfect rating.

POSTED BY: lyn , Durham, NC
Overall rating: 2 out of 5 2 out of 5

Lots of extras for price, but ports did not work for my flash drives.

laptop review

POSTED BY: Bob
Overall rating: 2 out of 5 2 out of 5

Very poor sound from speakers and from earphone. Very disappointed. Soundcard and speakers are the worst I have ever had on a laptop. Not going to buy Toshiba again with this obviously poor sound - why would any manufacturer produce such terrible sound and expect to have repeat sates.

bad computer

POSTED BY: slim , Ft. Worth, TX
Overall rating: 1 out of 5 1 out of 5

I tried for over a day to get the computer set up with no luck. I ended up returning laptop to store.

Worst laptop I've owned

POSTED BY: Buzz , Tampa, FL
Overall rating: 1 out of 5 1 out of 5

Hate this computer. Have already warned many people not to buy one. Horrible. Sorry I am stuck with it.

will go back to dell

POSTED BY: very unhappy , chicago,il
Overall rating: 1 out of 5 1 out of 5

I bought this machine in December, I got it on sale for a good price or so I thought. To start it has an AMD A4 quad core processor. This machine is slow and constantly hangs when browsing the internet. I know that it’s not my internet connection because my old dell machine running XP has no issues. This machine was stripped down didn’t come with any windows products (outside of the operating system). The constant charms popping up are very annoying, have tried to disable this feature with no luck. In short this machine was a waste of money. I will be going back to Dell and making sure that it has an Intel processor.

MSRP: $547.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i3-3120M Processor
  • Windows 8
  • 8GB DDR3 1600MHz memory
  • Intel® Integrated Graphics
  • 750 GB (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

build your own C50 shop for accessories