Toshiba Satellite C55-A5300 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Excelence

POSTED BY: Linux Lover
Overall rating: 5 out of 5 5 out of 5

This is a beautiful laptop with a good display. I don't worry about viruses because i use Ubuntu instead of windows. With this computer a recovery drive is easy to make.

Terrific!

POSTED BY: Penelope51 , Winnipeg, MB, Canada
Overall rating: 5 out of 5 5 out of 5

A terrific laptop for the price! I'm so glad I bought this one. Super fast, lightweight, overall a great buy. I'd recommend this model to anyone. (Just wish I could set my location as somewhere outside of the US.)

Love it

POSTED BY: candy , Michigan
Overall rating: 5 out of 5 5 out of 5

Love the laptop, functions well, good battery life. Hate the new windows 8!

I Love It!

POSTED BY: Noey
Overall rating: 4 out of 5 4 out of 5

This laptop is wonderful, but it is a little hard getting used to windows 8 so I mostly keep it on windows 7.

Fifth Laptop

POSTED BY: Happy , Clearwater,Fl
Overall rating: 4 out of 5 4 out of 5

This is my fifth Toshiba Laptop, and the performance has always been great. Little to no problems.

EVERYTHING AS ADVERTISED BUT......

POSTED BY: JOSHTX , TEXAS
Overall rating: 3 out of 5 3 out of 5

GREAT LAPTOP FRO THE PRICE. CANT COMPLAIN ABOUT WINDOWS 8 CAUSE THAT S MICROSOFTS PROBLEM NOT THEIRS. EVERYTHIG LOOKS AND WORKS GREAT. BUT THE PROBLEM I HAD IS THAT THE BATTERY FAILED WIHIN 3 MONTHS.AND TO SEND FOR REPLACEMENT (THE ONE THAT IS ONE THE WARRANTY, NOT A IM SOO SORRY THIS HAPPENED ONE) SO NOW NEXT ONE'S ON ME, AND TO MAKE MATTERS WORSE THE BATTERY IS ON BACK ORDER TIL ARPIL MAKING IT 5 MONTHS WITHOUT THE PORTABILITY OF A LAPTOP. OTHER THAN THAT I AM OK WITH IT.

Not bad

POSTED BY: victory , Houston, TX
Overall rating: 3 out of 5 3 out of 5

It's not bad. It'll do for what I need.

not happy

POSTED BY: harry , norfolk,va
Overall rating: 1 out of 5 1 out of 5

Not very happy. computer is hard to navigate. Won't work unless plugged in. Can't use with the battery and the computer is less than 2 months old. Can't get rid of pop-ups. Wanted to use AOL as browser but the computer is set to cause you problems f you use AOL as homepage.

MSRP: $336.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Celeron® Processor 1037U
  • Windows 8
  • 4GB DDR3 1333MHz memory
  • Intel® Integrated Graphics
  • 500GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

build your own C50 shop for accessories