Toshiba Satellite C55D-A5120 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Excellent Computer

POSTED BY: Bobby J , Portland, OR USA
Overall rating: 5 out of 5 5 out of 5

This is the first computer that I have owned just for myself and it is excellent . Very easy to use and it has all of the bells and whistles i need, not to many. I love the built in camera for Skyping. This great new computer actually helps me get on line more at home, I love it.

LOVING IT!!!

POSTED BY: marlborogal43 , greensboro,NC
Overall rating: 5 out of 5 5 out of 5

I am still learning how to use the windows 08, but I am loving the graphics, the speed. This was the best investment I made in a long tie.

First Laptop

POSTED BY: Wendixi , Whittier, CA
Overall rating: 5 out of 5 5 out of 5

I love the Toshiba C55D-A5120 Laptop. I have used other Laptop's before but this is my very first Laptop that I have purchased for myself. The price was very reasonable and the laptop has all the features that I need.

POSTED BY: sam , strawplains,tn
Overall rating: 5 out of 5 5 out of 5

Best laptop at good price. It has great features.

great value

POSTED BY: jonesy , Vanc. WA
Overall rating: 5 out of 5 5 out of 5

I like the bigger keys, seems to be a good value. Seems to operate smoothly. I only have 1 issue at this point, there are several commonly used keys that don't work on the 1st touch/strike when all the other letters show the 1st strike. I find that I have to go back and correct a lot of spelling, I have to proof read everything - taking more time to complete tasks. It will probably turn into a warranty issue. Other than that it seems smooth. I don't fully understand the OS, I like Vista more. Would I buy an upgraded later unit (in a couple years) in this brand? Yes, I would. I like the laptop, just not sure about the OS. Thank you for having a good unit for a very affordable price, I thought I was going to spend more money. Thanks, Jonesy.

Great laoptop

POSTED BY: Gigi , Auburndale, FL
Overall rating: 5 out of 5 5 out of 5

Good value

So far so Good!

POSTED BY: Lighthouse Lady , Stephens City, VA
Overall rating: 5 out of 5 5 out of 5

Still getting used to new laptop but it was easy to set up and its fairly easy to use. Haven't used on battery yet but I assume this is good also-battery life.

Great value

POSTED BY: NOYB , Maryland
Overall rating: 5 out of 5 5 out of 5

This is the 4th Toshiba I have owned. Toshiba is the only brand of laptop I will spend my money on!

it works realy good

POSTED BY: home computer , stamford ct
Overall rating: 5 out of 5 5 out of 5

since I got the laptop I can see that it works well, the picture density is excellent.

Great Laptop /Great price

POSTED BY: Virgi , Sacramento, CA
Overall rating: 5 out of 5 5 out of 5

Very happy with purchase-it was very easy to set up and would definitely recommend.

Great Laptop

POSTED BY: Marianne , Ash Flat, AR
Overall rating: 5 out of 5 5 out of 5

I love the Toshiba C55-A5120 Laptop. I love that you have added a number pad. Five years ago I bought a Toshiba Satellite L450 and loved it. The only problem I have with the new Toshiba is the keyboard. 20% of the time the key that is pushed doesn't register and I have to go back and correct the spelling. I looked at the L450 and the keys are slightly raised up where the keys on the new Toshiba are all flat. I think if they were slightly raised it would be easier to type. Other than that the Toshiba is tops in performance. My L450 is still going strong. My husband now uses it and has given up on any other product. The laptop is fast and easy to use. My programs run flawlessly. My husband is a computer techie and you have convinced him that Toshiba is the way to go. For the price, you can't buy a better laptop.

I love it!

POSTED BY: Charm , Charlotte, NC
Overall rating: 5 out of 5 5 out of 5

One thing that caught my attention was how good the battery life was. I love that the battery lasts for about 5-6 hours. I don't keep mines plugged in all the time because I don't have the need to and I don't overcharge neither. I like how light it is and easy to carry. It's lightweight and durable! I love the sound quality and the picture. It is very fast for it to have Windows 8.1 too. It could use some more storage though. But I love my Toshiba!!!!!

nice

POSTED BY: bustertoad , Alabama
Overall rating: 5 out of 5 5 out of 5

quiet and seems to cool itself very well. The USB drive recovery procedure went well.

first laptop

POSTED BY: wee1 , Pierpont, Ohio
Overall rating: 5 out of 5 5 out of 5

This is my 1st laptop. The old one was a desktop and had xp on it and I decided to get a new computer. I had excellent recommendations from folks about the Toshiba laptops so I purchased one. At first is was hard to get use to but I am making good progress. I like the 8.1 windows. My only problem is the Toshiba downloads and not knowing if there is security. I am working on it. For the price I am happy with my decision and your product.

Is as a new one should be.

POSTED BY: Marcus , Dallas, Tx.
Overall rating: 5 out of 5 5 out of 5

Like the layout of keyboard. The keys are good sized and well spaced. I do NOT like Win 8 and wish that I had gotten Win 7 Pro instead. Could be a tad bit faster...

All I have are Toshiba products

POSTED BY: Billy Bob , Cabot Arkansas USA
Overall rating: 5 out of 5 5 out of 5

Great products . And GREAT customer service Thanks keep up the good work. ((( ; Stephen

Good Value for the Money

POSTED BY: Fast Eddie
Overall rating: 5 out of 5 5 out of 5

old pc was a 7 yr. old desktop running Win XP sp3, so this is a big leap from what i'm used to. Win 8.1 also needs some time to learn as well. overall am very pleased with the new features and speed over the old system.

excellent experience with every use

POSTED BY: gimpy , Inverness, Florida 34453
Overall rating: 5 out of 5 5 out of 5

beautiful picture on screen,just learning the basics due to my own ignorance of all the new technology. I have a desk top I know it does way more than what I use it for. I got my laptop, as I am due for surgery on my hip and I assumed the laptop would be easier for me- bring the computer to me instead of me going to the desk top.

Great laptop

POSTED BY: Mk , Pa
Overall rating: 5 out of 5 5 out of 5

My review

POSTED BY: Zeke , Grand Rapids, MI
Overall rating: 5 out of 5 5 out of 5

I have always used Toshiba Laptop because of the reliabilty of them. I have found one issue with the C55 series. When you swipe for right to left on the touch pad, the right menu bar appears and at times can be a bit annoying. Not sure if this is a built in feature of this series. Overall, very dependable Laptop.

Great Basic Laptop

POSTED BY: Jf , Silver City, NM
Overall rating: 5 out of 5 5 out of 5

Probably too basic for a gamer but great for basic computer use.

Great Laptop

POSTED BY: Smily Face , Tomball,TX
Overall rating: 5 out of 5 5 out of 5

Great Laptop

POSTED BY: Bird , North Pole,AK
Overall rating: 5 out of 5 5 out of 5

What would make this laptop even greater would be a Blu-Ray DVD system

Satellite Laptop

POSTED BY: Rich , Houston, TX
Overall rating: 5 out of 5 5 out of 5

Purchased because high dollar HP failed and needed while HP being repaired. Really like Toshiba and will consider purchasing larger Toshiba and retiring HP.

Nice Laptop

POSTED BY: Vera , Chicago IL
Overall rating: 5 out of 5 5 out of 5

Nice laptop, runs smoothly and has all the features I could want...

games

POSTED BY: jameson4682 , Frisco, TX
Overall rating: 5 out of 5 5 out of 5

this is a good gaming computer. no lag at all

looks great

POSTED BY: SHER , ely, nv
Overall rating: 5 out of 5 5 out of 5

I haven't used it much and the windows 8 was hard to get use to, but I do like it.

laptop

POSTED BY: mike , west alexandria, oh
Overall rating: 5 out of 5 5 out of 5

This a good laptop for the price. I haven't tried to load any software yet. I would have like to have Windows Vista but am learning about 8.1.

Descent Laptop!

POSTED BY: Spongy , Brewer,ME
Overall rating: 5 out of 5 5 out of 5

Pretty descent laptop for price range and features. Easy to use once you figure out Window 8. It took me about a week to get comfortable with it. Love the HDMI output it works great with my HDTV. Glad that it comes with DVD player because most new laptops don't. Overall I am pretty excited with my new Laptop!!!!

Love my laptop

POSTED BY: Rozie , Indianapolis,IN.
Overall rating: 5 out of 5 5 out of 5

Love my laptop

POSTED BY: Glenda , Tyler, TX
Overall rating: 5 out of 5 5 out of 5

I like the overall performance of my Toshiba. I, however, do not like Windows 8.

I'm very happy with my "Satellite C55 Series "

POSTED BY: DAN OUTLAW , Linden, WI.
Overall rating: 5 out of 5 5 out of 5

First off I wasn't real keen on going to windows 8, but that's all I could find...... Well I ave a fiend whom has computer know how and he show'd me some of the features and how to work them so I'm learning and doing fine....... The biggest difference is the apps page and that's about it..... I'm still looking on where to find some things, but that's normal with anything new and different...... I do love this computer now...

A Jumpy Thing....

POSTED BY: Lilbit , West Warwick, RI
Overall rating: 5 out of 5 5 out of 5

I'm still learning this laptop, so maybe I'm writing this too soon.....But I don't like the way that it jumps to another screen if you go to far right or left....Thank Goodness I have learned to use the Homepage? to get back to where I was .....Other than that issue it seems to be an alright machine.....

Exelent laptop and good price.

POSTED BY: Maliante , Puerto Rico
Overall rating: 5 out of 5 5 out of 5

I love it. Big letters on keyboard, long battery working time and look gorgeous.

very good laptot

POSTED BY: Davi , Coral Springs, FL
Overall rating: 5 out of 5 5 out of 5

nothing negative to say about the computer i use every day to send estimate for clients thanks Toshiba.

Great laptop

POSTED BY: Ron , Elizabeth City, NC
Overall rating: 5 out of 5 5 out of 5

Laptop

POSTED BY: Me , Sarasota, FL
Overall rating: 5 out of 5 5 out of 5

Works well

Great laptop

POSTED BY: Millie , Dorado, PR
Overall rating: 5 out of 5 5 out of 5

Excellent for price!

POSTED BY: Sharon , Louisiana
Overall rating: 5 out of 5 5 out of 5

I have had no issues and would most definitely recommend this to a friend or family member.

Toshiba 1st

POSTED BY: Chelasew , TX
Overall rating: 5 out of 5 5 out of 5

I have never owned a Toshiba before,, I find it easy to work with. I would purchase another.

first laptop ever

POSTED BY: wolf , Towanda Pa
Overall rating: 5 out of 5 5 out of 5

this laptop does everything I need it to do.its very nice.

Very Functional Laptop

POSTED BY: Just Ask Jack , Irving, TX
Overall rating: 5 out of 5 5 out of 5

The quality is top notch. It has a CD drive and 3 USB ports and a card reader. So many machines are only online friendly these days. I like to be able to do both plug in and download. I like everything about this laptop except Windows 8. I have found a few workarounds that have made it easier to use. Thank you

I like it a lot

POSTED BY: Clem , Poway CA
Overall rating: 5 out of 5 5 out of 5

The laptop stays cool and works very well. I could not find the win 7 games like Freecell and Internet Backgammon I looked on line and found the games and installed them ,they should be included in a new laptop!

Toshiba CD55D-A5120 Laptop Computer

POSTED BY: Bob , Forest City, NC
Overall rating: 5 out of 5 5 out of 5

This is my second laptop and what a value. All features you could want in a small footprint that can be carried anywhere. Wireless connection makes it easy to use everywhere and battery power that last a very long time. I've used it for three hours and was still going strong when I finished the report. The screen is bright and extremely clear and with my upgrade to 8 Gig RAM it's fast. Says it's a AMD E-2 essential processor, don't know much about this. However I have always liked AMD processors above the others I've used in desktop computers. Above all else it's so easy to use and the keyboard works faultless. I highly recommend this laptop to anyone regardless of what for. I might add here I use flying games for pleasure and this computer handles everything I have given it, the external joystick, the speed, the graphics are just so satisfactory for me it makes me happy. Above all else I can't think of anything I might want more and especially for the price. Toshiba..... what a deal. Oh yeah, what's the deal about Windows 8.1? I can't find anything wrong with this operating system, it's worked flawless for me and it's fast.

POSTED BY: Charlie
Overall rating: 5 out of 5 5 out of 5

Laptop

POSTED BY: Sgt Heart , Lexington N.C.
Overall rating: 5 out of 5 5 out of 5

I like everything about the Toshiba Satellite C55D-A5120 but the sound quality. I do plan to buy extra speakers.

Godd laptop. ,good price

POSTED BY: Pat , Llano,Tx
Overall rating: 5 out of 5 5 out of 5

Love Toshiba's Laptops!!

POSTED BY: Casey1225 , Port Orange, FL
Overall rating: 5 out of 5 5 out of 5

This is my second Toshiba Laptop and I just love it!! I was so pleased with the one I bought back in 2009 that when it was time to get a new one I definitely wanted another Toshiba. The best ever!!

Very good laptop for home use

POSTED BY: Doctor Dan , Ocala, FL
Overall rating: 5 out of 5 5 out of 5

I have a desktop computer in our home office and I use the Toshiba Satellite laptop while watching TV in our living room surfing the Internet. Don't need all the bells and whistles that a more expensive laptop would offer. This C55D is just great for what my needs are.

Everything and more!

POSTED BY: James , Cincinnati, Ohio
Overall rating: 5 out of 5 5 out of 5

You can't beat the price !!

EXCELLENT BUY FOR THE MONEY

POSTED BY: Gibson527 , Milford , De
Overall rating: 5 out of 5 5 out of 5

I recently purchased the Toshiba Satellite C55D-A5120 Laptop I love this thing and with the new Windows 8 software it can do just about anything you want :)

have all ways had your product and know wouldent h

POSTED BY: Mikey , Newort'Michigan
Overall rating: 5 out of 5 5 out of 5

would reccomend to all my friends and won't have any other

Very Pleased

POSTED BY: Ruben , Oregon
Overall rating: 5 out of 5 5 out of 5

So far my Toshiba Laptop has been great. It is much faster than my old Laptop. I feel it was reasonably priced compared to other comparable laptops.

Good quality cool price

POSTED BY: Tai Tran , Garden grove, CA
Overall rating: 5 out of 5 5 out of 5

the laptop seem very build in quality in price value come with 6 cell battery which help last longer for student in school.

Love Toshiba

POSTED BY: Rocky , Titusville, FL
Overall rating: 5 out of 5 5 out of 5

This is my third Toshiba Satellite laptop and I wouldn't buy any other brand. Got the best, why try the rest?

POSTED BY: jeanne , elizabethville, pa
Overall rating: 5 out of 5 5 out of 5

this is my first laptop...also touchscreen..so far I amLOVING it

Worth the money

POSTED BY: Jays Mom , Montgomery, Tx
Overall rating: 5 out of 5 5 out of 5

This is a good one.

Good Buy

POSTED BY: happyguy72756 , Fayetteville, AR
Overall rating: 5 out of 5 5 out of 5

I reviewed several different brands before settling on Toshiba, and then only after the Computer Tech at my work recommend I get a Toshiba both for the reasonable price and great features, very pleased with what I got and would recommend it highly to anyone who is getting ready to purchase laptop.

Very good laptop, fast, smooth operating system

POSTED BY: DLA , Pike County, MS
Overall rating: 5 out of 5 5 out of 5

same as above...the screen brightness is excellent...

nice

POSTED BY: sluggie , maple city MI
Overall rating: 5 out of 5 5 out of 5

So far i love it. At one time i had a little problem getting on the internet exployer because the norton antivirus stop me from using it so i got it out of the programs and now works great. Doug MI

Good for the price

POSTED BY: Jaree , Charltte, NC
Overall rating: 4 out of 5 4 out of 5

I like it but still trying to get used to it.

It's ok

POSTED BY: sunnyt50 , Genesee Valley, NY
Overall rating: 4 out of 5 4 out of 5

For a basic laptop. This works well. Nothing special but I didn't expect it to be.

Pleased!

POSTED BY: sumac , Medina, oh
Overall rating: 4 out of 5 4 out of 5

Laptop arrived extremely quick. Easy to setup and add to home network. Not crazy about Windows 8 but I'm getting used to it. Loads programs fast & plays music wonderfully...sound is great for a laptop. Overall I'm pleased with my purchase.

I wish the Mic worked

POSTED BY: André , Arkansas
Overall rating: 4 out of 5 4 out of 5

I have had this laptop for almost 5 months, and I can honestly say that it is very much what I expected when I bought the computer: the screen is nice and large with great resolution, and I now have a full keyboard and NUM-pad. I was disappointed when I realized that the built-in microphone does not seem to operate, despite my best efforts. On the whole and thoroughly pleased with the result of my purchase. Thank you Toshiba.

good deal

POSTED BY: darkone , penna.
Overall rating: 4 out of 5 4 out of 5

Purchased the laptop online haven't gotten a new machine in 8 years! This laptop will work well for my needs and is probably capable of much more than I will ever use it for. Is for email browsing and social media only not a work machine. I am not tech person so I do not feeel I can give an in depth on the programs and apps. Did change the settings for the internet on its own when downloaded upgrades though. Had it's first trip to the geek squad.

Toshiba Satellite C55D-A5120 Laptop

POSTED BY: Bob , Deep South East Texas
Overall rating: 4 out of 5 4 out of 5

Finally had to buy a new laptop. The last Toshiba Satellite lasted 10 years and is still functional. The new one is terribly hard to use. The Windows 8.1 has a mind of it's own and does what it thinks you want done. It thinks you know how to use the computer, but in many cases this is not true. I want to be in control, not the computer. Too much games, shopping software on this machine, I need to do work, not play. And just try to delete the games, shopping apps, won't happen easily. Machine (Toshiba) is always trying to sell me something I don't want or need, it's wasting my time.

Very capable laptop for the money

POSTED BY: JWCamp , Bossier City, LA
Overall rating: 4 out of 5 4 out of 5

I needed to replace a 6-year-old laptop that had been very good until the video card went out. I saw this on a retailer website and decided , based on listed specs, it would do the job for which I need. The laptop is very capable for a budget machine. My only real complaint is the sound as it is terrible. You can improve the sound slightly by manually adjusting the equalizer.

Good Value for the Budget Minded

POSTED BY: cynicaltechie , San Francisco,Ca
Overall rating: 4 out of 5 4 out of 5

I think this model needs a better cpu and a blue ray drive. My battery life is great considering the fact it is new. I would have preferred less bloatware and windows 7 instead of windows 8.1 . I prefer Toshiba Laptops as a brand because they are made a little better than the last Dell I had. Toshiba Laptops have always been pretty reliable in the past including the antique, steel grey, thick brick, tecra model I had. The thing I don't like about this particular laptop is the lid cover design. It has a small line texture that doesn't make it easy to wipe down and it shows what would have been a simple scuff like it was a major scratch. I like a smooth finish there. When I got mine I also had to update the dvd drivers to make the dvd button function properly. It is great for someone just learning to use a computer or someone who doesn't do online gaming.

Glad I got it

POSTED BY: Mamaw , Cleveland,TN
Overall rating: 4 out of 5 4 out of 5

I got this computer as a replacement for a tablet that I had that was broken. I picked it due to the price. I am not very educated in computers and what all you can do with them but I love it for what I do use it for. I did have a problem with it which was not the computer's fault but mine and had to call for help. The man that helped me was very nice and helpful and corrected the problem. He was very patient with me and my lack of knowledge.

great for price w/some exceptions.....

POSTED BY: ycul1416 , South Bend, IN
Overall rating: 4 out of 5 4 out of 5

Very good price for product, and the laptop itself is great except for a pretty lame keyboard where many keys won't work without a pretty hard tap! Leads to lots of proofreading and going back to fix copy. I also hate Windows 8, but that is not fault of laptop. Other than keyboard, it seems to work great after my son-in-law fixed Windows 8 so it wasn't geared for a tablet, but works for a laptop.

Good hardware, software, eh

POSTED BY: Alchemist , Cerritos, CA
Overall rating: 4 out of 5 4 out of 5

The hardware is good (uses AMD rather than Intel). The screen has excellent resolution. The battery life is very good. It has the connections I need. I was looking for a well made laptop with Ethernet port at a reasonable price and this was it. The really bad part is Windows 8.1. It is not intuitive. It is hard to navigate. It seems to restrict the user rather than help. If I find a way, I will revert to an older version of windows.

Best Laptop I've used so far.

POSTED BY: Dinho61 , Monrovia, Liberia
Overall rating: 4 out of 5 4 out of 5

Can't use my Bluetooth devices with this tosheba laptop. Frustrating!! !

I'm no Teckie, but I love my Laptop!

POSTED BY: de , colo springs,co
Overall rating: 4 out of 5 4 out of 5

I have only basic computer use and knowledge, and have not gotten to really try all the functions, but the size and convenience is great! Now I rarely use my home computer, as I can use it when and where I want. Am still am told to be careful of using any private uses on wi fi. So guess I'm stuck with 2 for now.

Great for the price

POSTED BY: Apache's mom , Fort Myers, Florida
Overall rating: 4 out of 5 4 out of 5

This laptop would be the perfect computer for anyone if you would just get rid of windows 8.1.

First laptop.

POSTED BY: Frenchie , Colo, IA
Overall rating: 4 out of 5 4 out of 5

I am very happy with my choice of laptops. I only wish I had spent a little more and gotten the touch screen. I remedied that by getting a wireless mouse. I am still learning more about my laptop every day.

Good not great

POSTED BY: Joe , Ottawa, KS
Overall rating: 4 out of 5 4 out of 5

I am disappointed in the sound.

Great Laptop

POSTED BY: trealkiki , Phoenix, Arizona
Overall rating: 4 out of 5 4 out of 5

I am very pleased with my laptop. I find new things all the time.

Nice Laptop

POSTED BY: Moonman
Overall rating: 4 out of 5 4 out of 5

This is the first time I've owned a Toshiba laptop but I'm satisfied with it, so far. The features, sleek design and reasonable price led me to purchase this laptop.

Basic laptop

POSTED BY: wildamiky , TX
Overall rating: 4 out of 5 4 out of 5

The keyboard is sensitive and opens new tabs too easily. Very fast start up. Good battery life, so far. A basic laptop.

laptop ok, bad software

POSTED BY: Good Witch , House Springs, MO
Overall rating: 4 out of 5 4 out of 5

The laptop itself is ok, love the separate numeric keypad. This is my 4th Toshiba laptop. BUT, I absolutely HATE Windows 8.1. While I realize that is not Toshiba's fault, there should be an option to get a "free" downgrade to Windows 7. And you should not have to format your drive to reload everything.

Good not Great

POSTED BY: Ped98
Overall rating: 4 out of 5 4 out of 5

The only problem I have with this computer is the speed with which it processes as my last computer was a 6 GB and this one is only 4 GB. Everything else is rather easy to use. I thought I might have a problem with Windows 8, but it is easier than I had heard about from others.

Mostly Like

POSTED BY: Rusty , Sarasota, FL
Overall rating: 4 out of 5 4 out of 5

I got this computer to replace a really Old Friend. My old system support was discontinued by Microsoft, so I upgraded.....I thought! My Toshiba is a nice machine except with the difficulty I experience opening the CD compartment. I think that Toshiba attempted to hide the "open" button. My real frustration lies with Windows 8.1. To me, this OS is awful, really awful. I do not have a Smart Phone, and I don't do APPS!!!!! To be able to navigate this system in order to do simple tasks has taken me hours and hours of experimenting, reading HOW TO stuff and experimenting again. I keep a notebook so that I can repeat operations.

Great Going Toshiba

POSTED BY: Brightsunshine4u , Wilmington, NC
Overall rating: 4 out of 5 4 out of 5

This laptop has great performance for basic day to day usage. It is not a workhorse, but it does get the job done. The processor is better than I expected for the price. I'm using the Satellite C55D running Windows 8.1. First time I have used AMD E2 processor, hey, but it is better than previous experiences I've had with AMD type processors.... freezes a lot less and that's pretty good for me....I can make the best of Intel shutdown. Overall it is pretty nice laptop if you're not planning on doing too much gaming with it. It's a large enough screen to work with nicely, it is not too heavy and the ports available shame higher priced models.

POSTED BY: nae , shelton, wa
Overall rating: 4 out of 5 4 out of 5

POSTED BY: Ollie , Portland, OR
Overall rating: 4 out of 5 4 out of 5

The laptop is wonderful. The only issue it has, is the sound. The sound leaves a lot to be desired.

POSTED BY: m , E. Liverpool, OH
Overall rating: 4 out of 5 4 out of 5

Does the job...

POSTED BY: navyyardguy , Bensalem, PA
Overall rating: 4 out of 5 4 out of 5

Ok laptop for the money. No great expectations -- no great surprises. Adequate for the job.

Value for money

POSTED BY: mesum , Pakistan
Overall rating: 4 out of 5 4 out of 5

This laptop is must buy as money is concerned, the specs are quite good but when you start opening up few apps, the mouse stops moving. i have increased the ram to 16GB for maximum performance. it is an additional cost but still cheap as compared with other brands.

good for the money

POSTED BY: olddog , Albuquerque NM
Overall rating: 4 out of 5 4 out of 5

really good laptop for the money. I don't like windows 8 at all, it is annoying. Wish it had a hibernate setting, but for my purposes it is a very good laptop. no problems so far (knock on wood!).

I like it.

POSTED BY: Rusty_Not , Walnut Creek, CA
Overall rating: 4 out of 5 4 out of 5

Transitioned from XP(!). I'm new to WIN8.1 so there's a learning curve. However I AM having problems with the Synaptics touchpad. It has frozen twice, forcing an abnormal shut-down. I "Refreshed" the system, losing lots of updates and programs. I needed an external mouse to navigate and reinstall the mouse driver the last time (yesterday)

just a good laptop

POSTED BY: chinahand , newport, oregon
Overall rating: 4 out of 5 4 out of 5

I bought a Toshiba satellite L505D about five years ago which I still use. It is a good standard laptop and that is why I bought another Toshiba Satellite but now with windows 8.1 and a web cam. Toshiba makes good stuff.

Screen

POSTED BY: Slick Nick , Rochester, N.Y.
Overall rating: 4 out of 5 4 out of 5

On my screen there are little blemishes, stains.

ok for the money

POSTED BY: Dave , Greensburg, Ky
Overall rating: 4 out of 5 4 out of 5

I like your products. The last Satellite I purchased lasted for a very long time until the motherboard went bad.

Manual

POSTED BY: Judy , Santee, Ca
Overall rating: 4 out of 5 4 out of 5

My only complaint is that it did not come with a manual. I am from the old school of having a book in front of me. I was 3 hours trying to find out how to turn this laptop off. I do not want to download a manual to print it out.

First Time Owner

POSTED BY: Buggy
Overall rating: 4 out of 5 4 out of 5

This is my first very own laptop and I am really enjoying it.

Great Laptop

POSTED BY: Jodiblonde , Gray, KY
Overall rating: 4 out of 5 4 out of 5

I love my laptop, all but the speaker system. It really sounds terrible! You would think for that kind of money, they could make it sound much better. Even with headphones, it still sounds horrible! Other than that, I absolutely LOVE it! This is my first laptop. I have never owned one before.

good for every day use

POSTED BY: Onetrac 53 Master Techcontroller USNR , Dallas,Tx.
Overall rating: 4 out of 5 4 out of 5

Poor audio on internal speekers, even after 3hrs of tech support and installing Dts tool. The web cam is not Hd, it is very blochie. For everyday use for the bacis it is fast and stays cool. Super batt. life and easy to figure out if you are just getting into windows 8 or 8.1 as I am.

Really enjoy it

POSTED BY: Someone , ohio
Overall rating: 4 out of 5 4 out of 5

First laptop I ever bought. I really enjoy it! Keyboard is great and WINDOWS 8 is pretty easy to get use to.

POSTED BY: Evie , Sebring FL
Overall rating: 3 out of 5 3 out of 5

It a good laptop and the price is good but the. DVD drive takes to long to opening but the overall laptop is good

Not helpful for my use

POSTED BY: peanutz , Watertown TN
Overall rating: 3 out of 5 3 out of 5

I use a laptop for music playback during concerts through FOH PA. This Toshiba laptop does not have a line out, only headphone out. The music track playback was not a clear as I demand. Performance was fine. But I do not care for the new Windows 8. My reasons would take too long to explain. I prefer Windows 7.

Good laptop, TERRIBLE speakers

POSTED BY: stereoman1980 , Indianapolis, IN
Overall rating: 3 out of 5 3 out of 5

The computer is thin, plastic and lightweight, so I am very careful with the display when opening it. The keyboard is nice and feels responsive. The display is good, bright, and colorful. The processor does the job and is pretty fast (although I am not using a lot of high graphics programs or playing games on it). THE MAIN PROBLEM IS WITH THE SPEAKERS; THIS HAS HORRIBLE SOUND. I didn't buy it to be a high fidelity stereo, but I do expect music and videos to sound good. The sound is thin and tinny. My phone sounds better, much better. Sadly, this is the main reason that I could not recommend this model to a friend. I have not returned it because I already had a lot of stuff on it by the time I figured out how terrible the sound is.

Good entry level laptop

POSTED BY: Printer , Columbus,Oh
Overall rating: 3 out of 5 3 out of 5

I needed a computer for basic tasks to replace an my old laptop that was running XP. Compared to my old laptop this one is a great improvement in speed and storage. I have installed Dragon for to help with my word processing and is working fine. I have a concern with the audio, there is no adjustment in tone only volume. So far I really have no complaints.

Good performance/price product

POSTED BY: Nobu
Overall rating: 3 out of 5 3 out of 5

First, keep in mind that this is laptop's price is in the lower end. Thus you shouldn't expect that it will have high performance like those in the $600 or above range. That being said, its performance/price ration is good. It has 4 core although at a pretty low 1.3 Ghz. The 4GM memory can be problematic since some range are reserved by OS (thus not all 4GB are available to user program. But this is not unique to Toshiba). On top of that, some memory is reserved by the GPU which means GPU will compete with user for memory and its bandwidth. But my biggest issues are the following: 1) the speakers are tiny ones that produce terrible sounds; probably the worst in all laptops I have gone through (including 3 Toshiba products in the past). 2) the wireless performance is not optimal even with latest drivers (while I can get 2 to 5 times better performance on my Lenovo x201) in the same spot). 3) it does not bundle the AMD chipset driver and the disk performance suffers until I downloaded and installed the AMD ACHI driver. Still, sometimes it can be not responsible in some extended time when doing disk intensive I/O. 4) No TPM. Thus cannot BitLocker to utilize the HDD self-encryption! 5) This is not Toshiba's problem but Microsoft's - I decided to install ClassicShell to get the familiar Start menu back. (Not ready for the Windows 8.1's GUI yet. ;-)) In conclusion, this is not a bad laptop for beginners. You get what you have paid for.

Best Computer with Worst Operating System

POSTED BY: doug , Henderson, KY
Overall rating: 3 out of 5 3 out of 5

It's a shame what Microsoft did to a perfect Windows 7. I was so discouraged that I was going to have a Windows 7 installed on my new Toshiba. That is until I took it to PC-Quest, and a representative set it up to somewhat operate like a Windows 7. I would gladly pay more money to have an operating manual that is hand held

Laptop not functionally properly

POSTED BY: Blue Eyes , Louisville, KY
Overall rating: 3 out of 5 3 out of 5

I have connected my laptop to my WIFI and for some reason it wont let me go to certain websites - especially FACEBOOK which I love playing my games on there.. and I had to try to restore the setting after only having it 2 weeks - when I shouldn't have to do that. You would have figured they would have gave you a back up disk or something with it when you buy it but they don't.

Not elated with this laptop

POSTED BY: Fido , Desert Hot Springs, CA
Overall rating: 3 out of 5 3 out of 5

Will not connect to my LaserJet 5 printer and no one can help me.

Decent Laptop for the Price

POSTED BY: Kaylee , Arcanum, OH
Overall rating: 3 out of 5 3 out of 5

This laptop works pretty well. It has a good battery life and runs very quickly. The issue that I've had with it is the mouse. It freezes often and won't move when I move my finger.

Toshiba Satellite C55D-A5120 Laptop

POSTED BY: dbslws , Maine
Overall rating: 3 out of 5 3 out of 5

POSITIVES: WIDE screen, larger keyboard, good battery life, relatively fast boot-up / shut down. NEGATIVE: sound quality is abysmal! Great for Ebaying, computing; lousy for music, movies.

Laptop

POSTED BY: ttholen , Illionois
Overall rating: 3 out of 5 3 out of 5

2nd Toshiba I've owned. Not a bad computer but kind of slow and freezes now and then. Probably should have got one with a faster processor.

Better than a poke in the eye

POSTED BY: gunner , New York
Overall rating: 3 out of 5 3 out of 5

An adequate laptop for a reasonable price but loaded with adds and windows 8 which is very limited unless you get an msn account.

problem computor

POSTED BY: slick , okc. OK,
Overall rating: 3 out of 5 3 out of 5

have had 2 laptops in the last month one had problems with the windows updater could not turn it off it kept restarting. Now the one I have will not connect to the internet. I need this to complete and continue to work for the job title I have

GREAT FOR HOME USAGE

POSTED BY: TOETAPPER63 , LOS ANGELES, CA
Overall rating: 3 out of 5 3 out of 5

I good little laptop for home to work on music and video projects. Be careful of the MS Windows updates - they tend to cause problems to some functions.

POSTED BY: pamela , Cleveland, Ohio
Overall rating: 3 out of 5 3 out of 5

I don't find the Windows version 8 to be very user friendly. Otherwise it's a good buy for the price as you cannot buy a computer without version 8 on it. The Toshiba laptop is a good product.

Satellite Comp Rev

POSTED BY: moonman , Los Angeles, CA
Overall rating: 3 out of 5 3 out of 5

Still learning how to access the features of the laptop.

daughter laptop

POSTED BY: mom of 4 , NH
Overall rating: 3 out of 5 3 out of 5

A really good value. However, the sound volume is terrible. I will need to purchase external speakers for my daughter due to lack of volume. The overall performance is good.

Keys are sticking already

POSTED BY: babs , Orlando, FL
Overall rating: 3 out of 5 3 out of 5

Disappointed - keys are already sticking!!!

POSTED BY: Milkdud
Overall rating: 3 out of 5 3 out of 5

SLOW!!!

POSTED BY: Jon , Vegas
Overall rating: 2 out of 5 2 out of 5

10+ plus minutes to boot up! Nuff' said..

POSTED BY: Shelly , Stafford, VA
Overall rating: 2 out of 5 2 out of 5

decent low price laptop

POSTED BY: duckylucky1 , south amboy,new jersey
Overall rating: 2 out of 5 2 out of 5

It is slow and the speaker is awful. The resolution is just acceptable and the version of windows 8.1 needed a lot of tweaking. The Norton preinstalled is terrible.

very slow and limited software

POSTED BY: drwho64 , flagler beach florida
Overall rating: 2 out of 5 2 out of 5

This computer is very slow when surfing the internet and plays online games very poorly. It lacks even the most basic software like a word processor. I made a mistake buying this product without doing the research.

6 MINUTE STARTUP

POSTED BY: Valerie , Newark, DE
Overall rating: 2 out of 5 2 out of 5

6 Minute Start-Up Very Aggravating !! Performance is also slow (even after adjusting unnecessary services).

Poor Sound Quality

POSTED BY: SoundingOff
Overall rating: 2 out of 5 2 out of 5

Sound quality is much poorer than the old Satellite it replaced. Sounds like a speaker in a tin can. Connecting external speakers sounds like a speaker in larger tin can. These same speakers provided great quality sound with the Satellite it replaced. But now, no base tones, no depth to the sound. It's like listening to headphones from three feet away. I would be very pleased with the Satellite if the sound were better. Other than the poor sound quality, it is a great laptop. Unfortunately, even when connected to good external speakers, the Toshiba does not deliver adequate sound quality, preventing enjoyment of many of the intended uses that drove the purchase. Could Toshiba provide a downloadable fix to this audio problem?

Poor Quality

POSTED BY: Bill , BRFalls, WI
Overall rating: 1 out of 5 1 out of 5

Quit working in less than a week!

POSTED BY: Old man , Salt Lake City, utah
Overall rating: 1 out of 5 1 out of 5

Computer was ok, windows 8 is terrible, battery would not charge Sent laptop back for refund.

slowest laptop EVER!!!!

POSTED BY: smt , WI
Overall rating: 1 out of 5 1 out of 5

I am very unhappy with the performance of my NEW laptop!!!! It is truly slower than MOLASSES!!!!! It doesn't keep up with anything!!! Just general browsing on the internet, it takes FOREVER!!! I bought it because my older computer had windows XP on it and was told it was outdated and no longer secure. So we decided to get a laptop - wish I had my OLD CPU still able to work. As OLD as it was - it was still 10X faster than this laptop!!!!!!!!

DONT KNOW

POSTED BY: Jae , Jacksonville, FL
Overall rating: 1 out of 5 1 out of 5

I CANT REALLY GIVE AN OVER VIEW RIGHT NOW OF THE COMPUTER BECAUSE I HAVE NOT HAD TIME TO REALLY USE IT AND FIND ALL THE FEATURES THAT ARE ON IT. I WILL SAY ONE THING I DONT LIKE IS THAT THE BUTTONS STICK

Invirolated software to the max

POSTED BY: not happy with spying
Overall rating: 1 out of 5 1 out of 5

Bought the new computer. Installed my own anti virus software, and when I ran it. Brand new mind you, the results were 325 virus'. That is not a typo. I had the hard drive reformatted, and only the programs I wanted put on it. I can't even write a review without Toshiba trying to mine me for more personal data.

Wish I had made a different choice..,

POSTED BY: Jennpen , Isle of palms, SC
Overall rating: 1 out of 5 1 out of 5

Absolutely no ease of use. If you are computer saavy this one's probably for you. If you just want simple processes and internet access- steer clear.

THE SLOWES COMPUTER i EVERY HAD.

POSTED BY: ARN , FORT MCCOY FL.
Overall rating: 1 out of 5 1 out of 5

iIT IS SO SLOWI CAN GO TO SLEEP.

Worst Lap top ever made

POSTED BY: Paul , Brownsville, Tx
Overall rating: 1 out of 5 1 out of 5

This laptop does not connect to any search engine, slow to connect to email. Will not go to YouTube or Facebook, not to mention any google sites. Windows 8 is like dealing with Sybil I move the mouse to scroll down, and the. Screen changes

had major issue

POSTED BY: rog , glenwood ia
Overall rating: 1 out of 5 1 out of 5

the operation system would not work had to be flashed

MSRP: $308.52

not available for sale from
the toshiba online store

  • Laptop summary
  • AMD Quad-Core E2-3800 Accelerated Processor
  • Windows 8.1
  • 4GB DDR3 1333MHz memory
  • AMD® Integrated Graphics
  • 500GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

build your own C50 shop for accessories