Toshiba Satellite C55D-A5304 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Great laptop

POSTED BY: ashize
Overall rating: 5 out of 5 5 out of 5

It's a great laptop for a really good price. It's made specifically for a single person to use, although it can be used by multiple. The features take some time to get used to for windows 7 users. However, they can be very helpful. Toshiba is very efficient also. It works very well for regular day to day activities, and the windows 8 gives a wide range for use. You do have to get used to the sound being different then other computers, however, I think it's pretty good. I had to get used to it for a bit, but I like it overall. I've already recommended this laptop to one other person and would do so for others as well. This is a great laptop

Good

POSTED BY: Snoopy , Ga
Overall rating: 5 out of 5 5 out of 5

It A Good LAptop

Great buy & good solid technology

POSTED BY: Jon - California , American Canyon, CA
Overall rating: 5 out of 5 5 out of 5

Had other manufacturer laptops over the years and this is a return Toshiba. Forgot how they are good at design and build. Great screen and with this model, it is nice to have the number keypad now onboard. Will plan to replace another family member's PC with this model as well.

good laptop

POSTED BY: Big D , pensacola,fl
Overall rating: 5 out of 5 5 out of 5

had a toshiba before,till it fall and hit the floor and never had any problems with that one,so when i had more money to up grade to a lap top i whent back to a toshiba

Pleased with toshiba

POSTED BY: Rusty , Long Beach, CA
Overall rating: 5 out of 5 5 out of 5

I'm not mister computer wiz but I find my laptop very comfortable to work with.

Excellent Laptop!!

POSTED BY: garfield1970 , Henderson, TN
Overall rating: 5 out of 5 5 out of 5

This computer you get a lot of bang for your buck. It does very well I can run several programs at the same time and have no problem what so ever. Runs very smoothly.

One of the best

POSTED BY: Steelers9999 , Mahwah, NJ
Overall rating: 5 out of 5 5 out of 5

Excellent quality with decent price

Great

POSTED BY: Richp , Hammond IN
Overall rating: 5 out of 5 5 out of 5

Great laptop fast easy to use still working on some features

My first laptop

POSTED BY: Ava , Modesto CA
Overall rating: 5 out of 5 5 out of 5

About to start college and I really needed a laptop that wasn't too expensive, had a CD-ROM drive, headphone jack, good battery life and portable. After extensive research I came across this laptop and purchased it. Set up was fast and easy. Downloading apps was super fast. The screen is 15.6, very big and easy to see. I love Windows 8.Baterry life is 6-7 hours for me till I need to plug it in. At first the sound was awful but after tweaking a few things I am able to listen to music with no problems anymore. I have watched movies on my laptop with no lagging or buffering issues. I am very pleased with this laptop considering its my first.

So Good I Bought One For Myself, Too

POSTED BY: wu , Bonham, TX
Overall rating: 5 out of 5 5 out of 5

I bought the Toshiba Laptop for my husband on the recommendation of a friend. I liked it so much that I got one for myself the next week. We both love them.

Good laptop!

POSTED BY: Rohan , Henderson, NV
Overall rating: 5 out of 5 5 out of 5

Easy to use. Screen 'clean' and easily accessed on login. Great apps included. Virus protection promotion very helpful.

Good, Affordable easy to use Laptop

POSTED BY: retiree , Colorado and Michigan
Overall rating: 5 out of 5 5 out of 5

The computer has ONE MAJOR FLAW..WINDOWS 8 It is the worst thing ever. Spoils the joy f a new computer. It is the 2nd Toshiba I have owned.

great/quality/excellent

POSTED BY: frankie , wisconsin
Overall rating: 5 out of 5 5 out of 5

great product from what I can tell.This is my first lap-top and being not so good on computers it is very easy to use.Great features included like, a disc drive,web cam, sound recorder, etc. Plus many more built in. Good price value, and I would recommend this unit to everyone.

POSTED BY: Buckshot00 , Iowa
Overall rating: 5 out of 5 5 out of 5

Does every thing I need or want out of a laptop but windows 8.1 has been difficult to learn. Probably would not have gotten 8.1 if I knew it did not work with POP email. Not the computers fault. Very good price!!!!!!!!!!!! Only thing would be a better instruction manual and more info on 8.1

Toshiba Satellite P745-54217

POSTED BY: flagday1960 , Dupo, IL
Overall rating: 4 out of 5 4 out of 5

4/5 stars. Works "well" except for mid-screen cursor freeze. Enormously difficult to unlock(or "damaging" as one fix is "restore computer to 'out-of-box' condition", i.e., wipe out everything back to o-o-b condition (bye-bye photos/music). That problem has been a pox on my house. I should not HAVE to read stale and useless tech 'blogs from 2006 where users complain about the same problem (always w/ inanely "simple" but ineffective "fixes").

Great Laptop, But Slow

POSTED BY: Susan , Iowa
Overall rating: 4 out of 5 4 out of 5

The title says it all. It's a great laptop for kids probably, but anyone who needs speed shouldn't purchase it. For what i use it for it's ok. I would like it a little faster for gaming. It's great for regular stuff. Best quality for the price.

Good value laptop

POSTED BY: Rich
Overall rating: 4 out of 5 4 out of 5

Good laptop for price. Left mouse button too sensitive - causes unintended actions with extremely light touch - like changing zoom. Could find no way to adjust this mouse sensitivity. Fold-down screen has no finger grips to use to raise and lower and is of light enough construction to require extra care in positioning fingers to raise and lower. Case/shell is light plastic requiring extra care in handling. Speakers are adequate but do not produce high quality sound. Battery charge light often shows that battery charge is needed even though I have never used the laptop in battery mode.

good laptop

POSTED BY: jc , Montevideo, Uruguay
Overall rating: 4 out of 5 4 out of 5

good laptop

POSTED BY: mssfire , west falls, ny
Overall rating: 4 out of 5 4 out of 5

Overall this laptop is good...but am starting to have problems with keys sticking, and it's only been a month!! Also it seems to be slow in loading things. Other than that, the screen is outstanding, and the other features are good.

great find

POSTED BY: jarf , Bakersfield Ca.
Overall rating: 4 out of 5 4 out of 5

a great find at an exceptional value.

C55D good value for the money

POSTED BY: Danielle , Miami, Florida
Overall rating: 4 out of 5 4 out of 5

Well, I think this model is a good starter computer for everyday basic functions such as online videos, emails, web surfing, etc. With that said, I feel that the machine could operate a lot faster, its not exactly slow, but its not intuitive or lightning fast. Also for a PC operating windows 8 (which I feel is based largely on touch capabilities) operations maybe a bit quirky and frustrating. I feel that if the PC does not have touch capabilities, it should not operate with a touch based windows operation program. It just does work right and can be highly frustrating.

Toshiba Satellite is my favorate

POSTED BY: Henry , Boston,MA
Overall rating: 4 out of 5 4 out of 5

Affordable, for regular user not for tech person. Used to own Statellite M 35

Love my laptop!

POSTED BY: Miriah
Overall rating: 4 out of 5 4 out of 5

I only wish it would go a little faster but the graphics and color are great!

Great for the money!

POSTED BY: Sonnyblu42 , Englewood, FL
Overall rating: 4 out of 5 4 out of 5

My only issue is processor power and speed... just loading photos at sometimes can become laborious. However... For the price point and a absolutely great battery life (6 hours) I have no complaints. I needed a new laptop and quick... and this was there and right at the price I wanted to pay... including tax!

My First Laptop

POSTED BY: duckyThis is , Altoona,PA
Overall rating: 4 out of 5 4 out of 5

This is my first laptop. Even thou I have Windows 8.1 now. I still miss my Windows XP.

Very good value

POSTED BY: Darrell , Sun City, Az.
Overall rating: 4 out of 5 4 out of 5

Happy with performance, although it is somewhat slower than I had .hoped for. It is taking some time to become accustomed to windows 8. Overall, it is a wonderful value.

Drivers For W7

POSTED BY: Tininho , Brazil
Overall rating: 4 out of 5 4 out of 5

The laptop I acquired came with W8. For my use I prefer W7,and it was very difficult to acquire those drivers. It was a hard work but I could do it. The Toshiba home page does not provide drivers for W7 for this laptop.

Low Price High Quality

POSTED BY: PearlShopper , Boca Raton, FL
Overall rating: 4 out of 5 4 out of 5

Remarkably low priced yet fully functional laptop with as large a hard drive and as much memory as a laptop priced hundreds of dollars more. With every feature including a numeric keypad, camera, DVDRW drive, wireless N, USB 3.0, card reader, and HDMI out, it is more than what you need for home, school, or business. This is the best value on the market today. Sorry, but the secret to why it is so inexpensive is that it uses the cheapest available PCU Microprocessor, so if you're a gamer or graphic user, it will disappoint you. Strangely, Toshiba has replaced the function keys with TOSHIBA KEYS. No more Alt-F4 to close any app, no more Shift-F3 to change the case in Word documents, no more F11 full screen Internet Explorer. Instead, all you can do is change the volume or turn on a second screen.

Good for the Price

POSTED BY: TallyShopper , Tallahassee, FL
Overall rating: 4 out of 5 4 out of 5

Purchased this laptop after my HP laptop bit the dust in less than a year. It has a stronger processor than my HP had but seems to run much slower. I'm not sure if it's the Windows8 OS as I had Windows7 previously. It does what I need it to do. There aren't many features to speak of. The charger seems insubstantial and delicate more along the lines of what I'd expect from a lesser known brand. I do like the fact that the fan vent is on the side as opposed to the bottom of the laptop. I intend to replace this laptop when finances permit.

worst laptop ever

POSTED BY: musicman , United states of america
Overall rating: 3 out of 5 3 out of 5

The processor is too slow, the USB drivers don't recognize my MP3 player, not enough memory for my everyday use. This might have been the cheapest laptop on the market but I still expected better than this.

poor speakers

POSTED BY: captian , fl
Overall rating: 3 out of 5 3 out of 5

this unit has real poor speaker sound. and windows 8 is not for the average user

Not happy with performance

POSTED BY: lee television , New York, NY
Overall rating: 3 out of 5 3 out of 5

My new toshiba freezes and shuts off sometimes

Low end

POSTED BY: Tim
Overall rating: 2 out of 5 2 out of 5

I bought cheap. I got cheap.

Poor battery performance , etc.

POSTED BY: Spidermonkey Joe , Cinci, OH
Overall rating: 2 out of 5 2 out of 5

I am disappointed that the battery life is so short. My daughter can not even watch a movie on it without plugging in. Also, seems that Windows 8 taxes the available memory to the point that it is always freezing up and warning that system resources are critically low. This machine would probably be a fine performer with Windows XP, but it comes with Windows 8. Very nearly useless in its current configuration.

laptop

POSTED BY: Tortuga , Redding, CA
Overall rating: 2 out of 5 2 out of 5

Been having many little problems. Don't know what to do or how to handle them.

Worst experience ever!

POSTED BY: Keith , Richmond, VA
Overall rating: 2 out of 5 2 out of 5

Not at all happy with this PC.

Not HAPPY

POSTED BY: chinadoll , los angeles, CA
Overall rating: 2 out of 5 2 out of 5

Speakers are terrible, runs slow only have had the laptop 30 days and have not download anything. (afraid to) dull screen not very sharp. I guess you get what you pay for.

Basic Laptop but very slow and laggy

POSTED BY: Basic Computer Guy , Wentzville, MO
Overall rating: 2 out of 5 2 out of 5

Very Slow, speakers are terrible but screen is ok

orst laptop ever

POSTED BY: kj , skokie,il.
Overall rating: 1 out of 5 1 out of 5

thepages keep flipping back and forth and I do not like wins 8 as much as I liked windows 7

Horrible video card

POSTED BY: Kat23 , Chicago, IL
Overall rating: 1 out of 5 1 out of 5

I bought this laptop b/c my other laptop is over 7 years old. The video is HORRIBLE. I literally have been using my old laptop for video and I am starting to wonder why I even bought this laptop! It is slow and the video quality is horrible. maybe my video card is bad but i've never seen it like this.

HORRIBLE

POSTED BY: HJ , TN
Overall rating: 1 out of 5 1 out of 5

do not let the positive reviews on this page fool you, this computer is the biggest piece of junk i have ever used. it cant even type words into google without lagging. absolutely awful. even for the money

not happy!

POSTED BY: yeafaith , Cincinnati
Overall rating: 1 out of 5 1 out of 5

This new computer was a gift from dear friends. Sadly it is total let down Unlike Apple which is simple yet sophisticated this laptop is impossible. From the first day I turned it on, nothing made sense, nothing is easy and I still have major issues.. Programs close randomly while in use, things are difficult to navigate and very hard to find.

Avoid this computer

POSTED BY: FrenchDressing , Fort Myers, Fl
Overall rating: 1 out of 5 1 out of 5

We are a Mac family but I needed to run Access. I thought it would be better to buy a cheap laptop rather than install windows on my wife's 5 year old Mac Book. Boy was I ever wrong. this thing is so slow it almost runs backwards. It doesn't even come with Bluetooth. I didn't know that they even make computers without Bluetooth. Surfing the internet with my 7 year old Mac Mini is much better than this. Maybe its Windows fault but then they should not sell it with windows installed.

S-L-O-W

POSTED BY: dan , woodhaven MI
Overall rating: 1 out of 5 1 out of 5

Slowest lap top I ever used.

MSRP: $358.99

not available for sale from
the toshiba online store

  • Laptop summary
  • AMD Dual-Core E1-2100 Accelerated Processor
  • Windows 8.1
  • 4GB DDR3 1333MHz memory
  • AMD® Integrated Graphics
  • 500GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

build your own C50 shop for accessories