Toshiba Satellite C55D-A5362 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

GREAT STARTER!!!

POSTED BY: Jackson , Rochester MN
Overall rating: 5 out of 5 5 out of 5

I purchased this laptop for my son as a Christmas present. It has been great so far!!

Secret quadcore cpu

POSTED BY: Green Arrow , Miami Florida
Overall rating: 5 out of 5 5 out of 5

This quad core performs better than some i7 and even i5. I have incredible 11 second boot up time and blazing fast performance. I may have a faulty chip or something but I am glad I bought it. Im a former owner of i7 2.5 ghz quad 6gb cache and this cpu rocks on windows 8

Good Value

POSTED BY: Tiger , Lawrenceville, GA
Overall rating: 4 out of 5 4 out of 5

The only thing that disappointed me was the audio quality. I use external speakers sometimes to amplify the laptop audio, but when I do the sound is really low quality. It sounds thin and cheap. When I use the laptop speakers, it sounds exactly the same but the volume is much lower. I've noticed that watching movies and using a headset the Toshiba has the same low quality audio. My older Toshiba has a much better sound both internally and externally, and I assumed my new one would too. I still like the laptop, but I don't use it for music listening.

Needs Some Upgrades

POSTED BY: Helpingwithhomework , Hawaii
Overall rating: 3 out of 5 3 out of 5

We bought this as an extra laptop for my elementary school age children to do homework on. It definitely needs a better touchpad auto scrolling feature. Our Sony VAIO has a much more user friendly touchpad. Also the screen intermittantly dims and brightens and we don't know the cause. It may be due to low battery charge, or the computer getting updates, or a loose connection between the power cord and the laptop. Whatever the cause, it is annoying and distracting. It is also taking a while for us to get used to the Windows 8 operating system but that is not a Toshiba problem. Overall, it is nice to have another laptop in the house, I just don't know if it should be a Toshiba

Bad experiences

POSTED BY: Bear , Virginia
Overall rating: 1 out of 5 1 out of 5

I originally acquired a discontinued model with a 750 GB HDD. The battery failed the first time I charged it. The retailer was very helpful, though, and I was able to take the unit on a business trip a few days later. That's when the unit failed a second time. This time the HDD failed badly - taking out almost a week's work in configuring the system, loading software, and transferring data. It was useless on the trip. However, the company that sold me the unit is national. A west coast store very helpfully replaced my broken unit with a newer one... unfortunately with only 500 GB of HDD. However, without the destroyed data and software, it did me no good. Other than annoyances with Win 8.1, I was bothered only by the mouse cursor pad (badly located and too proximity sensitive for me), and was happy to see a software driver upgrade that recognized when I attached a USB mouse. That software has failed miserably. I cannot use the unit without the USB mouse at this time. After less than a minute, the software locks up the mouse cursor and ignores the cursor control pad. Two units, three batteries. No luck yet and a reduced HDD capacity. Hence the overall rating well below the features/performance/etc. - the very things that got me to buy the unit in the first place.

MSRP: $504.99

not available for sale from
the toshiba online store

  • Laptop summary
  • AMD Quad-Core A6-5200M Accelerated Processor
  • Windows 8
  • 6GB DDR3 1333MHz memory
  • AMD® Integrated Graphics
  • 750GB (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

build your own C50 shop for accessories