Toshiba Satellite C55D-A5382 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Love it!

POSTED BY: INTCMN
Overall rating: 5 out of 5 5 out of 5

The Laptop is very nice! I like the sleek design, but just a little heavy. A bit more portable that would be awesome!

Great Laptop With Amazing Quad-Core APU

POSTED BY: Bukshidow
Overall rating: 4 out of 5 4 out of 5

First off Let me say this. AMD had alot of driver issues that caused of issues with this laptop. lots of bluescreen of death. Which has been fixed mostly. I put a SSD in it and it runs smooth as silk. It does have a quad-core cpu and running windows 8.1 with 8 GBs of ram it runs extremely well for a cheap laptop. It can go up to 16 GBs of ram. In a lot of ways it can outperform a I core 3 CPU. Overall the hardware is amazing its the software that can be buggy. I would recommend putting an SSD in it to provide an even lower power taker.

POSTED BY: i am71 years old; am not computer smart , Shrewsbury, Ma
Overall rating: 1 out of 5 1 out of 5

i find it very difficult to follow window 8.0 I do not even use the computer because of this. I was used to the older format without apps. It is good for some, but absolutely not for me

MSRP: $375.99

not available for sale from
the toshiba online store

  • Laptop summary
  • AMD Quad Core A4-5000M Accelerated Processor
  • Windows 8
  • 4GB DDR3 1333MHz memory
  • AMD® Integrated Graphics
  • 500GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

build your own C50 shop for accessories