Toshiba Satellite C55Dt-A5241 Laptop

Average Customer Rating:

goes great with check to include

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

very good

POSTED BY: cooking , Hampton, VA
Overall rating: 5 out of 5 5 out of 5

Excellent

Overall very good

POSTED BY: Cruzey , Utah
Overall rating: 4 out of 5 4 out of 5

Two weaknesses, processor at 1.4 slow, the other windows 8 is terrible comparable to ME which was terrible.

Not worth the price.

POSTED BY: Unhappy
Overall rating: 2 out of 5 2 out of 5

I bought this laptop thinking it would be decent enough to use for browsing the internet, watching movies, and uploading pictures. However, this laptop has been unable to do any of those things. Trying to watch a TV show on netflix was impossible (and yes, I can watch fine from other devices in the house), even looking through photos that have been uploaded took forever. The touchpad is not very responsive even with the sensitivity turned up, and a lot of the time you have to use the touchscreen to get a response (which is a neat feature, but not overly useful in my opinion). Overall I'm not very pleased with this laptop, and wish I would've read the stores return policy better so I could've returned it.

Not recommended

POSTED BY: cone
Overall rating: 2 out of 5 2 out of 5

I bought this Laptop as my traveling just needed for internet laptop. I figured I could do some light gaming on it as well. Well, the CPU in this laptop can barely run an internet browser, much less anything else. The laptop quality and features not including the CPU are good. I have no other problems to report, but the CPU is kinda the heart and soul of your computer. So, if you just want internet and absolutely nothing more, then this would be a fair entry level computer at best. If you want anything more, I'd look for something with a better processor.

MSRP: $499.99

not available for sale from
the toshiba online store

  • Laptop summary
  • AMD Dual-Core E1-1200 Accelerated Processor
  • Windows 8
  • 6GB DDR3 1600MHz memory
  • AMD® Integrated Graphics
  • 500GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

build your own C50 shop for accessories