Toshiba Satellite C55Dt-A5250 Laptop

Average Customer Rating:

goes great with check to include

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

great value

POSTED BY: ejr , shamokin, pa
Overall rating: 5 out of 5 5 out of 5

I needed to get use to going from pc to notebook, after that everything was ok

mixed feelings

POSTED BY: cam , Fayetteville, nc
Overall rating: 4 out of 5 4 out of 5

Laptop is ok due to its touchscreen and ergonomics keyboard. No Bluetooth and slow loading of apps makes it a little sluggish.

worst laptop i have ever dealt with

POSTED BY: joe , orlando FL
Overall rating: 1 out of 5 1 out of 5

I needed a cheap laptop to get me through one semester of college. so i could save for a better one so i bought this thing by far i have had more headaches with this then it is worth; for the first month it worked okay that month being February . Once march started the laptop started to give me problems to turn on and even recognize windows 8.1, so i ran a few scans and searches and it seemed to work; once April came around the laptop completely crashed and would not turn on at all kept saying cannot recognize windows so i took it to geek squad who recommended i do a reset to factory basics and see if the problems persist. I did so and it worked up till yesterday when the mouse touch pad and touch screen will not work when needed only when they want, so now i must use an external mouse on this laptop. Plus the speakers are terrible and this laptop cannot run even the most basics of games with minimal settings so my experience with my first Toshiba laptop has been a complete failure. Hopefully in a few years they will make a product worth buying unless this is a completely defective model I will not be purchasing any more products from this company.

MSRP: $499.99

not available for sale from
the toshiba online store

  • Laptop summary
  • AMD Dual-Core E1-1200 Accelerated Processor
  • Windows 8
  • 6GB DDR3 1600MHz memory
  • AMD® Integrated Graphics
  • 500GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

build your own C50 shop for accessories