Toshiba Satellite C55DT-A5305 Laptop

Average Customer Rating:

goes great with check to include

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

very good laptop

POSTED BY: JB , Rio de Janeiro-Brasil
Overall rating: 5 out of 5 5 out of 5

Very comfortable to wear . Fast. I rather enjoy

Great unit for the price!!

POSTED BY: wizzo , London, Ontario,
Overall rating: 5 out of 5 5 out of 5

This laptop has lasted all day without plugging it in on wireless (though it was not in constant use) out of the box. I have been able to extend that by using the ECO settings for my battery. The touch screen makes Windows 8.1 very easy to use and I liked Windows XP a lot. I usually run Linux on my systems but I do like this unit with Windows 8 on it. I find it easy to navigate with the touch screen it is like having a tablet with a keboard permenantly attached (in my office that is what I see people doing with thier iPad's) This is great I love it

det5222

POSTED BY: det5222 , Weston WI
Overall rating: 5 out of 5 5 out of 5

Very nice real easy to use we like the touch screen

Great computer-Great Price

POSTED BY: Docked user , Belleville, IL
Overall rating: 5 out of 5 5 out of 5

For the price it's hard to beat! Combination of touchscreen and keyboard using Windows 8.1 is very handy. Computer works great with hardly ever a delay even with several programs running at the same time. Don't know how it would hold up under rough handling as the case is plastic but I haven't had any problems whatsoever. I have it hooked to a USB 3.0 docking station and hooked to the dock functions as a desktop with multiple monitors and printers attached with no issues.

POSTED BY: Lee , Lou.,Ky
Overall rating: 5 out of 5 5 out of 5

bought one for my wife and liked it so much I bought another for myself

Great Product

POSTED BY: mike
Overall rating: 5 out of 5 5 out of 5

Fast, reliable and economical Windows 8 touch screen. Much faster booting and Internet access is a joy to use.

LOVE THIS LAPTOP!

POSTED BY: KDJ22 , Oklahoma City, OK
Overall rating: 5 out of 5 5 out of 5

This is the first laptop that I actually went shopping for others that I've had were hand me downs. Last hand me down was a Toshiba Satellite laptop older model but I loved the performance of it. So went for a newer Toshiba and its awesome!

Very good buy

POSTED BY: Happy User , Greenwood IN
Overall rating: 5 out of 5 5 out of 5

I am very happy with this computer. My only request would be to be able to 'turn off' the touchpad. I am a senior, and much prefer the mouse to the touchpad.

Best Buy

POSTED BY: Terriblew/changes , Newark, NJ
Overall rating: 5 out of 5 5 out of 5

I wasnt quite sure what to expect w/this laptop, and have returned other items because I didnt like them, but I LOVE my Toshiba Laptop!! Very easy, almost like a smart phone, havent had a problem yet!! Its smooth to the touch, and gives me EXACTLY what I'm looking for, and its soooooo (did I mention before) - EASY!@! I HAVE recommended this product, and will surely keep doing so!!

Great Computer

POSTED BY: hdubs , Port Huron, MI
Overall rating: 4 out of 5 4 out of 5

The computer is fast, lasts long on the battery, and light-weight.

Great laptop

POSTED BY: GPO , Cleveland, Ohio
Overall rating: 4 out of 5 4 out of 5

Great laptop for the money. Lots of features and above average performance. The battery life is above average and a pleasant surprise for average use under normal conditions. The touch screen is an added bonus for me.

Good laptop and very fast indeed

POSTED BY: Logik , Tema , Ghana
Overall rating: 4 out of 5 4 out of 5

I bought one recently it so I cant say much but all the same i think its a good laptop. The touch feature is very fast and responsive. To the user who says the sound quality is poor, I wil advice u to run the DTS app (I mean turn it on) and ur sound quality will improve drastically.

awsome laptop

POSTED BY: sam , Spokane WA
Overall rating: 4 out of 5 4 out of 5

I love the fact that i can do apps as well as programs so its like my phone and a laptop. I dont like the fact that ive owned it 2 weeks and it already had an issue with one of the programs and i had to report a problem to fix it when it wasnt my fault. However it was a quick and easy fix which was nice. I have heard alot of complaints about windows 8 so I waited till i couldnt wait any longer for a new laptop because i WAS HANGING ONTO MY XP. but windows 8 took me 5 min to understand and start zooming through it without useing the how too guid. but it took my spouce 3 days to learn because he had it 1st after i explained it he was good to go because he disnt understand that the app page was basectly the start up window. now hes thinng about getting one too.

Love It

POSTED BY: Kissme_Trice , Antioch, TN
Overall rating: 4 out of 5 4 out of 5

So far I really like this pc. Im having a hard time adjusting to windows 8.1 but overall it's nice. The touchscreen is a great feature but I do still enjoy the regular mouse and keyboard. The battery does pretty well but per usual windows there's some freezing or crashing. It's not noisy, thank God! The keys tend to stick a little. Some times it takes a couple hits to get a letter to come up. For what I spent I couldn't ask for much more!

Great machine, but "Toshiba Start" aggravates me.

POSTED BY: Tony in Houston , Houston, TX
Overall rating: 4 out of 5 4 out of 5

This really is a great, fast laptop. My only complaint is that the "Toshiba Start" program interferes every time I move the mouse--and there's no way to disable this feature. I'm referring to the menu bar that appears on the right side of the screen every time I move the mouse cursor. This is a very frustrating feature, and I NEVER use it.

Love it's quickness!

POSTED BY: alpha86 , New York state
Overall rating: 4 out of 5 4 out of 5

My only complaint is that the keyboard is poor to the touch. VERY often I have to go back over a piece to insert letters not typed, even though I know I have hit the key. Otherwise, I love it!!

Trouble adjusting

POSTED BY: none
Overall rating: 4 out of 5 4 out of 5

Last computer had Vista operating system. Windows 8 I'm sure will do so many more things but I am having trouble adjusting.

Satellite

POSTED BY: Docoben , Phoenix, AZ
Overall rating: 4 out of 5 4 out of 5

Nice easy to read touch screen.

what i thnk

POSTED BY: la bellezza dentro , indianapolis IN
Overall rating: 4 out of 5 4 out of 5

Im pretty satisfied with it

good value

POSTED BY: Oreo , Colorado
Overall rating: 4 out of 5 4 out of 5

Good budget laptop, windows 8 takes some getting used to, but the laptop performs well.

Good performance and very good graphics

POSTED BY: Philos_in_quest , San Ysidro, CA
Overall rating: 4 out of 5 4 out of 5

Overall this computer is worth the price, the touch features and performance of the processor is excellent, but get is laggy when you conect to the internet, but i recomend this computer.

Very Happy

POSTED BY: simply satisfied , Hollidaysburg,PA
Overall rating: 4 out of 5 4 out of 5

Very happy with this laptop, was apprehensive going from my desktop to a laptop and I'm very satisfied with this product. Easy to use, and I like the app style home screen.

1 major flaw

POSTED BY: cowboy , St Paul, MN
Overall rating: 4 out of 5 4 out of 5

This laptop would be perfectly acceptable except for one HUGE flaw. The sound chip functions about as well as a tin can on a string. It literally sounds about that bad. It's tempting to think the speakers or the driver are the issue, but after finding some other reviews, reloading the drivers, and trying an external USB sound device, it's clear the problem is inside the machine and specific to the sound chip. It's actually difficult to listen to any sound output, either from the speakers or the sound jack. It is literally the WORST sound I've ever gotten from any digital device I've ever owned. Otherwise, the performance is fine for web surfing, general tasks, etc. The touch screen works perfectly. Any issues are more related to Windows 8 and its limitations (that it imposes on how you access things). Battery life is good, even better if you use power saver settings. I really want to like the machine and recommend it but the sound issue is too big a hurdle. For an extra $5, why couldn't they put in a functional chip!?

Looking for a solid laptop...look no further..

POSTED BY: ToshiRobbi , Orlando, FL
Overall rating: 4 out of 5 4 out of 5

Can't beat it...and I will purchase their tablet in the near future.

Great value

POSTED BY: symeta
Overall rating: 4 out of 5 4 out of 5

Good laptop. love the touch screen. good sound. reasonably fast. good for the price. It is my 4th Toshiba.

guide for win8

POSTED BY: grayfox
Overall rating: 3 out of 5 3 out of 5

Open box ....no info no guide ....NO HELP

Frustrated during first week!

POSTED BY: Janesa , Denver, CO
Overall rating: 3 out of 5 3 out of 5

We used our NEW computer for exactly one day before it quit working. Had to take it for service and found it CAME with malware. Unfortunately malware isn't covered under the warranty. You would think a new computer that comes preloaded with a anti-virus software wouldn't have a virus. After the computer was fixed, we are very pleased.

not exactly what i expected

POSTED BY: laptopdj , sanford floida
Overall rating: 3 out of 5 3 out of 5

sound quality when hooked to external speakers has no bass and sounds like a phones sound recorder. thought that was a standard feature. I bought the laptop for music related purposes, now I cant enjoy it

Good Laptop

POSTED BY: dan , Ghana
Overall rating: 3 out of 5 3 out of 5

After using the product for sometime i realized one screw was not in place. And I bought the product brand new, out of its box. Also if a provision was made so that the touch screen can be turned off, would have been better because sometimes i wished it could be turned off.

POSTED BY: oldman , Bothell, wa
Overall rating: 3 out of 5 3 out of 5

My computer is blinking a lot and eventually it dies down. It doesn't seem that fast.

POSTED BY: j
Overall rating: 3 out of 5 3 out of 5

too many problems the laptop as layout is standard so it is ok but windows has problems running i do not like thestart screen

Laptop Review

POSTED BY: College Student , Jackson, MS
Overall rating: 2 out of 5 2 out of 5

While the fat that the computer is a touch-screen is cool, it gets very annoying when I'm on the internet using the touch-screen and it suddenly switches me to the home screen for no apparent reason. It is also AWFUL to type on and I have to hit the letters several times for it to show up which does not work well for writing papers.

Huge disappointment

POSTED BY: Nykole , Chicago, IL
Overall rating: 2 out of 5 2 out of 5

After reading other reviews, I'm wondering if I got a defective product. This is the first time I have bought a new laptop that was slower than my 4-year old laptop. There is frequently a delay when the computer responds as if it is trying to decide if it is receiving a touch command or a keyboard/mouse command. If I have 2 apps running at once, the machine runs very slow and often freezes. The internet feels very sluggish and runs much faster on a different laptop on the same network. Wishing I had opted for a faster processor rather than a touch screen.

Less than reliable

POSTED BY: Mark , North Texas
Overall rating: 2 out of 5 2 out of 5

This is my second Toshiba Laptop. The first one failed about 2 weeks out of warranty. This one failed after 5 weeks. When working they were very nice. I would recomend finding a computer with Win 7 Pro instead of the horrible joke that Microsoft is pushing in Win 8. Got to be worst experiance ever!

Worst piece of equipment ever in 40 years

POSTED BY: mema , Sonora, CA
Overall rating: 2 out of 5 2 out of 5

I have been extremely disappointed with this product. Getting this with windows 8 after using the ease of using windows 7 was beyond frustration. Hours of trying to find what you wanted compared to how it was done is unbelievable. Although I had called to have it sent back, I am by nature not letting this beat me......sooo I am going to PAY someone to show me how to navigate on this horrid thing. I don't think it can be done but here goes.........

MSRP: $514.99

not available for sale from
the toshiba online store

  • Laptop summary
  • AMD Quad-Core A6-5200M Accelerated Processor
  • Windows 8.1
  • 4GB DDR3 1333MHz memory
  • AMD® Integrated Graphics
  • 750GB (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

build your own C50 shop for accessories