Toshiba Satellite C75D-A7370 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

great laptop

POSTED BY: k9hnlr , Sheboygan, WI
Overall rating: 5 out of 5 5 out of 5

This is a great laptop for the price. Starts right up and connects to the internet fast. Have had no problems what so ever. use it for browsing the internet and the web pages pop right up. Don't have to wait for a page to download. Would recommend this laptop.

So Far So good

POSTED BY: CollegeStudent
Overall rating: 5 out of 5 5 out of 5

Laptop has pretty good battery life. Windows 8 is kind of a pain at first. I don't do any gaming or anything like that but I do use multiple windows and programs at once and it seems to be great dealing with that so far. Also doesn't seem to overheat at all sitting on my lap.

Nice Computer

POSTED BY: Baconcooker , Madelia, MN
Overall rating: 5 out of 5 5 out of 5

If the laptop did not have Windows 8.1 it would be awesom. Too many programs that I have that are written for 8 don't work.

So far...great!

POSTED BY: thanny , Easman, GA
Overall rating: 5 out of 5 5 out of 5

Have not had any issues so far...has performed without any problems. However, the how-to-use function of the on-line support is not very easy to understand, even though I have not yet had any need. Since it is a new unit, I am unable to adequately judge "battery life," so entered "poor" on survey...Sorry, but you insist on an answer.

BEST LAPTOP

POSTED BY: BOWTIE , INDEPEDNENCE MO.
Overall rating: 5 out of 5 5 out of 5

VERY NICE EASY TO USE LOVE THE KEY BOARD AS ALWAYS TOSHIBA DOES IT AGAIN THIS IS MY 2ND LAPTOP FROM TOSHIBA THANKS LOVE IT.

My Puter

POSTED BY: Momma J , Somerville, TN
Overall rating: 5 out of 5 5 out of 5

I love it, but had major problems at first and had to return for a replacement twice. So far, this one is working great!

best for market price

POSTED BY: boogie man , canton michigan
Overall rating: 5 out of 5 5 out of 5

none

Satellite C75D-A7370

POSTED BY: piniella
Overall rating: 5 out of 5 5 out of 5

This laptop makes Windows 8.1 easy to use. The screen is a great size for someone who needs slightly larger icons. The RAM (8 GB) and the HD (750 GB) are more than enough for my current needs.

Delighted

POSTED BY: niteowl , Lake Orion, MI
Overall rating: 5 out of 5 5 out of 5

This is my first laptop and I am very happy with it. I know I haven't even scratched the surface of what its capabilities are, but I'm looking forward to learning more each time I use it. I will be using it mainly for my photographs and editing and creating with them and the amount of memory it has and the hard-drive are perfect for what I need. I am very excited and plan to create great things on my new Toshiba Laptop!

Great Laptop - Fair Price

POSTED BY: Tomcat104 , Charlotte, NC
Overall rating: 5 out of 5 5 out of 5

This has been a great laptop at a reasonable price. I was "leary" of an AMD processor at first but it has performed as well as my previous Intel i5. I'm more than pleased and would recommend it to a friend.

Satisfied Customer Here

POSTED BY: Jake's wife , Matteson, IL
Overall rating: 5 out of 5 5 out of 5

When my old computer died I was in dire need of a replacement. I tried to do my homework and checked Consumer Reports. They had good things to say about Toshiba computers so I decided to replace my Gateway... Two months have elapsed and I'm happy with my purchase: a C75D-A7370 Laptop. I had problems only with Windows 8.1 and Office 2013 as they are both revised versions. I'm working on both of them and enjoying the adjustment to my new computer.

A Great Laptop

POSTED BY: Sally , Eastern NC
Overall rating: 5 out of 5 5 out of 5

This laptop has a great keyboard and monitor plus it's lightweight and the price was right! Still learning Windows 8, but that will come........

Toshiba Satellite C75D-A7370 Laptop

POSTED BY: don , lexington,sc
Overall rating: 5 out of 5 5 out of 5

works great. have had no problems.

great first laptoop

POSTED BY: Sgt sheridan , New Britain Ct 06053
Overall rating: 5 out of 5 5 out of 5

I bought this to teach my grandson the right way to use a computer and how important keyboarding is. How ever, the keyboard compared to a regular keyboard made it harder to teach vs a standard keyboard . Also to many pop ups vs the desk top I do most of my stuff on in my home. but all and all its really noce, super screen. Kerry Sheridan

"Getting to know you"

POSTED BY: Candylions , Redondo Beach, CA
Overall rating: 5 out of 5 5 out of 5

My review is that of a "novice" so there is no tech talk. I'm at the mercy of Windows 8.1 I find this computer a bit touchy as far using a mouse. I will assume this is an 8.1 problem and not Toshiba. It never runs hot, keys are very comfortable to use and I like the "on" button , it's larger and lit..it connects to the internet instantly ...loads and downloads faster than my last Toshiba (which I also loved and still use). You get more for your dollar.

Love it!

POSTED BY: Reecie , Brookville, Ohio
Overall rating: 5 out of 5 5 out of 5

It does everything I want it to do, but I can't download the latest Adobe for videos, etc because it says there's a virus. I'm using something else, but it doesn't cover everything. It took a lot of doing to get Chrome off my last laptop, so that's not an option. It's fast enough for what I need. Great screen! I kept looking until I found the right Toshiba for me because they have always worked great. I didn't see any reason to buy another brand and have it sitting in a corner not working (like my Acer). And I realize Windows 8 design is not Toshiba's fault. But I would like to say that I would like to have had a hand in designing it for free and they paid people to screw it up!

POSTED BY: Sfamily , Texas
Overall rating: 5 out of 5 5 out of 5

Running pretty smooth. Windows 8 works better with a touch screen but adjusting after many years on XP. so all in all great lap top.

Sturdy Built Laptop

POSTED BY: Big Daddy
Overall rating: 5 out of 5 5 out of 5

Nice clear screen, nice size keyboard, easy to use.

Loving the big screen

POSTED BY: Jude , Kenosha, WI
Overall rating: 5 out of 5 5 out of 5

I am very pleased with this pc. For someone with limited eyesight the larger screen is wonderful. Little by little I am learning Windows 8.1, but I have lot more to learn.

Nice Laptop

POSTED BY: Skuguy , Ocala, FL
Overall rating: 5 out of 5 5 out of 5

Laptop was easy to setup and did not have a lot of needless "bloatware". It came with win 8 and I immediately upgraded to win 8.1 with no issues. I am pleased with the speed and the value for the money.

C75D A7370

POSTED BY: trout120 , CLAREMORE, OK
Overall rating: 5 out of 5 5 out of 5

TOSHIBA IS A WONDERFUL LAPTOP.THE SUPPORT CHAT ONLINE IS OUTSTANDING.

Gret Laptop

POSTED BY: Al , South Houston TX
Overall rating: 5 out of 5 5 out of 5

This laptop works better than I though it would. The start up time is far better than I have experienced before in the three other laptops I have owned. also I really enjoy the large screen. For the price it was cheaper than any other laptop I looked at.

Nice for the price

POSTED BY: Cramps
Overall rating: 5 out of 5 5 out of 5

I wanted a laptop with a bigger display. So the 17 inch fit my needs. I also wanted a laptop that was easy to maintain myself. Take out a few screws on the back side and you have easy access too both the RAM and hard drive. Kudos for that. Also this Laptop is running the 64 bit OS and surprisingly the mother board included in this build will accommodate up to 16 gigs of RAM. The laptop cam from the factory with 8 gigs. It's nice to know if I need that much I can do so with ease. Also if I want to go with a SSD I can gain access to the hard drive in just a few moments.

Best Laptop Ever

POSTED BY: Mom , Gloster, LA
Overall rating: 5 out of 5 5 out of 5

I love the convenience of using my laptop anywhere

Great Value, best laptop

POSTED BY: Student
Overall rating: 5 out of 5 5 out of 5

Best value even if I had paid a couple of hundred more. Win 8 will take some getting used to, however, in this day of smart phones, anyone familiar with smart phones should take to this in reasonable learning curve. I am very pleased. For the next 3 years of school...this is perfect. For entry level....Ok, for Mid level like me...great...for experienced level, maybe too basic.

POSTED BY: Bob , Farmington, MO
Overall rating: 5 out of 5 5 out of 5

I am very satisfied with my laptop.

Love it!

POSTED BY: kw , Memphis, Tn
Overall rating: 4 out of 5 4 out of 5

Everything I expected. My first laptop - need to get used to the keyboard but otherwise no problems. Screen seems huge - have traveled with it without problems.

Good Deal

POSTED BY: AriesMatt , Diamondheadh, MS
Overall rating: 4 out of 5 4 out of 5

There are few of areas for improvement on this laptop: 1. The sound quality could be better. My old XP Gateway had much better sound when using quality headphones, which is how I listen to audio on laptops. 2. Battery life could be better. 3. Some programs run a little sluggish. Could be that they are older versions not designed to run on Win8, but don't have problems on my desktop. 3. A shutdown button on the task bar (see Gateway products) would be very helpful. Other than these few things, product works great.

new Laptopt

POSTED BY: Tom , Wofford Heights, CA
Overall rating: 4 out of 5 4 out of 5

I do enjoy my new laptop and I did have a problem, however I went to the Toshiba Tec dept. and they were able to correct everything and I am up an rolling. Good piece of equipment.

internet explorer

POSTED BY: chuck , st. peters,mo
Overall rating: 4 out of 5 4 out of 5

I lose internet explorer when I am playing games on facebook

Toshiba Good Product for Cost

POSTED BY: Loyaluser , Tucson, AZ
Overall rating: 4 out of 5 4 out of 5

Generally, I really love Toshiba's. The new keyboard is an improvement over my other in which my fingers were getting stuck. Love the hardware; not so fond of the operating system! Please don't put a problematic operating system on the units.

Toshiba laptop

POSTED BY: smashedguy , Baltimore, MD
Overall rating: 4 out of 5 4 out of 5

bought it in a hurry because I needed a laptop immediately. No time to review. It is a neat machine with a wide screen, which is a plus: more real estate to work with. The processor is quite fast, and memory is adequate for most computing needs. The keyboard has large keys, which is good but the middle keys stick, especially the N and C keys. This is very annoying and I do not know how to fix it. Hard drive is quite adequate. Weight is very good : light. Size is a bit cumbersome, but that's what you get if you want a larger screen.

Great Laptop

POSTED BY: Erab , Rockford, IL
Overall rating: 4 out of 5 4 out of 5

I am very happy with my Toshiba Laptop, performance is excellent and is fully capable of doing everything I would expect. The only thing I don't like is Windows 8. I wish I could have purchased it with Windows 7. In fact I will soon be switching it to Windows 7 and will then have what I consider a perfect laptop.

Gets The Job Done!

POSTED BY: Back In School Mom , Atlanta, GA
Overall rating: 4 out of 5 4 out of 5

I'm one of those late bloomers so I just started my second year of college after taking a break and new I needed another laptop. My precious children took over the one I had during my first year and it gave me so many problems that I didn't mind. I wanted a Sony VIO but the salesperson showed me the Toshiba. I hadn't heard bad or good about it and the price was very good so I decided to try it. I love the big screen and so far its done a great job. I won't allow my kids to touch it so I haven't gotten the chance to see how well it holds up to viruses. When I get ready to purchase my next desk top, Toshiba will definitely be in the running.

good laptop

POSTED BY: starbfly , kiissimmee fl
Overall rating: 4 out of 5 4 out of 5

love it for a big screen laptop it's light weight

Slow for games.

POSTED BY: Matrix , Sioux Falls, SD
Overall rating: 4 out of 5 4 out of 5

Good features for the price, but it does not have enough speed for games like World of Warcraft. Streaming video works fine.

Good laptop but

POSTED BY: Bella , Colorado City, TX
Overall rating: 4 out of 5 4 out of 5

The laptop is good and will do everything I ask it to do but my husband and I hate the games! Had an HP previously and loved the solitaire and majong games but I hate the Tangent games. Give me a choice, do not make me put up with the ridiculous games on this laptop! Give me my games BACK!

Good value but

POSTED BY: yoaklar , Sacramento, ca
Overall rating: 4 out of 5 4 out of 5

Great laptop for the price. Only complaint I have is the wifi card is really weak and has troubles staying connected to certain routers.

Could use some work

POSTED BY: Sally , Pocatello, ID
Overall rating: 4 out of 5 4 out of 5

Keys are hard to push down. I'm an accomplished typist (120+ words per minute and this keyboard has got me down to half that). Space bar also hard to use. Why are the cases always black? How about blue, orange, white, yellow, pink, anything but black! It's heavy. R&D should be looking into fining lighter materials. Otherwise, it does beat my old desktop - but can't hold a candle to my ergonomic keyboard.

very good laptop

POSTED BY: olddxer
Overall rating: 4 out of 5 4 out of 5

laptop has performed well, no real issues, just not a fan off windows 8.

Not Toshiba's Best

POSTED BY: vegasmattaes , Alexandria, VA
Overall rating: 4 out of 5 4 out of 5

The keys are sticky and mushy - problem with the "0" key on the number pad and the "S" key sometimes enters a letter twice. The all plastic keyboard surround is really cheap and stains with skin oil instantly. Performance-wise it is a good machine if you get rid of the WIndows 8 and install 7, dump Norton (trial version - really?) for ESET, and disable the Windows Defender package.

Very Good Laptop

POSTED BY: Golfguy
Overall rating: 4 out of 5 4 out of 5

It runs pretty fast and smooth. No problems.

So far only one issue

POSTED BY: Mickey , Chicago, IL
Overall rating: 4 out of 5 4 out of 5

I wish that we could easily get rid of all the unwanted WIFI Connections that show up when I connect to my hot spot. Some of the names are pretty vulgar. I don't need to see 50 to 75 other wifi spots around

Very good lap top but with one reservation

POSTED BY: Draco , Bullhead City, AZ
Overall rating: 4 out of 5 4 out of 5

Overall I like the Toshiba C75D-A7370 lap top a lot. With one reservation. Previous I have always used desk top computers with a separate keyboard. I am having trouble adjusting to the lap top key board. As I have to really hit the keys in order to insure that my stroke registered. And I am having to do a lot of proof reading and fixing as a result. Maybe with time and experience it will get easier. I hope so. Otherwise it would be a ten.

Great Laptop

POSTED BY: rrwallis , Buchanan Lake, Tx
Overall rating: 4 out of 5 4 out of 5

I am very pleased with this Laptop in general, but I find it deficient in one respect. The sound volume is inadequate. This PC replaces an older Toshiba that I used for several years. I had a couple of small, USB powered, external speakers connected to the headphone jack and it worked very well with great volume. I tried those speakers with this PC and the volume is inadequate. I checked the Toshiba instructions and found that Toshiba recommends externally powered speakers for use with this PC. Since that time I have purchased two different sets of externally powered speakers. And while the volume is better it is still not adequate, nowhere near the volume level of USB powered speakers on my old Toshiba laptop.

very good

POSTED BY: gpjrock , springfield MO
Overall rating: 4 out of 5 4 out of 5

every thing works grate for the price and is made very will.

Average Across the Board

POSTED BY: Doc
Overall rating: 4 out of 5 4 out of 5

Let's talk about the Pro's first. Nice keyboard, very similar to a traditional desktop keyboard so it's easy to get used to. Batterly life is very good at 4-5 hours. Mine came with Windows 8.1, so that was a bonus of not having to download the service pack to get it. Very light weight for the size. Does not run too hot. Cons: extremely plasticy, feelds pretty cheap. Touch pad is mildly annoying but may be able to be tweaked a bit. The screen goes very light or dark if you move your head even the slightest bit, so that gets old. The speakers are the worst I've ever heard on a lappy. Even what the onboard soundcard pipes out through the head phone jack is terrible. 8GB DDR3 and 1GB of video memory should be sufficient for games but it's not on this model. The FPS suffer badly with 2005 games and you have to run everything on low. For an average connect to the internet computer or word processing it would be great. Just not very good at all for any kind of games.

Decent for price point

POSTED BY: Dixie , Wisconsin
Overall rating: 3 out of 5 3 out of 5

It is a decent laptop for the price point. No frills, light weight, large screen laptop. No backlight on keyboard. Widows 8 is annoying , but that isn't the fault of the laptop manufacturer. I needed the machine mostly for word processing, so it works well enough for that. Not a good machine for heavy graphics or anything you do lots of downloads.

Worst Keyboard Ever

POSTED BY: LG , New Mexico
Overall rating: 3 out of 5 3 out of 5

I have had good experiences with Toshiba laptops, so I thought that this seemed like a good value for the RAM/Harddrive/Price proposition. In general it seems like it has decent performance. But the keyboard is absolutely, positively the worst I have ever experienced. The keys are large and have to be pressed very hard to work. It simply does not work for touch typing. Just typing this review I had to go back and fix over a dozen letter omissions where the key did not engage enough to type the letter.

I just don't know

POSTED BY: Scotty , Greensboro, NC
Overall rating: 3 out of 5 3 out of 5

Having had a computer with Vista and my work computer with Windows 7, the transition to Windows 8.1 has been very fustrating. I cannot tell at the point if I like the computer or not.

Is Okay

POSTED BY: GiGi , Longs, SC
Overall rating: 3 out of 5 3 out of 5

Its Okay biggest thing is Windows 8- this is a computer NOT a smart phone! Apps that cost extra is not fun. It was an unpleasant surprise that there was only Wordpad and no real word document processor without paying an extra $100 for Microsoft Office! Also the case seems cheap- very plastic and doesn't seem as sturdy as the one I had to replace due to theft.

bad laptop

POSTED BY: Maryanne , PA
Overall rating: 3 out of 5 3 out of 5

the laptop had to be returned in a matter of three weeks the laptop operating system went bad and I am trying another new one and hope this lives up to my expectations. I do not like the windows 8 but I am try to perservire and learn the new system. here is hoping things work out

Good lap top but

POSTED BY: cowboy Pete , chico, ca
Overall rating: 3 out of 5 3 out of 5

The lap top is very good but I need you to tell me how to get Outlook Express e mail on it. I have it on my old computer for my E mails so it is important you get back to me. If you do not get back to me then my review is bad not very good. Also quit quit quit sending me any further E mails. Also quit quit quit sending me any further E mails.

Windows

POSTED BY: A , Huntsville, TX
Overall rating: 3 out of 5 3 out of 5

Have gone to windows 8.1 because that's what the new computer had on it. It's a major leap into the unknown from XP and windows 7 which we have on 2nd laptop. Big problem is the incompatibility with previous programs. Try to download drivers to increase compatibility, with no luck. Had to go to Tech Help to download Microsoft office and virus protection. It's getting better but still really confusing.

Slow loader

POSTED BY: NanaNancyG , Indiana
Overall rating: 3 out of 5 3 out of 5

Sometimes it takes forever to load a page on windows 8.1 satellite . I have inquired about this problem and I am not the only one having this problem. I also have a problem with typing on it. It doesn't like you typing fast because it misses letters.

2nd Toshiba Laptop

POSTED BY: East Coast User , Hampton, VA
Overall rating: 3 out of 5 3 out of 5

This is a replacement for the Toshiba laptop I purchased in 2010. The motherboard on the old laptop died unexpectedly. I decided to purchase the same model since the other one had treated me so well. The quality on the new laptop is so disappointing. For example, the speakers sound "tinny", the keys stick and there is no manual volume control. So many of the small features I had are gone on the new model. The price is comparable to the other brands with the same options, but hopefully this new one will last as long as my prior one.

keys

POSTED BY: bubba , milton fl.
Overall rating: 3 out of 5 3 out of 5

on my computer when i press one key it types another

hated it

POSTED BY: joe , kingston, WA
Overall rating: 3 out of 5 3 out of 5

While the new laptop is faster, I would take back my old desktop in a heartbeat. I finally hooked up a mouse which made things easier. I print a lot so I have to run into where the printer is and hook the laptop up all the time - the printing options are not the same so I can't get what I want. The old print program let me choose the size of the picture - 8 x 10 - 3 x 5 - etc. - now there is a long list with mostly centimeters.

Great except...

POSTED BY: TC , va beach, va
Overall rating: 3 out of 5 3 out of 5

Ram, HD, screen clarity, overall speed all great...however, drops wireless internet connection too often thus requiring a reboot.

first time laptop user

POSTED BY: Dan p , Texas
Overall rating: 3 out of 5 3 out of 5

I'm used to desktop, had to get the mouse option. I find windows 8 difficult to adjust to, and the keyboard on the laptop very difficult to use even though I am proficient in typing. Some of keys you have to hit extra hard to input key stroke. The feel of the keyboard is nothing like a desktop even though the size of this laptop makes the keyboard large enough. I guess my biggest complaint is the keyboard. Other ratings such as battery life I'm not experienced with laptops so can't give honest rating on.

Great Value.

POSTED BY: Rico , Faribault, MN
Overall rating: 3 out of 5 3 out of 5

This computer worked Ok out of the box. The only problem I found was the sound card has absolutely no dynamic response. So if you are going to plug it into an amplifier or headphones to enjoy your favorite tunes you will be extremely disappointed.

slowest laptop

POSTED BY: bill , cleveland, oh
Overall rating: 2 out of 5 2 out of 5

very disappointed in the speed. very very slow processor. windows 8 totally frustrating. the screen is nice. But the speed should be much faster.

Worst laptop ever

POSTED BY: Me , Delray beach fl
Overall rating: 2 out of 5 2 out of 5

Very confusing to understand. Keep losing site that you are on.

Slowest computer ever!

POSTED BY: JohnnyO , Port Charlotte, FL
Overall rating: 2 out of 5 2 out of 5

Of all the computers I have owned and used, which is many, this one is the slowest I have ever experienced on start up. With what comes in this computer it should be the fastest. Yes, I am very disappointed.

Keyboard Problems

POSTED BY: BC , Charlotte NC
Overall rating: 2 out of 5 2 out of 5

The keyboard is horrible. The keys do not consistently work when pressed. I continually have to retype and correct spelling due to this problem! Very Poor Quality!

Disappointing

POSTED BY: none , Albuquerque, NM
Overall rating: 2 out of 5 2 out of 5

Liked the feel, fit and overall finish of the produce. I was replacing an HP Pavilion which suffered the famous video display fail. I could not touch type on the newer HP keyboard purchased the Toshiba instead. The disappoint is in the performance despite being a quad core with lots of memory and big hard drive the actual performance is pretty bad. It's only fair as a web surfer but you cannot play a game of any speed. The second is I touch type and I can actually type faster than the laptop can respond if I have any windows open for the internet. This is getting very frustrating I would also wish for a backlit keyboard (that was my miss for not checking).

Decent

POSTED BY: Jay
Overall rating: 1 out of 5 1 out of 5

A decent computer...nothing flashy...but, the sound from the speakers is very, very tinny. Considering a return because of the sound.

Windows errors from first start up

POSTED BY: Utahst
Overall rating: 1 out of 5 1 out of 5

Received the blue screen of death from first start up. After 3 resets of Windows 8 and continued errors I returned the laptop. I have had Toshiba laptops before and was extremely satisfied but this one I wouldn't recommend.

retured nonworking new toshiba C75D to store

POSTED BY: b , charlotte nc
Overall rating: 1 out of 5 1 out of 5

I think hard drive was the problem. freeezes, not starting up, keyboard problems, touch pad not working, etc. Got error messages about hard drive.

Worse lap top ever

POSTED BY: didi , warner robins, ga
Overall rating: 1 out of 5 1 out of 5

I've only had it for about 1month or so, and it starts Internet explorer slowly, not to mention gets stuck while using.

MSRP: $535.99

not available for sale from
the toshiba online store

  • Laptop summary
  • AMD Quad-Core A6-5200M Accelerated Processor
  • Windows 8
  • 8GB DDR3 1333MHz memory
  • AMD® Integrated Graphics
  • 750GB (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

build your own C70 shop for accessories