Toshiba Satellite C855-S5349 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Great Laptop, Excellent Value

POSTED BY: Emjay , Portland, OR
Overall rating: 5 out of 5 5 out of 5

This laptop does everything I need it to do. The HDMI port is great to connect to my HDTV to view Netflix on-line. The USB 3.0 will be handy as new devices become available. The touch pad works very well. The Intel Pentium Duo Core B980 processor will provide me all the power I need now and into the future. It is lightweight, and does not get hot sitting on your lap. The wireless is very sensitive and easily picks up the wireless router in my house. The only negative comment I would have is the sound from the speakers is less than satisfactory. Overall I really like this laptop. Now Windows 8 is another story. At this point, I really dislike it, and I am sure that it is a learning curve for me. But Microsoft has some really annoying features they need to fix, like the disappearing scroll bar.

excellent laptop.

POSTED BY: Yam , Fremont, CA.
Overall rating: 5 out of 5 5 out of 5

The satellite null laptop is a excellent computer. I will recommend this products to all my friends.I always keep the brand name--Toshiba on my listing to buy.

good laptop

POSTED BY: pappy , los angeles,ca.
Overall rating: 5 out of 5 5 out of 5

like the laptop,but still trying to learn windows-8

My 7th Toshiba Laptop

POSTED BY: kallstate , Santa Cruz, Ca
Overall rating: 5 out of 5 5 out of 5

I saw a great price on this Windows 8 laptop and decided to try another Toshiba. This is my 7th one. I am keeping my old one as a backup and I usually recycle my old ones through my family. I would recommended Toshiba to anyone.

Excellent laptop

POSTED BY: MGP , Pismo Beach, CA
Overall rating: 5 out of 5 5 out of 5

Excellent laptop for the price.

Love my new laptop

POSTED BY: CyndiLouWho , Fairfield, OH
Overall rating: 5 out of 5 5 out of 5

My husband got me a new Toshiba Satellite Laptop. At first I was intimidated by it, but since I've been using it, I love it! I'm glad he bought this one for me. I'm learning something new every time I use it! Thank you Toshiba; & thank you my husband for choosing this Toshiba!!

Great Satellite Laptop

POSTED BY: Peppermint Patty , Fairfield, OH
Overall rating: 5 out of 5 5 out of 5

My new Satellite laptop is the best! It beats my old, slow laptop by far. I love the texture of the keyboard pad. The battery life is excellent--I was using the battery without realizing it & after 3 1/2 hours, I was warned to plug into power before my laptop shut down. I highly recommend this to anyone looking for a new laptop!

first and best laptop I ever had.

POSTED BY: woodsman , San Diego
Overall rating: 4 out of 5 4 out of 5

yes,I like the laptop, its easy to move around not to heavy.Its brightness and claridy makes it easy and simply to use and I think its its the best thing I have ever brought for myself. thanks again

HATE WINDOWS 8

POSTED BY: SWABBIE , SEWELL,NJ
Overall rating: 4 out of 5 4 out of 5

LOVE THE PRODUCT; LOVE TOSHIBA PRODUCTS; UTTERLY DESPISE WINDOWS 8

Nice Labtop

POSTED BY: Dave , Chicago
Overall rating: 4 out of 5 4 out of 5

It is a pretty good product.

Great Laptop for the price

POSTED BY: momma , williamsburg, va
Overall rating: 4 out of 5 4 out of 5

Love this lap top. Easy to use, just wish it had keyboard back light. Maybe it does and I just have not figured it our yet!!!

Great Laptop

POSTED BY: JVJY , Amarillo, TX
Overall rating: 4 out of 5 4 out of 5

I really like my Laptop.

Ok laptop

POSTED BY: Rambo777 , TX
Overall rating: 4 out of 5 4 out of 5

While the machine is Ok Widows 8 is absolutely and horrendously horrible. While the OS is not Toshiba's fault it is theirs for choosing it. Toshiba could fix this by offering us Windows 7 or Linux to replace this awful Windows 8.

toshiba laptop i purchased

POSTED BY: sydney , indianapolis,in
Overall rating: 3 out of 5 3 out of 5

had to return to purchase point. the sound on laptop was atrocious.

Decent for the price.

POSTED BY: Shadow2
Overall rating: 3 out of 5 3 out of 5

The laptop I purchased was missing some key functions which were available from the competitor for just a little more in cost. An over site on my part.

Laptop

POSTED BY: Jo , Peoria, Az
Overall rating: 2 out of 5 2 out of 5

The laptop may be fine without Windows 8. It is very sensitive with 8 and very difficult to use. I have lost documents right in the middle of typing them. Not a good feature.

Just Okay

POSTED BY: Together Shopper , Bridgeport, PA
Overall rating: 2 out of 5 2 out of 5

This laptop seemed okay but had a two draw backs for me. One was the sound/speakers are awful. I thought for the brand they would be better. The look is clean and simple which was fine. I think what really made me return it was what I paid for it. A friend had a better machine and paid close to $100 less. So that was my deal breaker.

Had to return laptop

POSTED BY: 3MMOM , PITTSBURGH,PA
Overall rating: 1 out of 5 1 out of 5

I was really disappointed in this Toshiba laptop. It would not hold a charge, kept shutting down so I had to return it. This is the third Toshiba that has had problems and I was not able to use them. At this point I have lost faith in Toshiba and will not buy another one.

MSRP: $429.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Pentium® Processor B980
  • Windows 8
  • 4GB DDR3 1333MHz memory
  • Intel® Integrated Graphics
  • 500GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)