Toshiba Satellite C855-S5349N Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

good laptop

POSTED BY: marilearsi , Morovis P.R.
Overall rating: 5 out of 5 5 out of 5

Me gusta

Excellent lap top

POSTED BY: diver , Alturas, CA
Overall rating: 5 out of 5 5 out of 5

Best investment I have made thank you for such a good product.

Good so far

POSTED BY: fxp7305 , riverton, wy
Overall rating: 5 out of 5 5 out of 5

I am new to the laptop experience. I really need an instruction manual on real paper to figure things out but am slowly finding my way around. As for the product itself I am impressed with the functionality.


POSTED BY: Coop , Keanee, IL
Overall rating: 5 out of 5 5 out of 5

I've had dell and hp and so for this is the best computer or lap top I've ever owned , lettering is large enough to read

pretty good laptops

POSTED BY: jerkoff88 , Rosenberg,Texas
Overall rating: 5 out of 5 5 out of 5

easy to use /light weight/built in webcam/microphone/camera/video player/DVD player/WIFI capabilities/longer battery life/built in speakers and easy to press down keyboard/and I just like it better than any other laptop on the market today...Toshiba has always been my favorite brand when it comes to laptops and pcs and digital electronic products ,and cell phones

Good product

POSTED BY: Dan , cab
Overall rating: 5 out of 5 5 out of 5

The computer does everything I want. Once I have figured out Windows 8, to operate the computer. In October 2013, Microsoft is selling Windows 8.1. What a bummer!

best laptop

POSTED BY: babygirl , gonzales,louisiana
Overall rating: 5 out of 5 5 out of 5

This the only brand computer I buy

Nice Labtop

POSTED BY: Harmuffin , Grenada,MS
Overall rating: 4 out of 5 4 out of 5

Overall this is a nice laptop with nice features, but when I first got this laptop, the internet connection would drop and not connect back even if I restarted it. I learned I had to update my wireless router. Now that that problem is solved, I'm currently suffering from a different problem. The laptop randomly shuts down. Overall this is a good labtop with great features, but with some quirks.


POSTED BY: jd , N.newton,ks,
Overall rating: 4 out of 5 4 out of 5

2nd unit 1st had a problem. This is ok A manual would help. Went and got a windows 8 book..

good laptop

POSTED BY: ge , parma,ohio
Overall rating: 3 out of 5 3 out of 5

The laptop itself I like. I also like the Toshiba software. The Problems I have are with the Windows 8 user interface that stops working and I can't do any thing about it. Except to turn off the unit and disconnect the battery and reconnect it and turn it back on.

Hate this laptop

POSTED BY: George , Venice, Fl
Overall rating: 2 out of 5 2 out of 5

There's nothing about this laptop that I like. I hate Windows 8, I hate the "speakers"- I only use this for a few programs that I need and don't use it for anything recreational at all.

No longer works after three weeks

POSTED BY: lambchop , Sulphur, LA
Overall rating: 1 out of 5 1 out of 5

Windows no longer works and it shuts down


POSTED BY: Mike , Chicago, IL
Overall rating: 1 out of 5 1 out of 5

Toshiba should consider removing this outdated and technically berift product from its inventory, as the satellite laptop has the potential to tarnish the overall superiority of the company brand.

Hate the operating system

POSTED BY: J.R. , Illinois
Overall rating: 1 out of 5 1 out of 5

I have had this laptop for 1 month now and still not using it because of windows 8. It is the hardest program I have ever tried to work with. If I could return this laptop I would. I got a book from the library called windows 8 for dummies and still it is difficult. I have been to college for computers so am not a newbie to computers. So disapointed since this is the first brand new computer I have ever owned. uggg I don't think there is a problem with the Toshiba brand it is the windows 8.

MSRP: $419.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Pentium® Processor B980
  • Windows 8
  • 4GB DDR3 1333MHz memory
  • Intel® Integrated Graphics
  • 500GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

shop for accessories