Toshiba Satellite C855-S5356 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Good deal

POSTED BY: Andy , Evansville, In.
Overall rating: 5 out of 5 5 out of 5

For the money, this computer is a good buy.

Very Good Laptop

POSTED BY: Olivia , Charlotte, NC
Overall rating: 5 out of 5 5 out of 5

I love my Toshiba Laptop. It has so many great features. I will recommend it to my friends. Toshiba Customer Support is available to assist me when I need help.

plan to make it a workhorse

POSTED BY: irishgal , indiana
Overall rating: 5 out of 5 5 out of 5

I bought this computer for a new at -home computer job. I plan to work it hard and feel that it will meet or exceed my expectations.

NANA'S LAPTOP

POSTED BY: NANA , TN
Overall rating: 5 out of 5 5 out of 5

I LOVE MY COMPUTER THE ONLY THING I DON'T LIKE IS THE SIDE BAR THAT POPS UP ALL THE TIME I'D LIKE TO BE ABLE TO REMOVE THIS FROM MY SIDE IF THAT IS POSSIBLE WOULD U PLEASE TELL ME HOW

Nice bang for the buck.

POSTED BY: Mad Max , Pittsburgh Pa
Overall rating: 5 out of 5 5 out of 5

Toshiba has a nice lap top on their hands. This is my first one and so far it works as good as the desk top. I am just getting use to the windows 8 also coming from a I-mac. So there is a bit of a learning curve to the lap top and the desk top but so far so good...

Excellent Laptop

POSTED BY: Withney , Puerto Rico
Overall rating: 5 out of 5 5 out of 5

Excellent Laptop, long battery life. I recommend it. And for the price is perfect.

c855-s5356

POSTED BY: Bub , Phoenix, Az
Overall rating: 4 out of 5 4 out of 5

fast startup, price was a bit much but that's due to the retailer I purchased it from. The key board seems a bit weak and flimsy at and around the j&k keys....seems unsupported. would like to see more apps. from Toshiba's support . All in all the performance is exceptional and haven't had any programing issues

Great Laptop for internet usage...

POSTED BY: jenjen , Waterloo, IA
Overall rating: 4 out of 5 4 out of 5

I bought the Toshiba because my husband and son have had great luck with theirs over the last 3 years. It was a challenge to get used to Windows 8 however once I got going things were very easy.

For that price, dude... Must buy it!

POSTED BY: epluribusunum26
Overall rating: 4 out of 5 4 out of 5

I don't care too much about the bluetooth issue 'cause I don't need it. It's a really cool and complete model for that price. If you want to buy your first laptop, this is one of your best options, I mean it.

Nice Laptop

POSTED BY: myrtlerp , Midvale, UT
Overall rating: 4 out of 5 4 out of 5

This seems to be a nice laptop but I did not receive a users manual. I have never used Toshiba before so a manual would have been helpfu

New Laptop User

POSTED BY: Dona , Binghamton, NY
Overall rating: 4 out of 5 4 out of 5

This machine makes it easy to learn Windows 8,Office 2013, and how to use a Laptop

The sound annoy me!

POSTED BY: CAp , Py
Overall rating: 3 out of 5 3 out of 5

I do not understand why you people make the sound on this Laptop so bad, I try to fix it but I can not. The volume level even on 100% is low, and well... I not happy about it. You diagnostic software is useful, and the other feature is OK.

worst labtop

POSTED BY: jurnee05p , richmond, in 47374
Overall rating: 1 out of 5 1 out of 5

We did not even have it a month and the screen is messed up. Should have with hb. I will not pay the money out for your lab top and its messed up less then a month. Not worth no stars

POSTED BY: Timber , Sylva, n.c.
Overall rating: 1 out of 5 1 out of 5

I am not sure if it was hardware problem or windows 8 problem but each day I experienced different issues until finally the computer would not even power up. I returned it after less than a week of ownership.

poores ever

POSTED BY: nonee , topeka ks
Overall rating: 1 out of 5 1 out of 5

it wil not scrolldound on e mails .it will not let one enlarge email an also will not reduce so one cad read the whole email it also doenot have spam or trash can what good is it when you can only read half of emails would like to ship back for full refund

MSRP: $479.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i3-2328M Processor
  • Windows 8
  • 4GB DDR3 1333MHz memory
  • Intel® Integrated Graphics
  • 640GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

shop for accessories