Toshiba Satellite C855-S5358 Laptop

Average Customer Rating:

goes great with check to include

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

VERY GOOD LAPTOP EVER SINCE

POSTED BY: ASTERN , MANAMA, BAHRAIN
Overall rating: 5 out of 5 5 out of 5

THIS KIND OF LAPTOP I DID NOT SEEN BEFORE IN MARKET.. TODAY I WOULD LIKE TO SAY ALL TOSHIBA COMPANY.. BEST WISHES ALL

amazing

POSTED BY: N/A , rockville centre, NY
Overall rating: 5 out of 5 5 out of 5

A friend has this same laptop and that was my deciding moment. i found it easy to munerver, light weight and easy to learn.

Tohiba

POSTED BY: taz , Kissimmee, Fl
Overall rating: 5 out of 5 5 out of 5

I have owned Toshiba laptops in the past and they are great, im glad I have this new one !!!

Very Good Laptop!

POSTED BY: ROMPEDOR , Atlanta GA
Overall rating: 4 out of 5 4 out of 5

Performance es very good. and I know I made a good investment I can always trust to be available.

Toshiba c855-s5358

POSTED BY: 30378 , Deer Park Tx
Overall rating: 4 out of 5 4 out of 5

Great mid level computer. Does everything I want. Wish the keyboard had a little more reflectivity to the lettering. Only thing I don't like is Windows 8. I hate the 8!!!

poketypoke

POSTED BY: poketypoke , california
Overall rating: 4 out of 5 4 out of 5

First, let me tell Big Joe, push F5 and it will unlock the cursor,. Next I think for the money this is a great machine Have not had this machine long but for the time I have had it its great

Power cord faulty

POSTED BY: Jan , Stanford. Ky
Overall rating: 4 out of 5 4 out of 5

Seems to be a good computer but my power cord will not stay plugged in at converter box!

Great computer and for the price can't be beat.

POSTED BY: captbanny , Lakeland, Fl
Overall rating: 4 out of 5 4 out of 5

I would definately recommend this laptop to a friend that has had a computer for a while, but not as a first one as this windows 8 takes a lot of getting use to. I have had a computer for around 18 years and I am still having some issues that I am still learning. As far as the quality and speed it is great.

POSTED BY: Marty , Palo Alto, CA
Overall rating: 4 out of 5 4 out of 5

Very good price value. And the processing is fast!! But the touchpad is frustrating. Its very sensitive and is way too easy to inadvertently switch screens and not be able to get back to where you were working. That's where I loose performance.

It's Ok

POSTED BY: javabrk , New York
Overall rating: 3 out of 5 3 out of 5

The computer is fine. It's fast and can handle muti-tasking easily but, when it arrived, I found the back plate that covers the drive not secured properly. It was put on carelessly. The sound system sounds like a tin can phone and there is not enough expansion ports. Other than that, So far, it does the job.

CUSOR LOCKED UP

POSTED BY: BIG JOE , LAS VEGAS
Overall rating: 2 out of 5 2 out of 5

NOT WORKING --WHAT DO I DO TO GET FIXED??

Very Disappointed

POSTED BY: tjouras , Bloomfield Hills, MI
Overall rating: 1 out of 5 1 out of 5

Laptop quality was disappointing. Especially for the price. Speakers were terrible. Returned item immediately after listening to the speakers. Would not recommend to others. Very disappointed!!

MSRP: $529.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i3-2328M Processor
  • Windows 8
  • 6GB DDR3 1333MHz memory
  • Intel® Integrated Graphics
  • 500GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

shop for accessories